![]() |
![]() |
Need to further review and define. Probably need hooks for user-defined states, in addition to some pre-defined ones.
Complete description. Original was "gives lesser output buffer size, don't return error"
inBufs
and outBufs
are correctly described. Need to better wordsmith this section.
Need further description.
We should explore what we did in the speech interfaces and perhaps create an ivideo_vc1.h with VC1-specific definitions.
Need further description.
We should explore what we did in the speech interfaces and perhaps create an ivideo_vc1.h with VC1-specific definitions.
Is this in pixels?
Should this field and scalingHeight use a XDM_Rect data type?
Do we need a default value for this enum?
Request from DM365 team to split IVIDEO_SLICEMODE into IVIDEO_SLICEMODE_BYTE and IVIDEO_SLICEMODE_NAL.
Do we need a default value for this enum?
Should "decode" and "encode" modes change to "process full frame"? For example, setting DECODE_ONLY for an encoder is wrong - can we make it impossible for codecs/apps to make this error?
Do we need a default value for this enum?
Needs review
Needs review
What cache coherency responsibilities are placed on this buffer?
Needs review and further detail
Needs review