![]() |
![]() |
Defines the input arguments for all IVIDENC2 instance process function. More...
#include <ividenc2.h>
Data Fields | |
XDAS_Int32 | size |
XDAS_Int32 | inputID |
XDAS_Int32 | control |
Defines the input arguments for all IVIDENC2 instance process function.
size
parameter. size
field must be correctly set by the caller.Size of this structure in bytes. Because this structure can be extended, this field must be correctly set by the caller.
Identifier to attach with the corresponding input frames to be encoded.
Encoder control operations