XDM_DataSyncDesc Struct Reference
[XDM - Shared XDM Definitions]

Descriptor for the chunk of data being transferred in one call to putData or getData. More...

#include <xdm.h>

Data Fields

XDAS_Int32 size
XDAS_Int32 scatteredBlocksFlag
XDAS_Int32baseAddr
XDAS_Int32 numBlocks
XDAS_Int32 varBlockSizesFlag
XDAS_Int32blockSizes

Detailed Description

Descriptor for the chunk of data being transferred in one call to putData or getData.


Field Documentation

Size of this structure in bytes. Because this structure can be extended, this field must be correctly set by the caller.

Flag indicating whether the individual data blocks may be scattered in memory.

Remarks:
Note that each individual block must be physically contiguous.
Valid values are XDAS_TRUE and XDAS_FALSE.
If set to XDAS_FALSE, the baseAddr field points directly to the start of the first block, and is not treated as a pointer to an array.
If set to XDAS_TRUE, the baseAddr array must contain the base address of each individual block.

Base address of single data block or pointer to an array of data block addresses of size numBlocks.

Remarks:
If scatteredBlocksFlag is set to XDAS_FALSE, this field points directly to the start of the first block, and is not treated as a pointer to an array.
If scatteredBlocksFlag is set to XDAS_TRUE, this field points to an array of pointers to the data blocks.

Number of blocks available

Flag indicating whether any of the data blocks vary in size.

Remarks:
Valid values are XDAS_TRUE and XDAS_FALSE.

Variable block sizes array.

Remarks:
If varBlockSizesFlag is XDAS_TRUE, this array contains the sizes of each block. If varBlockSizesFlag is XDAS_FALSE, this contains the size of same-size blocks.
Memory for this array (of size numBlocks) has to be allocated by the caller of the putData API.

The documentation for this struct was generated from the following file:
 All Data Structures Files Functions Variables Typedefs Enumerations Enumerator Defines

Copyright 2009, Texas Instruments Incorporated