![]() |
![]() |
This structure defines the codec parameters that can be modified after creation via control() calls. More...
#include <ividenc.h>
This structure defines the codec parameters that can be modified after creation via control() calls.
size
parameter. size
field must be correctly set by the caller.Size of this structure in bytes. Because this structure can be extended, this field must be correctly set by the caller.
Input frame height.
Input frame width.
Reference or input frame rate * 1000.
Target frame rate * 1000.
Target bit rate in bits per second.
I frame interval. For example, 30.
Encode entire access unit or only header.
DEFAULT(0): use imagewidth as pitch else use given capture width for pitch provided it is greater than image width.
Force the current frame to be encoded as an I-frame.