IVIDDEC_Params Struct Reference
[IVIDDEC - XDM Video Decoder Interface]

Defines the creation time parameters for all IVIDDEC instance objects. More...

#include <ividdec.h>

Data Fields

XDAS_Int32 size
XDAS_Int32 maxHeight
XDAS_Int32 maxWidth
XDAS_Int32 maxFrameRate
XDAS_Int32 maxBitRate
XDAS_Int32 dataEndianness
XDAS_Int32 forceChromaFormat

Detailed Description

Defines the creation time parameters for all IVIDDEC instance objects.

Remarks:
The application should set the parameters to 0 to use the algorithm's default values.
This structure may be extended by individual codec implementation allowing customization with vendor specific parameters.
The size field must be correctly set by the caller.

Field Documentation

Size of this structure in bytes. Because this structure can be extended, this field must be correctly set by the caller.

Maximum video height in pixels.

Maximum video width in pixels.

Maximum frame rate in fps * 1000.

Maximum bit rate, bits per second. For example, if bit rate is 10 Mbps, set this field to 10000000

Endianness of input data.

See also:
XDM_DataFormat

Force decode in given Chroma format.

See also:
XDM_ChromaFormat

The documentation for this struct was generated from the following file:
 All Data Structures Files Functions Variables Typedefs Enumerations Enumerator Defines

Copyright 2009, Texas Instruments Incorporated