IAUDENC1_Status Struct Reference
[IAUDENC1 - Audio Encoder Interface]

Defines instance status parameters (read-only). More...

#include <iaudenc1.h>

Collaboration diagram for IAUDENC1_Status:
Collaboration graph
[legend]

Data Fields

XDAS_Int32 size
XDAS_Int32 extendedError
XDM1_SingleBufDesc data
XDM_AlgBufInfo bufInfo
XDAS_Int32 validFlag
XDAS_Int32 lfeFlag
XDAS_Int32 bitRate
XDAS_Int32 sampleRate
XDAS_Int32 channelMode
XDAS_Int32 encMode

Detailed Description

Defines instance status parameters (read-only).

Remarks:
This structure may be extended by individual codec implementations allowing customization with vendor specific parameters. The presence of vendor specific extensions will be detected by the value of the size parameter.
The size field must be correctly set by the caller.
See also:
IAUDENC1_Fxns::control()

Field Documentation

Size of this structure in bytes. Because this structure can be extended, this field must be correctly set by the caller.

Extended error information.

Remarks:
When an internal error occurs, the algorithm will return an error return value (e.g. EFAIL, EUNSUPPORTED)
The value of each enum is the bit which is set.
Bits 31-16 are reserved. Bits 7-0 are codec and implementation specific.
The algorithm can set multiple bits to 1 based on conditions. e.g. it will set bits XDM_FATALERROR (fatal) and XDM_UNSUPPORTEDPARAM (unsupported params) in case of unsupported run time parameters.
This enumeration data type should not be used for storage, but rather only for its constant values.

See also:
XDM_ErrorBit

Buffer descriptor for data passing.

Remarks:
This buffer can be used as either input or output, depending on the command.
The buffer will be provided by the application, and returned to the application upon return of the control() call. The algorithm must not retain a pointer to this data.
See also:
XDM_GETVERSION

Input and output buffer information.

See also:
XDM_AlgBufInfo

Flag indicating the validity of the status struct.

Valid values for this field are XDAS_TRUE and XDAS_FALSE.

Flag indicating whether LFE channel data is present or not in the input.

Valid values for this field are XDAS_TRUE and XDAS_FALSE.

Average bit rate, in bits per second.

See also:
IAUDENC1_Params.bitRate
IAUDENC1_DynamicParams.bitRate

Sampling frequency in Hz. For example, if the sampling frequency is 44.1 kHz, this field will be 44100.

See also:
IAUDENC1_Params.sampleRate
IAUDENC1_DynamicParams.sampleRate

Encoding mode.

See also:
IAUDIO_EncMode
IAUDENC1_Params.encMode

The documentation for this struct was generated from the following file:
 All Data Structures Files Functions Variables Typedefs Enumerations Enumerator Defines

Copyright 2009, Texas Instruments Incorporated