![]() |
![]() |
This structure defines the algorithm parameters that can be modified after creation via control() calls. More...
#include <ividenc1.h>
This structure defines the algorithm parameters that can be modified after creation via control() calls.
size
parameter. size
field must be correctly set by the caller.Size of this structure in bytes. Because this structure can be extended, this field must be correctly set by the caller.
Input frame height.
Input frame width.
Reference, or input, frame rate in fps * 1000.
Target frame rate in fps * 1000.
Target bit rate in bits per second.
The number of frames between two I frames. For example, 30.
Encode entire access unit or only header.
DEFAULT(0): use imagewidth as pitch else use given capture width for pitch provided it is greater than image width.
Force the current (immediate) frame to be encoded as a specific frame type.
Number of B frames between two reference frames; that is, the number of B frames between two P frames or I/P frames. DEFAULT(0).
Flag to indicate that the algorithm should use MB data supplied in additional buffer within inBufs.