![]() |
![]() |
Defines the creation time parameters for all IAUDDEC instance objects. More...
#include <iauddec.h>
Data Fields | |
XDAS_Int32 | size |
XDAS_Int32 | maxSampleRate |
XDAS_Int32 | maxBitrate |
XDAS_Int32 | maxNoOfCh |
XDAS_Int32 | dataEndianness |
Defines the creation time parameters for all IAUDDEC instance objects.
size
parameter. size
field must be correctly set by the caller. Size of this structure in bytes. Because this structure can be extended, this field must be correctly set by the caller.
Maximum sampling frequency in Hz. For example, if the maximum sampling frequency is 44.1 kHz, this field should be 44100.
Maximum bit rate in bits per second. For example, if the maximum bit rate is 128 kbps, set this field to 128000.
Maximum Channels. See IAUDIO_ChannelId.
Endianness of input data.