IVIDANALYTICS_Params Struct Reference
[XDM Beta Video Analytics Interface]

Defines the creation time parameters for all IVIDANALYTICS instance objects. More...

#include <ividanalytics.h>

Data Fields

XDAS_Int32 size
XDAS_Int32 maxHeight
XDAS_Int32 maxWidth
XDAS_Int32 maxFrameRate
XDAS_Int32 dataEndianness
XDAS_Int32 inputChromaFormat
XDAS_Int32 maxRules

Detailed Description

Defines the creation time parameters for all IVIDANALYTICS instance objects.

Remarks:
This structure may be extended by individual codec implementations allowing customization with vendor specific parameters. The presence of vendor specific extensions will be detected by the value of the size parameter.
The size field must be correctly set by the caller.

Field Documentation

Size of this structure in bytes. Because this structure can be extended, this field must be correctly set by the caller.

Maximum video height in pixels.

Maximum video width in pixels.

Maximum frame rate in fps * 1000. For example, if max frame rate is 30 frames per second, set this field to 30000.

Endianness of output data.

See also:
XDM_DataFormat

Chroma format for the input buffer.

See also:
XDM_ChromaFormat

Maximum number of rules allowed.


The documentation for this struct was generated from the following file:
 All Data Structures Files Functions Variables Typedefs Enumerations Enumerator Defines

Copyright 2010, Texas Instruments Incorporated