![]() |
![]() |
Defines the input arguments for all ISPHENC1 instance process function. More...
#include <isphenc1.h>
Data Fields | |
XDAS_Int16 | size |
XDAS_Int16 | nullTrafficChannel |
XDM1_SingleBufDesc | data |
Defines the input arguments for all ISPHENC1 instance process function.
size
parameter. size
field must be correctly set by the caller. Size of this structure in bytes. Because this structure can be extended, this field must be correctly set by the caller.
Enable/disable the null traffic channel.
Raw data input for data transmission.