![]() |
![]() |
Data Structures | |
struct | IVIDENC1_Obj |
This must be the first field of all IVIDENC1 instance objects. More... | |
struct | IVIDENC1_Params |
Defines the creation time parameters for all IVIDENC1 instance objects. More... | |
struct | IVIDENC1_DynamicParams |
This structure defines the algorithm parameters that can be modified after creation via control() calls. More... | |
struct | IVIDENC1_InArgs |
Defines the input arguments for all IVIDENC1 instance process function. More... | |
struct | IVIDENC1_Status |
Defines instance status parameters. More... | |
struct | IVIDENC1_OutArgs |
Defines the run time output arguments for all IVIDENC1 instance objects. More... | |
struct | IVIDENC1_MbData |
Defines the structure that contains macroblock related encoding parameter estimates. More... | |
struct | IVIDENC1_Fxns |
Defines all of the operations on IVIDENC1 objects. More... | |
Defines | |
#define | IVIDENC1_EOK XDM_EOK |
#define | IVIDENC1_EFAIL XDM_EFAIL |
#define | IVIDENC1_EUNSUPPORTED XDM_EUNSUPPORTED |
Typedefs | |
typedef struct IVIDENC1_Obj * | IVIDENC1_Handle |
Opaque handle to an IVIDENC1 objects. | |
typedef IALG_Cmd | IVIDENC1_Cmd |
Defines the control commands for the IVIDENC1 module. |
This is the XDM IVIDENC1 Video Encoder Interface.
#define IVIDENC1_EOK XDM_EOK |
Success.
#define IVIDENC1_EFAIL XDM_EFAIL |
General failure.
#define IVIDENC1_EUNSUPPORTED XDM_EUNSUPPORTED |
Request is unsupported.
typedef struct IVIDENC1_Obj* IVIDENC1_Handle |
Opaque handle to an IVIDENC1 objects.
typedef IALG_Cmd IVIDENC1_Cmd |
Defines the control commands for the IVIDENC1 module.