![]() |
![]() |
Defines the run time output arguments for all IVIDDEC2FRONT instance objects. More...
#include <ividdec2.h>
Data Fields | |
XDAS_Int32 | size |
XDAS_Int32 | extendedError |
XDAS_Int32 | bytesConsumed |
Defines the run time output arguments for all IVIDDEC2FRONT instance objects.
size
parameter. size
field must be correctly set by the caller.Size of this structure in bytes. Because this structure can be extended, this field must be correctly set by the caller.
Extended error information.
Number of bytes consumed during the process() call.