![]() |
![]() |
#include <ividenc1.h>
Collaboration diagram for IVIDENC1_Status:
size
parameter.
The size
field must be correctly set by the caller.
Data Fields | |
XDAS_Int32 | size |
XDAS_Int32 | extendedError |
XDM1_SingleBufDesc | data |
XDM_AlgBufInfo | bufInfo |
Size of this structure in bytes. Because this structure can be extended, this field must be correctly set by the caller.
Extended error information.
The value of each enum is the bit which is set.
Bits 31-16 are reserved. Bits 7-0 are codec and implementation specific.
The algorithm can set multiple bits to 1 based on conditions. e.g. it will set bits XDM_FATALERROR (fatal) and XDM_UNSUPPORTEDPARAM (unsupported params) in case of unsupported run time parameters.
This enumeration data type should not be used for storage, but rather only for its constant values.
Buffer descriptor for data passing.
data.buf
to NULL.This buffer can be used as either input or output, depending on the command.
The buffer will be provided by the application, and returned to the application upon return of the IVIDENC1_Fxns.control() call. The algorithm must not retain a pointer to this data.
Input and output buffer information.
When configured to generate reconstruction buffers (see IVIDENC1_Params::reconChromaFormat), the recontruction buffer information will also be reported here.