![]() |
![]() |
#include <ividenc.h>
This structure may be extended by individual codec implementations allowing customization with vendor specific parameters. The presence of vendor specific extensions will be detected by the value of the size
parameter.
The size
field must be correctly set by the caller.
Size of this structure in bytes. Because this structure can be extended, this field must be correctly set by the caller.
Input frame height.
Input frame width.
Reference or input frame rate * 1000.
Target frame rate * 1000.
Target bit rate in bits per second.
I frame interval. For example, 30.
Encode entire access unit or only header.
This enumeration defines a base set of values. Algorithms which require proprietary enumeration values may define them - much like extended fields in base structures. These extended enums should be between XDM_CUSTOMENUMBASE and 0x7FFF.
DEFAULT(0): use imagewidth as pitch else use given capture width for pitch provided it is greater than image width.
Force the current frame to be encoded as an I-frame.