#include <iauddec.h>
Collaboration diagram for IAUDDEC_Status:
size
parameter.
The size
field must be correctly set by the caller.
Size of this structure in bytes. Because this structure can be extended, this field must be correctly set by the caller.
Extended error information.
The value of each enum is the bit which is set.
Bits 31-16 are reserved. Bits 7-0 are codec and implementation specific.
The algorithm can set multiple bits to 1 based on conditions. e.g. it will set bits XDM_FATALERROR (fatal) and XDM_UNSUPPORTEDPARAM (unsupported params) in case of unsupported run time parameters.
This enumeration data type should not be used for storage, but rather only for its constant values.
Average bit rate, in bits per second.
Sampling frequency, in Hz. For example, if the sampling frequency is 44.1 kHz, this field will be 44100.
Number of Channels. See IAUDIO_ChannelId.
Number of LFE (Low Frequency Effects) channels in the stream.
The output PCM format. See IAUDIO_PcmFormat.
Flag to indicate support for random position decoding, which means that a stream can be decoded from any point. 0 indicates this feature is not supported, 1 indicates this feature is supported.
Recommended fast forward length in bytes in case of random position decoding.
Number of samples decoded per process() call.
Number of bits per output sample. For example, if the value of the field is 16, there are 16 output bits per PCM sample.
Input and output buffer information. See XDM_AlgBufInfo.