![]() |
![]() |
#include <xdm.h>
Data Fields | |
XDAS_Int8 * | buf |
XDAS_Int32 | bufSize |
XDAS_Int32 | accessMask |
Pointer to a buffer address.
Size of buf
in 8-bit bytes.
Mask filled by the algorithm, declaring how the buffer was accessed by the algorithm processor.
It is acceptible (and appropriate!)to set several bits in this mask if the algorithm accessed the buffer in several ways.
This mask is often used by the application and/or framework to appropriately manage cache on cache-based systems.