![]() |
![]() |
TI-RTOS Drivers
tidrivers_cc13xx_cc26xx_2_21_01_01
|
CryptoCC26XX AES-CCM Transaction. More...
#include <CryptoCC26XX.h>
Data Fields | |
CryptoCC26XX_Operation | opType |
CryptoCC26XX_Mode | mode |
uint8_t | keyIndex |
uint8_t | authLength |
char * | nonce |
char * | msgIn |
char * | header |
void * | msgOut |
uint8_t | fieldLength |
uint16_t | msgInLength |
uint16_t | headerLength |
CryptoCC26XX AES-CCM Transaction.
The Counter with CBC-MAC (CCM) mode of operation is a generic authenticated encryption block cipher mode. It can be used with any 128-bit block cipher. AES-CCM combines CBC-MAC with an AES block cipher.
AES-CCM encryption has the following inputs and outputs:
Encryption | Decryption |
---|---|
Input | |
Shared AES key | Shared AES key |
Nonce | Nonce |
Cleartext | Ciphertext (encrypted cleartext + MAC) |
AAD (optional) | AAD (optional) |
Output | |
Ciphertext (encrypted cleartext + MAC) | Cleartext |
The AES key is a shared secret between the two parties and has a length of 128 Bit. The key is stored in the dedicated RAM of the AES hardware unit before the crypto operation.
The nonce is generated by the party performing the authenticated encryption operation. Within the scope of any authenticated encryption key, the nonce value must be unique. That is, the set of nonce values used with any given key must not contain any duplicate values. Using the same nonce for two different messages encrypted with the same key destroys the security properties.
The optional AAD is authenticated, but not encrypted. Thus, the AAD is not included in the AES-CCM output. It can be used to authenticate packet headers for transport layer security.
After the encryption operation, the ciphertext contains the encrypted data and the message authentication code (MAC). The MAC can be seen as an encrypted fingerprint of the message header and content.
AES-CCM works in both ways: encryption and decryption. When a message is decrypted, then ciphertext, AAD and nonce are used as inputs while the output comprises the cleartext only. The decryption operation is successful, when the received ciphertext, the nonce and the AAD can reproduce the containing MAC.
The CryptoCC26XX_AESCCM_Transaction structure defines all necessary parameters for a AES-CCM transaction.
CryptoCC26XX_Operation CryptoCC26XX_AESCCM_Transaction::opType |
The type of the crypto operation
CryptoCC26XX_Mode CryptoCC26XX_AESCCM_Transaction::mode |
The mode of current transaction. Set by transact function.
uint8_t CryptoCC26XX_AESCCM_Transaction::keyIndex |
The key store index to be used
uint8_t CryptoCC26XX_AESCCM_Transaction::authLength |
Is the the length of the authentication field 0, 2, 4, 6, 8, 10, 12, 14 or 16 octets.
char* CryptoCC26XX_AESCCM_Transaction::nonce |
A pointer to 13-byte or 12-byte Nonce.
char* CryptoCC26XX_AESCCM_Transaction::msgIn |
char* CryptoCC26XX_AESCCM_Transaction::header |
The Additional Authentication Data (AAD). This header is authenticated but not encrypted.
void* CryptoCC26XX_AESCCM_Transaction::msgOut |
A pointer to the encrypted CBC-MAC
uint8_t CryptoCC26XX_AESCCM_Transaction::fieldLength |
Encoded length of the nonce.
fieldLength | nonce length |
---|---|
2 | 13 byte nonce |
3 | 12 byte nonce |
uint16_t CryptoCC26XX_AESCCM_Transaction::msgInLength |
uint16_t CryptoCC26XX_AESCCM_Transaction::headerLength |
The length of the header in octets