![]() |
![]() |
TI-RTOS Drivers
tidrivers_cc13xx_cc26xx_2_21_01_01
|
![]() |
Macros | |
#define | WiFi_STATUS_SUCCESS 0 |
Successful status code returned by WiFi_control(). More... | |
#define | WiFi_STATUS_ERROR -1 |
Generic error status code returned by WiFi_control(). More... | |
#define | WiFi_STATUS_UNDEFINEDCMD -2 |
An error status code returned by WiFi_control() for undefined command codes. More... | |
WiFi_STATUS_* macros are general status codes returned by WiFi_control()
#define WiFi_STATUS_SUCCESS 0 |
Successful status code returned by WiFi_control().
WiFi_control() returns WiFi_STATUS_SUCCESS if the control code was executed successfully.
#define WiFi_STATUS_ERROR -1 |
Generic error status code returned by WiFi_control().
WiFi_control() returns WiFi_STATUS_ERROR if the control code was not executed successfully.
#define WiFi_STATUS_UNDEFINEDCMD -2 |
An error status code returned by WiFi_control() for undefined command codes.
WiFi_control() returns WiFi_STATUS_UNDEFINEDCMD if the control code is not recognized by the driver implementation.