Receiver Test Command. More...
#include <rf_common_cmd.h>
Data Fields | |
| uint16_t | commandNo |
| The command ID number 0x0807. More... | |
| uint16_t | status |
| An integer telling the status of the command. This value is updated by the radio CPU during operation and may be read by the system CPU at any time. More... | |
| rfc_radioOp_t * | pNextOp |
| Pointer to the next operation to run after this operation is done. More... | |
| ratmr_t | startTime |
Absolute or relative start time (depending on the value of startTrigger) More... | |
| struct { | |
| uint8_t triggerType:4 | |
| The type of trigger. More... | |
| uint8_t bEnaCmd:1 | |
| 0: No alternative trigger command 1: CMD_TRIGGER can be used as an alternative trigger More... | |
| uint8_t triggerNo:2 | |
| The trigger number of the CMD_TRIGGER command that triggers this action. More... | |
| uint8_t pastTrig:1 | |
| 0: A trigger in the past is never triggered, or for start of commands, give an error 1: A trigger in the past is triggered as soon as possible More... | |
| } | startTrigger |
| Identification of the trigger that starts the operation. More... | |
| struct { | |
| uint8_t rule:4 | |
| Condition for running next command: Rule for how to proceed. More... | |
| uint8_t nSkip:4 | |
| Number of skips + 1 if the rule involves skipping. 0: same, 1: next, 2: skip next, ... More... | |
| } | condition |
| struct { | |
| uint8_t bEnaFifo:1 | |
| 0: Do not enable FIFO in modem, so that received data is not available 1: Enable FIFO in modem – the data must be read out by the application More... | |
| uint8_t bFsOff:1 | |
| 0: Keep frequency synth on after command 1: Turn frequency synth off after command More... | |
| uint8_t bNoSync:1 | |
| 0: Run sync search as normal for the configured mode 1: Write correlation thresholds to the maximum value to avoid getting sync More... | |
| } | config |
| struct { | |
| uint8_t triggerType:4 | |
| The type of trigger. More... | |
| uint8_t bEnaCmd:1 | |
| 0: No alternative trigger command 1: CMD_TRIGGER can be used as an alternative trigger More... | |
| uint8_t triggerNo:2 | |
| The trigger number of the CMD_TRIGGER command that triggers this action. More... | |
| uint8_t pastTrig:1 | |
| 0: A trigger in the past is never triggered, or for start of commands, give an error 1: A trigger in the past is triggered as soon as possible More... | |
| } | endTrigger |
| Trigger classifier for ending the operation. More... | |
| uint32_t | syncWord |
| Sync word to use for receiver. More... | |
| ratmr_t | endTime |
| Time to end the operation. More... | |
Receiver Test Command.
Definition at line 290 of file rf_common_cmd.h.
| uint8_t rfc_CMD_RX_TEST_s::bEnaCmd |
0: No alternative trigger command
1: CMD_TRIGGER can be used as an alternative trigger
Definition at line 299 of file rf_common_cmd.h.
| uint8_t rfc_CMD_RX_TEST_s::bEnaFifo |
0: Do not enable FIFO in modem, so that received data is not available
1: Enable FIFO in modem – the data must be read out by the application
Definition at line 310 of file rf_common_cmd.h.
| uint8_t rfc_CMD_RX_TEST_s::bFsOff |
0: Keep frequency synth on after command
1: Turn frequency synth off after command
Definition at line 312 of file rf_common_cmd.h.
| uint8_t rfc_CMD_RX_TEST_s::bNoSync |
0: Run sync search as normal for the configured mode
1: Write correlation thresholds to the maximum value to avoid getting sync
Definition at line 314 of file rf_common_cmd.h.
| uint16_t rfc_CMD_RX_TEST_s::commandNo |
The command ID number 0x0807.
Definition at line 291 of file rf_common_cmd.h.
| struct { ... } rfc_CMD_RX_TEST_s::condition |
| struct { ... } rfc_CMD_RX_TEST_s::config |
| ratmr_t rfc_CMD_RX_TEST_s::endTime |
Time to end the operation.
Definition at line 326 of file rf_common_cmd.h.
| struct { ... } rfc_CMD_RX_TEST_s::endTrigger |
Trigger classifier for ending the operation.
| uint8_t rfc_CMD_RX_TEST_s::nSkip |
Number of skips + 1 if the rule involves skipping. 0: same, 1: next, 2: skip next, ...
Definition at line 307 of file rf_common_cmd.h.
| uint8_t rfc_CMD_RX_TEST_s::pastTrig |
0: A trigger in the past is never triggered, or for start of commands, give an error
1: A trigger in the past is triggered as soon as possible
Definition at line 302 of file rf_common_cmd.h.
| rfc_radioOp_t* rfc_CMD_RX_TEST_s::pNextOp |
Pointer to the next operation to run after this operation is done.
Definition at line 295 of file rf_common_cmd.h.
| uint8_t rfc_CMD_RX_TEST_s::rule |
Condition for running next command: Rule for how to proceed.
Definition at line 306 of file rf_common_cmd.h.
| ratmr_t rfc_CMD_RX_TEST_s::startTime |
Absolute or relative start time (depending on the value of startTrigger)
Definition at line 296 of file rf_common_cmd.h.
| struct { ... } rfc_CMD_RX_TEST_s::startTrigger |
Identification of the trigger that starts the operation.
| uint16_t rfc_CMD_RX_TEST_s::status |
An integer telling the status of the command. This value is updated by the radio CPU during operation and may be read by the system CPU at any time.
Definition at line 292 of file rf_common_cmd.h.
| uint32_t rfc_CMD_RX_TEST_s::syncWord |
Sync word to use for receiver.
Definition at line 325 of file rf_common_cmd.h.
| uint8_t rfc_CMD_RX_TEST_s::triggerNo |
The trigger number of the CMD_TRIGGER command that triggers this action.
Definition at line 301 of file rf_common_cmd.h.
| uint8_t rfc_CMD_RX_TEST_s::triggerType |
The type of trigger.
Definition at line 298 of file rf_common_cmd.h.