![]() |
![]() |
TI-RTOS Drivers
tidrivers_cc13xx_cc26xx_2_21_00_04
|
UDMACC26XX hardware attributes. More...
#include <UDMACC26XX.h>
Data Fields | |
uint32_t | baseAddr |
PowerCC26XX_Resource | powerMngrId |
uint8_t | intNum |
uint8_t | intPriority |
UDMACC26XX error interrupt priority. intPriority is the DMA peripheral's interrupt priority, as defined by the underlying OS. It is passed unmodified to the underlying OS's interrupt handler creation code, so you need to refer to the OS documentation for usage. For example, for SYS/BIOS applications, refer to the ti.sysbios.family.arm.m3.Hwi documentation for SYS/BIOS usage of interrupt priorities. If the driver uses the ti.drivers.ports interface instead of making OS calls directly, then the HwiP port handles the interrupt priority in an OS specific way. In the case of the SYS/BIOS port, intPriority is passed unmodified to Hwi_create(). More... | |
UDMACC26XX hardware attributes.
uint32_t UDMACC26XX_HWAttrs::baseAddr |
Base adddress for UDMACC26XX
Referenced by UDMACC26XX_channelDisable(), UDMACC26XX_channelDone(), UDMACC26XX_channelEnable(), and UDMACC26XX_clearInterrupt().
PowerCC26XX_Resource UDMACC26XX_HWAttrs::powerMngrId |
UDMACC26XX Peripheral's power manager ID
uint8_t UDMACC26XX_HWAttrs::intNum |
UDMACC26XX error interrupt number
uint8_t UDMACC26XX_HWAttrs::intPriority |
UDMACC26XX error interrupt priority. intPriority is the DMA peripheral's interrupt priority, as defined by the underlying OS. It is passed unmodified to the underlying OS's interrupt handler creation code, so you need to refer to the OS documentation for usage. For example, for SYS/BIOS applications, refer to the ti.sysbios.family.arm.m3.Hwi documentation for SYS/BIOS usage of interrupt priorities. If the driver uses the ti.drivers.ports interface instead of making OS calls directly, then the HwiP port handles the interrupt priority in an OS specific way. In the case of the SYS/BIOS port, intPriority is passed unmodified to Hwi_create().
The CC26xx uses three of the priority bits, meaning ~0 has the same effect as (7 << 5).
(7 << 5) will apply the lowest priority.
(1 << 5) will apply the highest priority.
Setting the priority to 0 is not supported by this driver.
HWI's with priority 0 ignore the HWI dispatcher to support zero-latency interrupts, thus invalidating the critical sections in this driver.