![]() |
![]() |
TI-RTOS Drivers
tidrivers_cc13xx_cc26xx_2_21_00_04
|
![]() |
Macros | |
#define | RF_EventCmdDone (1<<0) |
Radio operation command finished. More... | |
#define | RF_EventLastCmdDone (1<<1) |
Last radio operation command in a chain finished. More... | |
#define | RF_EventTxDone (1<<4) |
Packet transmitted. More... | |
#define | RF_EventTXAck (1<<5) |
ACK packet transmitted. More... | |
#define | RF_EventTxCtrl (1<<6) |
Control packet transmitted. More... | |
#define | RF_EventTxCtrlAck (1<<7) |
Acknowledgement received on a transmitted control packet. More... | |
#define | RF_EventTxCtrlAckAck (1<<8) |
Acknowledgement received on a transmitted control packet, and acknowledgement transmitted for that packet. More... | |
#define | RF_EventTxRetrans (1<<9) |
Packet retransmitted. More... | |
#define | RF_EventTxEntryDone (1<<10) |
Tx queue data entry state changed to Finished. More... | |
#define | RF_EventTxBufferChange (1<<11) |
A buffer change is complete. More... | |
#define | RF_EventRxOk (1<<16) |
Packet received with CRC OK, payload, and not to be ignored. More... | |
#define | RF_EventRxNOk (1<<17) |
Packet received with CRC error. More... | |
#define | RF_EventRxIgnored (1<<18) |
Packet received with CRC OK, but to be ignored. More... | |
#define | RF_EventRxEmpty (1<<19) |
Packet received with CRC OK, not to be ignored, no payload. More... | |
#define | RF_EventRxCtrl (1<<20) |
Control packet received with CRC OK, not to be ignored. More... | |
#define | RF_EventRxCtrlAck (1<<21) |
Control packet received with CRC OK, not to be ignored, then ACK sent. More... | |
#define | RF_EventRxBufFull (1<<22) |
Packet received that did not fit in the Rx queue. More... | |
#define | RF_EventRxEntryDone (1<<23) |
Rx queue data entry changing state to Finished. More... | |
#define | RF_EventDataWritten (1<<24) |
Data written to partial read Rx buffer. More... | |
#define | RF_EventNDataWritten (1<<25) |
Specified number of bytes written to partial read Rx buffer. More... | |
#define | RF_EventRxAborted (1<<26) |
Packet reception stopped before packet was done. More... | |
#define | RF_EventRxCollisionDetected (1<<27) |
A collision was indicated during packet reception. More... | |
#define | RF_EventModulesUnlocked (1<<29) |
As part of the boot process, the CM0 has opened access to RF core modules and memories. More... | |
#define | RF_EventInternalError (uint32_t)(1<<31) |
Internal error observed. More... | |
#define | RF_EventMdmSoft 0x0000002000000000 |
Modem Sync detected (MDMSOFT IFG) More... | |
RF Events reported to callback functions, and used in RF_runCmd(), RF_pendCmd()
#define RF_EventCmdDone (1<<0) |
Radio operation command finished.
#define RF_EventLastCmdDone (1<<1) |
Last radio operation command in a chain finished.
#define RF_EventTxDone (1<<4) |
Packet transmitted.
#define RF_EventTXAck (1<<5) |
ACK packet transmitted.
#define RF_EventTxCtrl (1<<6) |
Control packet transmitted.
#define RF_EventTxCtrlAck (1<<7) |
Acknowledgement received on a transmitted control packet.
#define RF_EventTxCtrlAckAck (1<<8) |
Acknowledgement received on a transmitted control packet, and acknowledgement transmitted for that packet.
#define RF_EventTxRetrans (1<<9) |
Packet retransmitted.
#define RF_EventTxEntryDone (1<<10) |
Tx queue data entry state changed to Finished.
#define RF_EventTxBufferChange (1<<11) |
A buffer change is complete.
#define RF_EventRxOk (1<<16) |
Packet received with CRC OK, payload, and not to be ignored.
#define RF_EventRxNOk (1<<17) |
Packet received with CRC error.
#define RF_EventRxIgnored (1<<18) |
Packet received with CRC OK, but to be ignored.
#define RF_EventRxEmpty (1<<19) |
Packet received with CRC OK, not to be ignored, no payload.
#define RF_EventRxCtrl (1<<20) |
Control packet received with CRC OK, not to be ignored.
#define RF_EventRxCtrlAck (1<<21) |
Control packet received with CRC OK, not to be ignored, then ACK sent.
#define RF_EventRxBufFull (1<<22) |
Packet received that did not fit in the Rx queue.
#define RF_EventRxEntryDone (1<<23) |
Rx queue data entry changing state to Finished.
#define RF_EventDataWritten (1<<24) |
Data written to partial read Rx buffer.
#define RF_EventNDataWritten (1<<25) |
Specified number of bytes written to partial read Rx buffer.
#define RF_EventRxAborted (1<<26) |
Packet reception stopped before packet was done.
#define RF_EventRxCollisionDetected (1<<27) |
A collision was indicated during packet reception.
#define RF_EventModulesUnlocked (1<<29) |
As part of the boot process, the CM0 has opened access to RF core modules and memories.
#define RF_EventInternalError (uint32_t)(1<<31) |
Internal error observed.
#define RF_EventMdmSoft 0x0000002000000000 |
Modem Sync detected (MDMSOFT IFG)