CC26xx Driver Library
uart.h
Go to the documentation of this file.
1 /******************************************************************************
2 * Filename: uart.h
3 * Revised: 2016-07-07 19:12:02 +0200 (Thu, 07 Jul 2016)
4 * Revision: 46848
5 *
6 * Description: Defines and prototypes for the UART.
7 *
8 * Copyright (c) 2015 - 2016, Texas Instruments Incorporated
9 * All rights reserved.
10 *
11 * Redistribution and use in source and binary forms, with or without
12 * modification, are permitted provided that the following conditions are met:
13 *
14 * 1) Redistributions of source code must retain the above copyright notice,
15 * this list of conditions and the following disclaimer.
16 *
17 * 2) Redistributions in binary form must reproduce the above copyright notice,
18 * this list of conditions and the following disclaimer in the documentation
19 * and/or other materials provided with the distribution.
20 *
21 * 3) Neither the name of the ORGANIZATION nor the names of its contributors may
22 * be used to endorse or promote products derived from this software without
23 * specific prior written permission.
24 *
25 * THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS "AS IS"
26 * AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT LIMITED TO, THE
27 * IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR A PARTICULAR PURPOSE
28 * ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT HOLDER OR CONTRIBUTORS BE
29 * LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, SPECIAL, EXEMPLARY, OR
30 * CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT LIMITED TO, PROCUREMENT OF
31 * SUBSTITUTE GOODS OR SERVICES; LOSS OF USE, DATA, OR PROFITS; OR BUSINESS
32 * INTERRUPTION) HOWEVER CAUSED AND ON ANY THEORY OF LIABILITY, WHETHER IN
33 * CONTRACT, STRICT LIABILITY, OR TORT (INCLUDING NEGLIGENCE OR OTHERWISE)
34 * ARISING IN ANY WAY OUT OF THE USE OF THIS SOFTWARE, EVEN IF ADVISED OF THE
35 * POSSIBILITY OF SUCH DAMAGE.
36 *
37 ******************************************************************************/
38 
39 //*****************************************************************************
40 //
45 //
46 //*****************************************************************************
47 
48 #ifndef __UART_H__
49 #define __UART_H__
50 
51 //*****************************************************************************
52 //
53 // If building with a C++ compiler, make all of the definitions in this header
54 // have a C binding.
55 //
56 //*****************************************************************************
57 #ifdef __cplusplus
58 extern "C"
59 {
60 #endif
61 
62 #include <stdbool.h>
63 #include <stdint.h>
64 #include <inc/hw_types.h>
65 #include <inc/hw_uart.h>
66 #include <inc/hw_memmap.h>
67 #include <inc/hw_ints.h>
68 #include <driverlib/interrupt.h>
69 #include <driverlib/debug.h>
70 
71 //*****************************************************************************
72 //
73 // Support for DriverLib in ROM:
74 // This section renames all functions that are not "static inline", so that
75 // calling these functions will default to implementation in flash. At the end
76 // of this file a second renaming will change the defaults to implementation in
77 // ROM for available functions.
78 //
79 // To force use of the implementation in flash, e.g. for debugging:
80 // - Globally: Define DRIVERLIB_NOROM at project level
81 // - Per function: Use prefix "NOROM_" when calling the function
82 //
83 //*****************************************************************************
84 #if !defined(DOXYGEN)
85  #define UARTFIFOLevelGet NOROM_UARTFIFOLevelGet
86  #define UARTConfigSetExpClk NOROM_UARTConfigSetExpClk
87  #define UARTConfigGetExpClk NOROM_UARTConfigGetExpClk
88  #define UARTDisable NOROM_UARTDisable
89  #define UARTCharGetNonBlocking NOROM_UARTCharGetNonBlocking
90  #define UARTCharGet NOROM_UARTCharGet
91  #define UARTCharPutNonBlocking NOROM_UARTCharPutNonBlocking
92  #define UARTCharPut NOROM_UARTCharPut
93  #define UARTIntRegister NOROM_UARTIntRegister
94  #define UARTIntUnregister NOROM_UARTIntUnregister
95 #endif
96 
97 //*****************************************************************************
98 //
99 // Values that can be passed to UARTIntEnable, UARTIntDisable, and UARTIntClear
100 // as the ui32IntFlags parameter, and returned from UARTIntStatus.
101 //
102 //*****************************************************************************
103 #define UART_INT_OE 0x400 // Overrun Error Interrupt Mask
104 #define UART_INT_BE 0x200 // Break Error Interrupt Mask
105 #define UART_INT_PE 0x100 // Parity Error Interrupt Mask
106 #define UART_INT_FE 0x080 // Framing Error Interrupt Mask
107 #define UART_INT_RT 0x040 // Receive Timeout Interrupt Mask
108 #define UART_INT_TX 0x020 // Transmit Interrupt Mask
109 #define UART_INT_RX 0x010 // Receive Interrupt Mask
110 #define UART_INT_CTS 0x002 // CTS Modem Interrupt Mask
111 
112 //*****************************************************************************
113 //
114 // Values that can be passed to UARTConfigSetExpClk as the ui32Config parameter
115 // and returned by UARTConfigGetExpClk in the pui32Config parameter.
116 // Additionally, the UART_CONFIG_PAR_* subset can be passed to
117 // UARTParityModeSet as the ui32Parity parameter, and are returned by
118 // UARTParityModeGet.
119 //
120 //*****************************************************************************
121 #define UART_CONFIG_WLEN_MASK 0x00000060 // Mask for extracting word length
122 #define UART_CONFIG_WLEN_8 0x00000060 // 8 bit data
123 #define UART_CONFIG_WLEN_7 0x00000040 // 7 bit data
124 #define UART_CONFIG_WLEN_6 0x00000020 // 6 bit data
125 #define UART_CONFIG_WLEN_5 0x00000000 // 5 bit data
126 #define UART_CONFIG_STOP_MASK 0x00000008 // Mask for extracting stop bits
127 #define UART_CONFIG_STOP_ONE 0x00000000 // One stop bit
128 #define UART_CONFIG_STOP_TWO 0x00000008 // Two stop bits
129 #define UART_CONFIG_PAR_MASK 0x00000086 // Mask for extracting parity
130 #define UART_CONFIG_PAR_NONE 0x00000000 // No parity
131 #define UART_CONFIG_PAR_EVEN 0x00000006 // Even parity
132 #define UART_CONFIG_PAR_ODD 0x00000002 // Odd parity
133 #define UART_CONFIG_PAR_ONE 0x00000082 // Parity bit is one
134 #define UART_CONFIG_PAR_ZERO 0x00000086 // Parity bit is zero
135 
136 //*****************************************************************************
137 //
138 // Values that can be passed to UARTFIFOLevelSet as the ui32TxLevel parameter
139 // and returned by UARTFIFOLevelGet in the pui32TxLevel.
140 //
141 //*****************************************************************************
142 #define UART_FIFO_TX1_8 0x00000000 // Transmit interrupt at 1/8 Full
143 #define UART_FIFO_TX2_8 0x00000001 // Transmit interrupt at 1/4 Full
144 #define UART_FIFO_TX4_8 0x00000002 // Transmit interrupt at 1/2 Full
145 #define UART_FIFO_TX6_8 0x00000003 // Transmit interrupt at 3/4 Full
146 #define UART_FIFO_TX7_8 0x00000004 // Transmit interrupt at 7/8 Full
147 
148 //*****************************************************************************
149 //
150 // Values that can be passed to UARTFIFOLevelSet as the ui32RxLevel parameter
151 // and returned by UARTFIFOLevelGet in the pui32RxLevel.
152 //
153 //*****************************************************************************
154 #define UART_FIFO_RX1_8 0x00000000 // Receive interrupt at 1/8 Full
155 #define UART_FIFO_RX2_8 0x00000008 // Receive interrupt at 1/4 Full
156 #define UART_FIFO_RX4_8 0x00000010 // Receive interrupt at 1/2 Full
157 #define UART_FIFO_RX6_8 0x00000018 // Receive interrupt at 3/4 Full
158 #define UART_FIFO_RX7_8 0x00000020 // Receive interrupt at 7/8 Full
159 
160 //*****************************************************************************
161 //
162 // Values that can be passed to UARTDMAEnable() and UARTDMADisable().
163 //
164 //*****************************************************************************
165 #define UART_DMA_ERR_RXSTOP 0x00000004 // Stop DMA receive if UART error
166 #define UART_DMA_TX 0x00000002 // Enable DMA for transmit
167 #define UART_DMA_RX 0x00000001 // Enable DMA for receive
168 
169 //*****************************************************************************
170 //
171 // Values returned from UARTRxErrorGet().
172 //
173 //*****************************************************************************
174 #define UART_RXERROR_OVERRUN 0x00000008
175 #define UART_RXERROR_BREAK 0x00000004
176 #define UART_RXERROR_PARITY 0x00000002
177 #define UART_RXERROR_FRAMING 0x00000001
178 
179 //*****************************************************************************
180 //
181 // Values returned from the UARTBusy().
182 //
183 //*****************************************************************************
184 #define UART_BUSY 0x00000001
185 #define UART_IDLE 0x00000000
186 
187 //*****************************************************************************
188 //
189 // API Functions and prototypes
190 //
191 //*****************************************************************************
192 
193 #ifdef DRIVERLIB_DEBUG
194 //*****************************************************************************
195 //
206 //
207 //*****************************************************************************
208 static bool
209 UARTBaseValid(uint32_t ui32Base)
210 {
211  return(( ui32Base == UART0_BASE ) || ( ui32Base == UART0_NONBUF_BASE ));
212 }
213 #endif
214 
215 //*****************************************************************************
216 //
233 //
234 //*****************************************************************************
235 __STATIC_INLINE void
236 UARTParityModeSet(uint32_t ui32Base, uint32_t ui32Parity)
237 {
238  //
239  // Check the arguments.
240  //
241  ASSERT(UARTBaseValid(ui32Base));
242  ASSERT((ui32Parity == UART_CONFIG_PAR_NONE) ||
243  (ui32Parity == UART_CONFIG_PAR_EVEN) ||
244  (ui32Parity == UART_CONFIG_PAR_ODD) ||
245  (ui32Parity == UART_CONFIG_PAR_ONE) ||
246  (ui32Parity == UART_CONFIG_PAR_ZERO));
247 
248  //
249  // Set the parity mode.
250  //
251  HWREG(ui32Base + UART_O_LCRH) = ((HWREG(ui32Base + UART_O_LCRH) &
253  UART_LCRH_PEN)) | ui32Parity);
254 }
255 
256 //*****************************************************************************
257 //
271 //
272 //*****************************************************************************
273 __STATIC_INLINE uint32_t
274 UARTParityModeGet(uint32_t ui32Base)
275 {
276  //
277  // Check the arguments.
278  //
279  ASSERT(UARTBaseValid(ui32Base));
280 
281  //
282  // Return the current parity setting
283  //
284  return(HWREG(ui32Base + UART_O_LCRH) &
286 }
287 
288 //*****************************************************************************
289 //
310 //
311 //*****************************************************************************
312 __STATIC_INLINE void
313 UARTFIFOLevelSet(uint32_t ui32Base, uint32_t ui32TxLevel,
314  uint32_t ui32RxLevel)
315 {
316  //
317  // Check the arguments.
318  //
319  ASSERT(UARTBaseValid(ui32Base));
320  ASSERT((ui32TxLevel == UART_FIFO_TX1_8) ||
321  (ui32TxLevel == UART_FIFO_TX2_8) ||
322  (ui32TxLevel == UART_FIFO_TX4_8) ||
323  (ui32TxLevel == UART_FIFO_TX6_8) ||
324  (ui32TxLevel == UART_FIFO_TX7_8));
325  ASSERT((ui32RxLevel == UART_FIFO_RX1_8) ||
326  (ui32RxLevel == UART_FIFO_RX2_8) ||
327  (ui32RxLevel == UART_FIFO_RX4_8) ||
328  (ui32RxLevel == UART_FIFO_RX6_8) ||
329  (ui32RxLevel == UART_FIFO_RX7_8));
330 
331  //
332  // Set the FIFO interrupt levels.
333  //
334  HWREG(ui32Base + UART_O_IFLS) = ui32TxLevel | ui32RxLevel;
335 }
336 
337 //*****************************************************************************
338 //
361 //
362 //*****************************************************************************
363 extern void UARTFIFOLevelGet(uint32_t ui32Base, uint32_t *pui32TxLevel,
364  uint32_t *pui32RxLevel);
365 
366 //*****************************************************************************
367 //
399 //
400 //*****************************************************************************
401 extern void UARTConfigSetExpClk(uint32_t ui32Base, uint32_t ui32UARTClk,
402  uint32_t ui32Baud, uint32_t ui32Config);
403 
404 //*****************************************************************************
405 //
424 //
425 //*****************************************************************************
426 extern void UARTConfigGetExpClk(uint32_t ui32Base, uint32_t ui32UARTClk,
427  uint32_t *pui32Baud, uint32_t *pui32Config);
428 
429 //*****************************************************************************
430 //
439 //
440 //*****************************************************************************
441 __STATIC_INLINE void
442 UARTEnable(uint32_t ui32Base)
443 {
444  //
445  // Check the arguments.
446  //
447  ASSERT(UARTBaseValid(ui32Base));
448 
449  //
450  // Enable the FIFO.
451  //
452  HWREG(ui32Base + UART_O_LCRH) |= UART_LCRH_FEN;
453 
454  //
455  // Enable RX, TX, and the UART.
456  //
457  HWREG(ui32Base + UART_O_CTL) |= (UART_CTL_UARTEN | UART_CTL_TXE |
458  UART_CTL_RXE);
459 }
460 
461 //*****************************************************************************
462 //
471 //
472 //*****************************************************************************
473 extern void UARTDisable(uint32_t ui32Base);
474 
475 //*****************************************************************************
476 //
484 //
485 //*****************************************************************************
486 __STATIC_INLINE void
487 UARTFIFOEnable(uint32_t ui32Base)
488 {
489  //
490  // Check the arguments.
491  //
492  ASSERT(UARTBaseValid(ui32Base));
493 
494  //
495  // Enable the FIFO.
496  //
497  HWREG(ui32Base + UART_O_LCRH) |= UART_LCRH_FEN;
498 }
499 
500 //*****************************************************************************
501 //
509 //
510 //*****************************************************************************
511 __STATIC_INLINE void
512 UARTFIFODisable(uint32_t ui32Base)
513 {
514  //
515  // Check the arguments.
516  //
517  ASSERT(UARTBaseValid(ui32Base));
518 
519  //
520  // Disable the FIFO.
521  //
522  HWREG(ui32Base + UART_O_LCRH) &= ~(UART_LCRH_FEN);
523 }
524 
525 //*****************************************************************************
526 //
537 //
538 //*****************************************************************************
539 __STATIC_INLINE bool
540 UARTCharsAvail(uint32_t ui32Base)
541 {
542  //
543  // Check the arguments.
544  //
545  ASSERT(UARTBaseValid(ui32Base));
546 
547  //
548  // Return the availability of characters.
549  //
550  return((HWREG(ui32Base + UART_O_FR) & UART_FR_RXFE) ? false : true);
551 }
552 
553 //*****************************************************************************
554 //
565 //
566 //*****************************************************************************
567 __STATIC_INLINE bool
568 UARTSpaceAvail(uint32_t ui32Base)
569 {
570  //
571  // Check the arguments.
572  //
573  ASSERT(UARTBaseValid(ui32Base));
574 
575  //
576  // Return the availability of space.
577  //
578  return((HWREG(ui32Base + UART_O_FR) & UART_FR_TXFF) ? false : true);
579 }
580 
581 //*****************************************************************************
582 //
598 //
599 //*****************************************************************************
600 extern int32_t UARTCharGetNonBlocking(uint32_t ui32Base);
601 
602 //*****************************************************************************
603 //
614 //
615 //*****************************************************************************
616 extern int32_t UARTCharGet(uint32_t ui32Base);
617 
618 //*****************************************************************************
619 //
633 //
634 //*****************************************************************************
635 extern bool UARTCharPutNonBlocking(uint32_t ui32Base, uint8_t ui8Data);
636 
637 //*****************************************************************************
638 //
649 //
650 //*****************************************************************************
651 extern void UARTCharPut(uint32_t ui32Base, uint8_t ui8Data);
652 
653 //*****************************************************************************
654 //
667 //
668 //*****************************************************************************
669 __STATIC_INLINE bool
670 UARTBusy(uint32_t ui32Base)
671 {
672  //
673  // Check the argument.
674  //
675  ASSERT(UARTBaseValid(ui32Base));
676 
677  //
678  // Determine if the UART is busy.
679  //
680  return((HWREG(ui32Base + UART_O_FR) & UART_FR_BUSY) ?
681  UART_BUSY : UART_IDLE);
682 }
683 
684 //*****************************************************************************
685 //
697 //
698 //*****************************************************************************
699 __STATIC_INLINE void
700 UARTBreakCtl(uint32_t ui32Base, bool bBreakState)
701 {
702  //
703  // Check the arguments.
704  //
705  ASSERT(UARTBaseValid(ui32Base));
706 
707  //
708  // Set the break condition as requested.
709  //
710  HWREG(ui32Base + UART_O_LCRH) =
711  (bBreakState ?
712  (HWREG(ui32Base + UART_O_LCRH) | UART_LCRH_BRK) :
713  (HWREG(ui32Base + UART_O_LCRH) & ~(UART_LCRH_BRK)));
714 }
715 
716 //*****************************************************************************
717 //
733 //
734 //*****************************************************************************
735 extern void UARTIntRegister(uint32_t ui32Base, void (*pfnHandler)(void));
736 
737 //*****************************************************************************
738 //
752 //
753 //*****************************************************************************
754 extern void UARTIntUnregister(uint32_t ui32Base);
755 
756 //*****************************************************************************
757 //
777 //
778 //*****************************************************************************
779 __STATIC_INLINE void
780 UARTIntEnable(uint32_t ui32Base, uint32_t ui32IntFlags)
781 {
782  //
783  // Check the arguments.
784  //
785  ASSERT(UARTBaseValid(ui32Base));
786 
787  //
788  // Enable the specified interrupts.
789  //
790  HWREG(ui32Base + UART_O_IMSC) |= ui32IntFlags;
791 }
792 
793 //*****************************************************************************
794 //
813 //
814 //*****************************************************************************
815 __STATIC_INLINE void
816 UARTIntDisable(uint32_t ui32Base, uint32_t ui32IntFlags)
817 {
818  //
819  // Check the arguments.
820  //
821  ASSERT(UARTBaseValid(ui32Base));
822 
823  //
824  // Disable the specified interrupts.
825  //
826  HWREG(ui32Base + UART_O_IMSC) &= ~(ui32IntFlags);
827 }
828 
829 //*****************************************************************************
830 //
851 //
852 //*****************************************************************************
853 __STATIC_INLINE uint32_t
854 UARTIntStatus(uint32_t ui32Base, bool bMasked)
855 {
856  //
857  // Check the arguments.
858  //
859  ASSERT(UARTBaseValid(ui32Base));
860 
861  //
862  // Return either the interrupt status or the raw interrupt status as
863  // requested.
864  //
865  if(bMasked)
866  {
867  return(HWREG(ui32Base + UART_O_MIS));
868  }
869  else
870  {
871  return(HWREG(ui32Base + UART_O_RIS));
872  }
873 }
874 
875 //*****************************************************************************
876 //
910 //
911 //*****************************************************************************
912 __STATIC_INLINE void
913 UARTIntClear(uint32_t ui32Base, uint32_t ui32IntFlags)
914 {
915  //
916  // Check the arguments
917  //
918  ASSERT(UARTBaseValid(ui32Base));
919 
920  //
921  // Clear the requested interrupt sources
922  //
923  HWREG(ui32Base + UART_O_ICR) = ui32IntFlags;
924 }
925 
926 //*****************************************************************************
927 //
945 //
946 //*****************************************************************************
947 __STATIC_INLINE void
948 UARTDMAEnable(uint32_t ui32Base, uint32_t ui32DMAFlags)
949 {
950  //
951  // Check the arguments.
952  //
953  ASSERT(UARTBaseValid(ui32Base));
954 
955  //
956  // Set the requested bits in the UART DMA control register.
957  //
958  HWREG(ui32Base + UART_O_DMACTL) |= ui32DMAFlags;
959 }
960 
961 //*****************************************************************************
962 //
976 //
977 //*****************************************************************************
978 __STATIC_INLINE void
979 UARTDMADisable(uint32_t ui32Base, uint32_t ui32DMAFlags)
980 {
981  //
982  // Check the arguments.
983  //
984  ASSERT(UARTBaseValid(ui32Base));
985 
986  //
987  // Clear the requested bits in the UART DMA control register.
988  //
989  HWREG(ui32Base + UART_O_DMACTL) &= ~ui32DMAFlags;
990 }
991 
992 //*****************************************************************************
993 //
1009 //
1010 //*****************************************************************************
1011 __STATIC_INLINE uint32_t
1012 UARTRxErrorGet(uint32_t ui32Base)
1013 {
1014  //
1015  // Check the arguments.
1016  //
1017  ASSERT(UARTBaseValid(ui32Base));
1018 
1019  //
1020  // Return the current value of the receive status register.
1021  //
1022  return(HWREG(ui32Base + UART_O_RSR) & 0x0000000F);
1023 }
1024 
1025 //*****************************************************************************
1026 //
1037 //
1038 //*****************************************************************************
1039 __STATIC_INLINE void
1040 UARTRxErrorClear(uint32_t ui32Base)
1041 {
1042  //
1043  // Check the arguments.
1044  //
1045  ASSERT(UARTBaseValid(ui32Base));
1046 
1047  //
1048  // Any write to the Error Clear Register will clear all bits which are
1049  // currently set.
1050  //
1051  HWREG(ui32Base + UART_O_ECR) = 0;
1052 }
1053 
1054 //*****************************************************************************
1055 //
1063 //
1064 //*****************************************************************************
1065 __STATIC_INLINE void
1066 UARTHwFlowControlEnable( uint32_t ui32Base )
1067 {
1068  //
1069  // Check the arguments.
1070  //
1071  ASSERT( UARTBaseValid( ui32Base ));
1072 
1073  HWREG( ui32Base + UART_O_CTL ) |= ( UART_CTL_CTSEN | UART_CTL_RTSEN );
1074 }
1075 
1076 //*****************************************************************************
1077 //
1085 //
1086 //*****************************************************************************
1087 __STATIC_INLINE void
1088 UARTHwFlowControlDisable( uint32_t ui32Base )
1089 {
1090  //
1091  // Check the arguments.
1092  //
1093  ASSERT( UARTBaseValid( ui32Base ));
1094 
1095  HWREG( ui32Base + UART_O_CTL ) &= ~( UART_CTL_CTSEN | UART_CTL_RTSEN );
1096 }
1097 
1098 
1099 //*****************************************************************************
1100 //
1101 // Support for DriverLib in ROM:
1102 // Redirect to implementation in ROM when available.
1103 //
1104 //*****************************************************************************
1105 #if !defined(DRIVERLIB_NOROM) && !defined(DOXYGEN)
1106  #include <driverlib/rom.h>
1107  #ifdef ROM_UARTFIFOLevelGet
1108  #undef UARTFIFOLevelGet
1109  #define UARTFIFOLevelGet ROM_UARTFIFOLevelGet
1110  #endif
1111  #ifdef ROM_UARTConfigSetExpClk
1112  #undef UARTConfigSetExpClk
1113  #define UARTConfigSetExpClk ROM_UARTConfigSetExpClk
1114  #endif
1115  #ifdef ROM_UARTConfigGetExpClk
1116  #undef UARTConfigGetExpClk
1117  #define UARTConfigGetExpClk ROM_UARTConfigGetExpClk
1118  #endif
1119  #ifdef ROM_UARTDisable
1120  #undef UARTDisable
1121  #define UARTDisable ROM_UARTDisable
1122  #endif
1123  #ifdef ROM_UARTCharGetNonBlocking
1124  #undef UARTCharGetNonBlocking
1125  #define UARTCharGetNonBlocking ROM_UARTCharGetNonBlocking
1126  #endif
1127  #ifdef ROM_UARTCharGet
1128  #undef UARTCharGet
1129  #define UARTCharGet ROM_UARTCharGet
1130  #endif
1131  #ifdef ROM_UARTCharPutNonBlocking
1132  #undef UARTCharPutNonBlocking
1133  #define UARTCharPutNonBlocking ROM_UARTCharPutNonBlocking
1134  #endif
1135  #ifdef ROM_UARTCharPut
1136  #undef UARTCharPut
1137  #define UARTCharPut ROM_UARTCharPut
1138  #endif
1139  #ifdef ROM_UARTIntRegister
1140  #undef UARTIntRegister
1141  #define UARTIntRegister ROM_UARTIntRegister
1142  #endif
1143  #ifdef ROM_UARTIntUnregister
1144  #undef UARTIntUnregister
1145  #define UARTIntUnregister ROM_UARTIntUnregister
1146  #endif
1147 #endif
1148 
1149 //*****************************************************************************
1150 //
1151 // Mark the end of the C bindings section for C++ compilers.
1152 //
1153 //*****************************************************************************
1154 #ifdef __cplusplus
1155 }
1156 #endif
1157 
1158 #endif // __UART_H__
1159 
1160 //*****************************************************************************
1161 //
1165 //
1166 //*****************************************************************************
void UARTCharPut(uint32_t ui32Base, uint8_t ui8Data)
Waits to send a character from the specified port.
Definition: uart.c:302
#define UART_CONFIG_PAR_ODD
Definition: uart.h:132
#define UART_FIFO_RX2_8
Definition: uart.h:155
static void UARTFIFODisable(uint32_t ui32Base)
Disables the transmit and receive FIFOs.
Definition: uart.h:512
#define UART_FIFO_TX7_8
Definition: uart.h:146
static void UARTIntEnable(uint32_t ui32Base, uint32_t ui32IntFlags)
Enables individual UART interrupt sources.
Definition: uart.h:780
#define UART_FIFO_RX6_8
Definition: uart.h:157
static void UARTFIFOLevelSet(uint32_t ui32Base, uint32_t ui32TxLevel, uint32_t ui32RxLevel)
Sets the FIFO level at which interrupts are generated.
Definition: uart.h:313
static uint32_t UARTIntStatus(uint32_t ui32Base, bool bMasked)
Gets the current interrupt status.
Definition: uart.h:854
void UARTConfigSetExpClk(uint32_t ui32Base, uint32_t ui32UARTClk, uint32_t ui32Baud, uint32_t ui32Config)
Sets the configuration of a UART.
Definition: uart.c:104
static void UARTHwFlowControlEnable(uint32_t ui32Base)
Enables hardware flow control for both CTS and RTS.
Definition: uart.h:1066
#define UART_FIFO_RX7_8
Definition: uart.h:158
void UARTIntRegister(uint32_t ui32Base, void(*pfnHandler)(void))
Registers an interrupt handler for a UART interrupt.
Definition: uart.c:328
static void UARTIntDisable(uint32_t ui32Base, uint32_t ui32IntFlags)
Disables individual UART interrupt sources.
Definition: uart.h:816
void UARTDisable(uint32_t ui32Base)
Disables transmitting and receiving.
Definition: uart.c:174
static void UARTFIFOEnable(uint32_t ui32Base)
Enables the transmit and receive FIFOs.
Definition: uart.h:487
#define UART_BUSY
Definition: uart.h:184
int32_t UARTCharGetNonBlocking(uint32_t ui32Base)
Receives a character from the specified port.
Definition: uart.c:207
#define UART_CONFIG_PAR_EVEN
Definition: uart.h:131
static void UARTBreakCtl(uint32_t ui32Base, bool bBreakState)
Causes a BREAK to be sent.
Definition: uart.h:700
static bool UARTBusy(uint32_t ui32Base)
Determines whether the UART transmitter is busy or not.
Definition: uart.h:670
static void UARTEnable(uint32_t ui32Base)
Enables transmitting and receiving.
Definition: uart.h:442
#define ASSERT(expr)
Definition: debug.h:74
static bool UARTSpaceAvail(uint32_t ui32Base)
Determines if there is any space in the transmit FIFO.
Definition: uart.h:568
#define UART_FIFO_TX6_8
Definition: uart.h:145
#define UART_FIFO_TX4_8
Definition: uart.h:144
void UARTConfigGetExpClk(uint32_t ui32Base, uint32_t ui32UARTClk, uint32_t *pui32Baud, uint32_t *pui32Config)
Gets the current configuration of a UART.
Definition: uart.c:143
#define UART_FIFO_TX1_8
Definition: uart.h:142
#define UART_FIFO_RX4_8
Definition: uart.h:156
static bool UARTCharsAvail(uint32_t ui32Base)
Determines if there are any characters in the receive FIFO.
Definition: uart.h:540
#define UART_CONFIG_PAR_NONE
Definition: uart.h:130
int32_t UARTCharGet(uint32_t ui32Base)
Waits for a character from the specified port.
Definition: uart.c:239
#define UART_CONFIG_PAR_ZERO
Definition: uart.h:134
static void UARTRxErrorClear(uint32_t ui32Base)
Clears all reported receiver errors.
Definition: uart.h:1040
static void UARTDMADisable(uint32_t ui32Base, uint32_t ui32DMAFlags)
Disable UART DMA operation.
Definition: uart.h:979
static uint32_t UARTRxErrorGet(uint32_t ui32Base)
Gets current receiver errors.
Definition: uart.h:1012
static void UARTParityModeSet(uint32_t ui32Base, uint32_t ui32Parity)
Sets the type of parity.
Definition: uart.h:236
#define UART_FIFO_RX1_8
Definition: uart.h:154
bool UARTCharPutNonBlocking(uint32_t ui32Base, uint8_t ui8Data)
Sends a character to the specified port.
Definition: uart.c:265
#define UART_FIFO_TX2_8
Definition: uart.h:143
void UARTFIFOLevelGet(uint32_t ui32Base, uint32_t *pui32TxLevel, uint32_t *pui32RxLevel)
Gets the FIFO level at which interrupts are generated.
Definition: uart.c:76
#define UART_IDLE
Definition: uart.h:185
static void UARTDMAEnable(uint32_t ui32Base, uint32_t ui32DMAFlags)
Enable UART DMA operation.
Definition: uart.h:948
void UARTIntUnregister(uint32_t ui32Base)
Unregisters an interrupt handler for a UART interrupt.
Definition: uart.c:352
static void UARTIntClear(uint32_t ui32Base, uint32_t ui32IntFlags)
Clears UART interrupt sources.
Definition: uart.h:913
#define UART_CONFIG_PAR_ONE
Definition: uart.h:133
static uint32_t UARTParityModeGet(uint32_t ui32Base)
Gets the type of parity currently being used.
Definition: uart.h:274
static void UARTHwFlowControlDisable(uint32_t ui32Base)
Disables hardware flow control for both CTS and RTS.
Definition: uart.h:1088