CC26xx Driver Library
aux_tdc.c
Go to the documentation of this file.
1 /******************************************************************************
2 * Filename: aux_tdc.c
3 * Revised: 2016-06-30 09:21:03 +0200 (Thu, 30 Jun 2016)
4 * Revision: 46799
5 *
6 * Description: Driver for the AUX Time to Digital Converter interface.
7 *
8 * Copyright (c) 2015 - 2016, Texas Instruments Incorporated
9 * All rights reserved.
10 *
11 * Redistribution and use in source and binary forms, with or without
12 * modification, are permitted provided that the following conditions are met:
13 *
14 * 1) Redistributions of source code must retain the above copyright notice,
15 * this list of conditions and the following disclaimer.
16 *
17 * 2) Redistributions in binary form must reproduce the above copyright notice,
18 * this list of conditions and the following disclaimer in the documentation
19 * and/or other materials provided with the distribution.
20 *
21 * 3) Neither the name of the ORGANIZATION nor the names of its contributors may
22 * be used to endorse or promote products derived from this software without
23 * specific prior written permission.
24 *
25 * THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS "AS IS"
26 * AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT LIMITED TO, THE
27 * IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR A PARTICULAR PURPOSE
28 * ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT HOLDER OR CONTRIBUTORS BE
29 * LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, SPECIAL, EXEMPLARY, OR
30 * CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT LIMITED TO, PROCUREMENT OF
31 * SUBSTITUTE GOODS OR SERVICES; LOSS OF USE, DATA, OR PROFITS; OR BUSINESS
32 * INTERRUPTION) HOWEVER CAUSED AND ON ANY THEORY OF LIABILITY, WHETHER IN
33 * CONTRACT, STRICT LIABILITY, OR TORT (INCLUDING NEGLIGENCE OR OTHERWISE)
34 * ARISING IN ANY WAY OUT OF THE USE OF THIS SOFTWARE, EVEN IF ADVISED OF THE
35 * POSSIBILITY OF SUCH DAMAGE.
36 *
37 ******************************************************************************/
38 
39 #include <driverlib/aux_tdc.h>
40 
41 //*****************************************************************************
42 //
43 // Handle support for DriverLib in ROM:
44 // This section will undo prototype renaming made in the header file
45 //
46 //*****************************************************************************
47 #if !defined(DOXYGEN)
48  #undef AUXTDCConfigSet
49  #define AUXTDCConfigSet NOROM_AUXTDCConfigSet
50  #undef AUXTDCMeasurementDone
51  #define AUXTDCMeasurementDone NOROM_AUXTDCMeasurementDone
52 #endif
53 
54 //*****************************************************************************
55 //
57 //
58 //*****************************************************************************
59 void
60 AUXTDCConfigSet(uint32_t ui32Base, uint32_t ui32StartCondition,
61  uint32_t ui32StopCondition)
62 {
63  //
64  // Check the arguments.
65  //
66  ASSERT(AUXTDCBaseValid(ui32Base));
67 
68  //
69  // Make sure the AUX TDC is in the idle state before changing the
70  // configuration.
71  //
72  while(!((HWREG(ui32Base + AUX_TDC_O_STAT) & AUX_TDC_STAT_STATE_M) ==
74  {
75  }
76 
77  //
78  // Clear previous results.
79  //
80  HWREG(ui32Base + AUX_TDC_O_CTL) = 0x0;
81 
82  //
83  // Change the configuration.
84  //
85  HWREG(ui32Base + AUX_TDC_O_TRIGSRC) = ui32StartCondition | ui32StopCondition;
86 }
87 
88 //*****************************************************************************
89 //
91 //
92 //*****************************************************************************
93 uint32_t
94 AUXTDCMeasurementDone(uint32_t ui32Base)
95 {
96  uint32_t ui32Reg;
97  uint32_t ui32Status;
98 
99  //
100  // Check the arguments.
101  //
102  ASSERT(AUXTDCBaseValid(ui32Base));
103 
104  //
105  // Check if the AUX TDC is done measuring.
106  //
107  ui32Reg = HWREG(ui32Base + AUX_TDC_O_STAT);
108  if(ui32Reg & AUX_TDC_STAT_DONE)
109  {
110  ui32Status = AUX_TDC_DONE;
111  }
112  else if(ui32Reg & AUX_TDC_STAT_SAT)
113  {
114  ui32Status = AUX_TDC_TIMEOUT;
115  }
116  else
117  {
118  ui32Status = AUX_TDC_BUSY;
119  }
120 
121  //
122  // Return the status.
123  //
124  return (ui32Status);
125 }
#define AUX_TDC_BUSY
Definition: aux_tdc.h:93
#define AUX_TDC_TIMEOUT
Definition: aux_tdc.h:94
void AUXTDCConfigSet(uint32_t ui32Base, uint32_t ui32StartCondition, uint32_t ui32StopCondition)
Configure the operation of the AUX TDC.
Definition: aux_tdc.c:60
#define ASSERT(expr)
Definition: debug.h:74
#define AUX_TDC_DONE
Definition: aux_tdc.h:95
uint32_t AUXTDCMeasurementDone(uint32_t ui32Base)
Check if the AUX TDC is done measuring.
Definition: aux_tdc.c:94