module ti.sysbios.family.arm.a15.Mmu

Memory Management Unit Manager

This module allows the ARM processor to map a 32-bit virtual address to a 40-bit physical address (supports Large physical address extensions) and enable/disable the MMU. It does this through translation tables in memory. The MMU hardware supports upto 3-levels of translation tables. This module only supports the first 2 levels of translation tables. The level1 translation table is a 32B descriptor table comprising of four 64bit entries. There can be upto 4 level2 translation tables, each 4KB in size and comprising of 512 64bit entries. [ more ... ]
C synopsis target-domain sourced in ti/sysbios/family/arm/a15/Mmu.xdc
#include <ti/sysbios/family/arm/a15/Mmu.h>
Functions
Void 
Void 
Void 
Bool 
Void 
Void 
Void 
Void 
Void 
Functions common to all target modules
Defines
#define
#define
Typedefs
typedef struct
typedef enum
Constants
extern const Assert_Id 
extern const Assert_Id 
extern const Assert_Id 
extern const Mmu_DescriptorAttrs 
extern const Bool 
extern const Bool 
 
DETAILS
This module allows the ARM processor to map a 32-bit virtual address to a 40-bit physical address (supports Large physical address extensions) and enable/disable the MMU. It does this through translation tables in memory. The MMU hardware supports upto 3-levels of translation tables. This module only supports the first 2 levels of translation tables. The level1 translation table is a 32B descriptor table comprising of four 64bit entries. There can be upto 4 level2 translation tables, each 4KB in size and comprising of 512 64bit entries.
Each entry in the level1 table either gives the base address and defines the attributes of a memory area of size 1GB or gives the address of the next level of translation table and some attributes for that translation.
Each entry in the level2 table either gives the base address and defines the attributes of a memory area of size 2MB or gives the address of the next level of translation table and some attributes for that translation.
By default, the MMU level1 and level2 translation tables are initialized with cache-enabled entries for every memory-segment defined in the platform (see cachePlatformMemory). Cache-disabled entries are also added for the peripheral addresses used by SYS/BIOS (i.e. Timers, Interrupt controller).
The level1 translation table is placed in an output section called "ti.sysbios.family.arm.a15.mmuFirstLevelTableSection". Each of the level2 translation tables are placed in output sections called "ti.sysbios.family.arm.a15.mmuSecondLevelTableSection0", "ti.sysbios.family.arm.a15.mmuSecondLevelTableSection1", "ti.sysbios.family.arm.a15.mmuSecondLevelTableSection2", and "ti.sysbios.family.arm.a15.mmuSecondLevelTableSection3". These sections are placed into the platform's default dataMemory and in order to minimize object file size, specified to not be initialized via the "NOLOAD" type on GNU compilers and "NOINIT" on TI compilers.
This module does not manage the third level descriptor tables.
The following is an example of how to place the MMU table and how to enable L1/L2 data caching for the address range 0x80000000-0x90000000 in the *.cfg file:
    var Mmu = xdc.useModule('ti.sysbios.family.arm.a15.Mmu');

    // descriptor attribute structure
    var attrs = new Mmu.DescriptorAttrs();

    // Note: If running in SMP mode, all page table entries for memory
    //       shared between the SMP cores should mark the memory as
    //       inner-shareable. This is to ensure that the cached copy of
    //       the memory region is kept coherent accross cores.

    Mmu.initDescAttrsMeta(attrs);
    attrs.type = Mmu.DescriptorType_BLOCK;    // BLOCK descriptor
    attrs.shareable = 3;                      // inner-sharerable
    attrs.attrIndx = 2;                       // MAIR0 Byte2 describes
                                              // memory attributes for
                                              // this level2 entry

    // write memory region attribute in mairRegAttr[2] i.e. MAIR0 Reg Byte2
    Mmu.setMAIRMeta(2, 0xFF);              // Mark mem regions as cacheable

    // Set the descriptor for each entry in the address range
    for (var i=0x80000000; i < 0x90000000; i = i + 0x00200000) {
        // Each 'BLOCK' descriptor entry spans a 2MB address range
        Mmu.setSecondLevelDescMeta(i, i, attrs);
    }

    var memmap = Program.cpu.memoryMap;
    var DDR = null;

    // Find DDR in memory map
    for (var i=0; i < memmap.length; i++) {
        if (memmap[i].name == "DDR") {
            DDR = memmap[i];
        }
    }

    // Place the MMU table in the DDR memory segment if it exists
    if (DDR != null) {
        var sectionName =
                  "ti.sysbios.family.arm.a15.mmuSecondLevelTableSection2";
        Program.sectMap[sectionName] = new Program.SectionSpec();
        Program.sectMap[sectionName].type = "NOLOAD";
        Program.sectMap[sectionName].loadSegment = "DDR";
    }
    else {
        print("No DDR memory segment was found");
    }

The following example demonstrates how to add a peripheral's address to the MMU table so that it can be accessed by code at runtime:
    var Cache = xdc.useModule('ti.sysbios.family.arm.a15.Cache');
    var Mmu = xdc.useModule('ti.sysbios.family.arm.a15.Mmu');

    // Enable the cache
    Cache.enableCache = true;

    // Enable the MMU (Required for L1/L2 data caching)
    Mmu.enableMMU = true;

    // descriptor attribute structure
    var peripheralAttrs = new Mmu.DescriptorAttrs();

    Mmu.initDescAttrsMeta(peripheralAttrs);

    peripheralAttrs.type = Mmu.DescriptorType_BLOCK;  // BLOCK descriptor
    peripheralAttrs.noExecute = true;                 // not executable
    peripheralAttrs.accPerm = 0;                      // read/write at PL1
    peripheralAttrs.attrIndx = 1;                     // MAIR0 Byte1 describes
                                                      // memory attributes for
                                                      // each BLOCK MMU entry

    // write memory region attribute in mairRegAttr[1] i.e. MAIR0 Reg Byte1
    Mmu.setMAIRMeta(1, 0x0);    // Mark mem regions as strongly ordered memory

    // Define the base address of the 2 MB page
    // the peripheral resides in.
    var peripheralBaseAddr = 0xa0400000;

    // Configure the corresponding MMU page descriptor accordingly
    Mmu.setSecondLevelDescMeta(peripheralBaseAddr,
                               peripheralBaseAddr,
                               peripheralAttrs);
The following example demonstrates how to modify the first level MMU entry at runtime. This example changes the descriptor type of the first level table entry from Table (default) to Block (maps memory region of size 1GB).
  ...

  Void main(Int argc, Char * argv[])
  {
      Mmu_DescriptorAttrs attrs;
      Mmu_initDescAttrs(&attrs);

     // Note: If running in SMP mode, all page table entries for memory
     //       shared between the SMP cores should mark the memory as
     //       inner-shareable. This is to ensure that the cached copy of
     //       the memory region is kept coherent accross cores.

      attrs.type = Mmu_DescriptorType_BLOCK;
      attrs.shareable = 3;            // inner-shareable
      attrs.accPerm = 1;              // read/write at any privelege level
      attrs.attrIndx = 3;             // Use MAIR0 Register Byte 3 for
                                      // determining the memory attributes
                                      // for each MMU entry

      // Note: If running in SMP mode, Mmu_setMAIR() and
      //       Mmu_setFirstLevelDesc() should not be called with Hwi, Swi
      //       or Tasking disabled.

      // attrIndx[2] = 0b0 selects MAIR0
      // attrIndx[1:0] = 0b11 selects Byte 3 in MAIR0
      //
      // A value of 0x4F is written to Byte 3 of MAIR0. This marks the memory
      // as Normal Memory that is outer non-cacheable and inner write-back
      // cacheable for both reads and writes.

      Mmu_setMAIR(3, 0x4F);

      // Update the first level table's MMU entry for 0x80000000 with the
      // new attributes.
      Mmu_setFirstLevelDesc((Ptr)0x80000000, (UInt64)0x80000000, &attrs);
  }

The following example demonstrates how to modify the memory attributes for a second level MMU entry at runtime.
  ...

  Void main(Int argc, Char * argv[])
  {
      Mmu_DescriptorAttrs attrs;
      Mmu_initDescAttrs(&attrs);

      attrs.type = Mmu_DescriptorType_BLOCK;
      attrs.shareable = 0;            // non-shareable
      attrs.accPerm = 1;              // read/write at any privelege level
      attrs.attrIndx = 4;             // Use MAIR1 Register Byte 0 for
                                      // determining the memory attributes
                                      // for each MMU entry

      // Note: If running in SMP mode, Mmu_setMAIR() and
      //       Mmu_setSecondLevelDesc() should not be called with Hwi, Swi
      //       or Tasking disabled.

      // attrIndx[2] = 0b1 selects MAIR1
      // attrIndx[1:0] = 0b00 selects Byte 0 in MAIR1
      //
      // A value of 0x4F is written to Byte 0 of MAIR1. This marks the memory
      // as Normal Memory that is outer non-cacheable and inner write-back
      // cacheable for both reads and writes.

      Mmu_setMAIR(4, 0x4F);

      // Update the MMU entry for 0x80000000 with the new attributes.
      Mmu_setSecondLevelDesc((Ptr)0x80000000, (UInt64)0x80000000, &attrs);
  }

The following example demonstrates how to use setFirstLevelDesc() to create a mapping from the first level descriptor table to the second level descriptor table for an unmapped first level entry.
  ...

  Void main(Int argc, Char * argv[])
  {
      UInt32 peripheralBaseAddr;
      Mmu_DescriptorAttrs attrs;
      Mmu_initDescAttrs(&attrs);

      attrs.type = Mmu_DescriptorType_TABLE;

      // Note: If running in SMP mode, Mmu_setMAIR(), Mmu_setFirstLevelDesc()
      //       and Mmu_setSecondLevelDesc() should not be called with Hwi, Swi
      //       or Tasking disabled.

      // This example assumes that the first level descriptor table does
      // not have a valid entry for virtual address 0x40000000-0x7FFFFFFF.
      // The below call will map this virtual address range in the first
      // level table to the correponding second level descriptor table.
      Mmu_setFirstLevelDesc((Ptr)0x40000000, (UInt64)0x0, &attrs);

      // Note: Second argument to Mmu_setFirstLevelDesc() is ignored
      //       when attrs.type is DescriptorType_TABLE.


      attrs.type = Mmu.DescriptorType_BLOCK;  // BLOCK descriptor
      attrs.noExecute = true;                 // not executable
      attrs.accPerm = 0;                      // read/write at PL1
      attrs.attrIndx = 1;                     // MAIR0 Byte1 describes
                                              // memory attributes for
                                              // each BLOCK MMU entry

      // write memory region attribute in mairRegAttr[1] i.e. MAIR0 Reg Byte1
      Mmu_setMAIRMeta(1, 0x0); // Mark mem regions as strongly ordered memory

      // Define the base address of the 2 MB page
      // the peripheral resides in.
      peripheralBaseAddr = 0x40400000;

      // Now that there is a first level entry for virtual addresses
      // 0x40000000-0x7FFFFFFF that maps these addresses to a second
      // level descriptor table, we can add a second level entry that
      // maps the peripheral base address to a physical address.
      Mmu_setSecondLevelDesc(peripheralBaseAddr, peripheralBaseAddr, &attrs);
  }

Notes:
 
const Mmu_NUM_LEVEL1_ENTRIES
C synopsis target-domain
#define Mmu_NUM_LEVEL1_ENTRIES (UInt)4
 
 
const Mmu_NUM_LEVEL2_ENTRIES
C synopsis target-domain
#define Mmu_NUM_LEVEL2_ENTRIES (UInt)512
 
 
enum Mmu_DescriptorType

Different descriptor type encodings:

C synopsis target-domain
typedef enum Mmu_DescriptorType {
    Mmu_DescriptorType_INVALID0,
    // Virtual address is unmapped
    Mmu_DescriptorType_BLOCK,
    // Block descriptor
    Mmu_DescriptorType_INVALID1,
    // Virtual address is unmapped
    Mmu_DescriptorType_TABLE
    // Next-level table address
} Mmu_DescriptorType;
 
DETAILS
  • Invalid or Fault entry (0b00 or 0b10)
  • Block descriptor entry (0b01)
  • Table descriptor entry (0b11)
If a First-level table contains only one entry, it would be skipped, and the TTBR points to the Second-level table. This happens if the VA address range is 30 bits or less.
 
struct Mmu_DescriptorAttrs

Structure for setting first and second level descriptor entries

C synopsis target-domain
typedef struct Mmu_DescriptorAttrs {
    Mmu_DescriptorType type;
    // first level descriptor type
    Bool nsTable;
    // security level for subsequent levels
    UInt8 apTable;
    // access perm limit for subsequent levels
    Bool xnTable;
    // XN limit for subsequent levels
    Bool pxnTable;
    // PXN limit for subsequent levels
    Bool noExecute;
    // execute-never bit
    Bool privNoExecute;
    // privileged execute-never bit
    Bool contiguous;
    // hint bit indicating 16 adjacent table entries point to contiguos memory
    Bool notGlobal;
    // not global bit
    Bool accessFlag;
    // access flag
    UInt8 shareable;
    // shareability field value 0-3
    UInt8 accPerm;
    // access permission bits value 0-3
    Bool nonSecure;
    // non-secure bit
    UInt8 attrIndx;
    // stage 1 memory attributes index field for the indicated MAIRn register value 0-7
    UInt8 reserved;
    // Bits[58:55] reserved for software use
} Mmu_DescriptorAttrs;
 
DETAILS
nsTable, apTable, xnTable and pxnTable fields are used only for DescriptorType.TABLE
noExecute, privNoExecute, contiguous, notGlobal, accessFlag, shareable, accPerm, nonSecure and attrIndx fields are used only for DescriptorType.BLOCK
 
config Mmu_A_disableUnsupported  // module-wide

Assert raised if Mmu_disable() called when running in SMP mode

C synopsis target-domain
extern const Assert_Id Mmu_A_disableUnsupported;
 
 
config Mmu_A_nullPointer  // module-wide

Assert raised when a pointer is null

C synopsis target-domain
extern const Assert_Id Mmu_A_nullPointer;
 
 
config Mmu_A_unknownDescType  // module-wide

Assert raised when the descriptor type is not recognized

C synopsis target-domain
extern const Assert_Id Mmu_A_unknownDescType;
 
 
config Mmu_defaultAttrs  // module-wide

default descriptor attributes structure

C synopsis target-domain
extern const Mmu_DescriptorAttrs Mmu_defaultAttrs;
 
 
config Mmu_enableMMU  // module-wide

Configuration parameter to enable MMU

C synopsis target-domain
extern const Bool Mmu_enableMMU;
 
 
config Mmu_errata798181  // module-wide

Enable workaround for ARM errata 798181

C synopsis target-domain
extern const Bool Mmu_errata798181;
 
DETAILS
Errata 798181 brief description: Moving a virtual page that is being accessed by an active process can lead to unexpected behavior.
 
Mmu_disable()  // module-wide

Disables the MMU

C synopsis target-domain
Void Mmu_disable();
 
DETAILS
If the MMU is already disabled, then simply return. Otherwise this function does the following:
  • If the L1 data cache is enabled, write back invalidate all of L1 data cache.
  • If the L1 program cache is enabled, invalidate all of L1 program cache.
This function is not supported when running in SMP mode and will generate an assertion failure if called.
On ARM cores like Cortex-A15, both the cache and MMU need to be enabled for data caching to work. Also, on certain SoC's like Keystone 2, the caches need to be enabled for the inter-core lock (used in SMP mode) to work. Therefore, disabling the MMU is not permitted when running in SMP mode.
NOTE
This function does not change the cache L1 data/program settings.
 
Mmu_enable()  // module-wide

Enables the MMU

C synopsis target-domain
Void Mmu_enable();
 
DETAILS
If the MMU is already enabled, then simply return. Otherwise this function does the following:
  • If the L1 program cache is enabled, invalidate all of L1 program cache.
This function enables the MMU on the core it is called from.
NOTE
This function does not change the L1 data/program cache settings.
 
Mmu_initDescAttrs()  // module-wide

Initializes the descriptor attribute structure

C synopsis target-domain
Void Mmu_initDescAttrs(Mmu_DescriptorAttrs *descAttrs);
 
ARGUMENTS
attrs — Pointer to descriptor attribute struct
 
Mmu_isEnabled()  // module-wide

Determines if the MMU is enabled

C synopsis target-domain
Bool Mmu_isEnabled();
 
 
Mmu_setFirstLevelDesc()  // module-wide

Sets the descriptor for the virtual address

C synopsis target-domain
Void Mmu_setFirstLevelDesc(Ptr virtualAddr, UInt64 phyAddr, Mmu_DescriptorAttrs *attrs);
 
ARGUMENTS
virtualAddr — The modified virtual address
phyAddr — The physical address
attrs — Pointer to first level descriptor attribute struct
DETAILS
The first level table entry for the virtual address is mapped to either a physical address with the attributes specified or maps to a second level descriptor table. The descriptor table is effective when the MMU is enabled.
If attrs.type is set to DescriptorType_TABLE then the physical address which is passed as the second argument to setFirstLevelDesc() is ignored and the virtual address (aligned to 1GB) is mapped to the corresponding second level descriptor table.
SEE
NOTE
If running in SMP mode, this function broadcasts to the other cores to ensure all cores execute a barrier instruction and the MMU table updates are visible to them. Therefore, this function should not be called with Hwi, Swi or Tasking disabled as that would cause the inter-core lock to be taken by the current core and will prevent the function from broadcasting to the other cores. If not running in SMP mode, it is okay to call this function with Hwi, Swi or Tasking disabled.
 
Mmu_setMAIR()  // module-wide

Sets the memory attribute encoding in the MAIRn register

C synopsis target-domain
Void Mmu_setMAIR(UInt attrIndx, UInt attr);
 
ARGUMENTS
attrIndx — Select appropriate MAIR register (0 or 1) and byte offset within the selected register
attr — Memory attribute encoding
DETAILS
MAIR0 and MAIR1 provide the memory attribute encodings to the possible attrIndx values in a long-descriptor format translation table entry for stage 1 translations.
attrIndx[1:0] selects the ATTRn bit-field in the selected MAIR register.
attrIndx[2] selects the MAIR register.
Memory Attribute Indirection Register (MAIR) 0 and 1 bit assignments:
        |31     |    24|23     |     16|15     |      8|7      |      0|
         --------------------------------------------------------------
  MAIR0 |     ATTR3    |     ATTR2     |     ATTR1     |     ATTR0     |
         --------------------------------------------------------------
  MAIR1 |     ATTR7    |     ATTR6     |     ATTR5     |     ATTR4     |
         --------------------------------------------------------------
SYS/BIOS assigns the following defaults to MAIR0 ATTR0, ATTR1 and ATTR2:
  ATTR0 -> 0x44 (mark memory region as non-cacheable normal memory)
  ATTR1 -> 0x00 (mark memory region as strongly ordered and non-cacheable)
  ATTR2 -> 0xFF (mark memory region as normal memory, RW cacheable and
  RW allocate)
The level1 and level2 MMU Table entries use the above default attributes created by this module and should preferably not be changed. Please note that if the default value assigned to ATTR0 is changed, then the cachePlatformMemory config param may not behave correctly as it uses this attribute to mark the memory as non-cacheable normal memory. If ATTR1 or ATTR2 are changed, it will affect all existing MMU Table entries which use ATTR1 or ATTR2.
For more details on MAIR0 and MAIR1 encodings please refer v7A ARM Architecture Reference Manual
NOTE
This function only invalidates the TLB and does not flush the cache. If the cacheability attribute of a region of memory is changed by modifying the MAIR entry for the region, the application needs to flush and invalidate the region of memory from the cache.
If running in SMP mode, this function broadcasts to the other cores and ensures the MAIR entry is updated on all cores. Therefore, this function should not be called with Hwi, Swi or Tasking disabled as that would cause the inter-core lock to be taken by the current core and will prevent the function from broadcasting a MAIR update request to the other cores. If not running in SMP mode, it is okay to call this function with Hwi, Swi or Tasking disabled.
 
Mmu_setSecondLevelDesc()  // module-wide

Sets the descriptor for the virtual address

C synopsis target-domain
Void Mmu_setSecondLevelDesc(Ptr virtualAddr, UInt64 phyAddr, Mmu_DescriptorAttrs *attrs);
 
ARGUMENTS
virtualAddr — The modified virtual address
phyAddr — The physical address
attrs — Pointer to second level descriptor attribute struct
DETAILS
The second level table entry for the virtual address is mapped to the physical address with the attributes specified. The descriptor table is effective when the MMU is enabled.
SEE
NOTE
If running in SMP mode, this function broadcasts to the other cores to ensure all cores execute a barrier instruction and the MMU table updates are visible to them. Therefore, this function should not be called with Hwi, Swi or Tasking disabled as that would cause the inter-core lock to be taken by the current core and will prevent the function from broadcasting to the other cores. If not running in SMP mode, it is okay to call this function with Hwi, Swi or Tasking disabled.
 
Mmu_tlbInv()  // module-wide

Invalidate the TLB entries (both data and instruction) for the range of memory within the specified starting address and byte count. The range of addresses operated on gets quantized to page size

C synopsis target-domain
Void Mmu_tlbInv(Ptr startAddr, SizeT byteCnt);
 
 
Mmu_tlbInvAll()  // module-wide

Invalidate entire TLB (both data and instruction)

C synopsis target-domain
Void Mmu_tlbInvAll();
 
Module-Wide Built-Ins

C synopsis target-domain
Types_ModuleId Mmu_Module_id();
// Get this module's unique id
 
Bool Mmu_Module_startupDone();
// Test if this module has completed startup
 
IHeap_Handle Mmu_Module_heap();
// The heap from which this module allocates memory
 
Bool Mmu_Module_hasMask();
// Test whether this module has a diagnostics mask
 
Bits16 Mmu_Module_getMask();
// Returns the diagnostics mask for this module
 
Void Mmu_Module_setMask(Bits16 mask);
// Set the diagnostics mask for this module
 
Configuration settings sourced in ti/sysbios/family/arm/a15/Mmu.xdc
var Mmu = xdc.useModule('ti.sysbios.family.arm.a15.Mmu');
module-wide constants & types
    const Mmu.NUM_LEVEL1_ENTRIES//  = 4;
    const Mmu.NUM_LEVEL2_ENTRIES//  = 512;
 
 
        obj.nsTable// security level for subsequent levels = Bool  ...
        obj.apTable// access perm limit for subsequent levels = UInt8  ...
        obj.xnTable// XN limit for subsequent levels = Bool  ...
        obj.pxnTable// PXN limit for subsequent levels = Bool  ...
        obj.noExecute// execute-never bit = Bool  ...
        obj.privNoExecute// privileged execute-never bit = Bool  ...
        obj.notGlobal// not global bit = Bool  ...
        obj.accessFlag// access flag = Bool  ...
        obj.shareable// shareability field value 0-3 = UInt8  ...
        obj.accPerm// access permission bits value 0-3 = UInt8  ...
        obj.nonSecure// non-secure bit = Bool  ...
        obj.reserved// Bits[58:55] reserved for software use = UInt8  ...
module-wide config parameters
        msg: "A_disableUnsupported: MMU disable is not supported in SMP mode."
    };
        msg: "A_nullPointer: Pointer is null"
    };
        msg: "A_unknownDescType: Descriptor type is not recognized"
    };
        type: Mmu.DescriptorType_TABLE,
        nsTable: false,
        apTable: 0,
        xnTable: false,
        pxnTable: false,
        noExecute: false,
        privNoExecute: false,
        contiguous: false,
        notGlobal: false,
        accessFlag: true,
        shareable: 0,
        accPerm: 0,
        nonSecure: false,
        attrIndx: 0,
        reserved: 0
    };
 
module-wide functions
 
 
const Mmu.NUM_LEVEL1_ENTRIES
Configuration settings
const Mmu.NUM_LEVEL1_ENTRIES = 4;
 
C SYNOPSIS
 
const Mmu.NUM_LEVEL2_ENTRIES
Configuration settings
const Mmu.NUM_LEVEL2_ENTRIES = 512;
 
C SYNOPSIS
 
enum Mmu.DescriptorType

Different descriptor type encodings:

Configuration settings
values of type Mmu.DescriptorType
    const Mmu.DescriptorType_INVALID0;
    // Virtual address is unmapped
    const Mmu.DescriptorType_BLOCK;
    // Block descriptor
    const Mmu.DescriptorType_INVALID1;
    // Virtual address is unmapped
    const Mmu.DescriptorType_TABLE;
    // Next-level table address
 
DETAILS
  • Invalid or Fault entry (0b00 or 0b10)
  • Block descriptor entry (0b01)
  • Table descriptor entry (0b11)
If a First-level table contains only one entry, it would be skipped, and the TTBR points to the Second-level table. This happens if the VA address range is 30 bits or less.
C SYNOPSIS
 
struct Mmu.DescriptorAttrs

Structure for setting first and second level descriptor entries

Configuration settings
var obj = new Mmu.DescriptorAttrs;
 
    obj.type = Mmu.DescriptorType  ...
    // first level descriptor type
    obj.nsTable = Bool  ...
    // security level for subsequent levels
    obj.apTable = UInt8  ...
    // access perm limit for subsequent levels
    obj.xnTable = Bool  ...
    // XN limit for subsequent levels
    obj.pxnTable = Bool  ...
    // PXN limit for subsequent levels
    obj.noExecute = Bool  ...
    // execute-never bit
    obj.privNoExecute = Bool  ...
    // privileged execute-never bit
    obj.contiguous = Bool  ...
    // hint bit indicating 16 adjacent table entries point to contiguos memory
    obj.notGlobal = Bool  ...
    // not global bit
    obj.accessFlag = Bool  ...
    // access flag
    obj.shareable = UInt8  ...
    // shareability field value 0-3
    obj.accPerm = UInt8  ...
    // access permission bits value 0-3
    obj.nonSecure = Bool  ...
    // non-secure bit
    obj.attrIndx = UInt8  ...
    // stage 1 memory attributes index field for the indicated MAIRn register value 0-7
    obj.reserved = UInt8  ...
    // Bits[58:55] reserved for software use
 
DETAILS
nsTable, apTable, xnTable and pxnTable fields are used only for DescriptorType.TABLE
noExecute, privNoExecute, contiguous, notGlobal, accessFlag, shareable, accPerm, nonSecure and attrIndx fields are used only for DescriptorType.BLOCK
C SYNOPSIS
 
config Mmu.A_disableUnsupported  // module-wide

Assert raised if Mmu_disable() called when running in SMP mode

Configuration settings
Mmu.A_disableUnsupported = Assert.Desc {
    msg: "A_disableUnsupported: MMU disable is not supported in SMP mode."
};
 
C SYNOPSIS
 
config Mmu.A_nullPointer  // module-wide

Assert raised when a pointer is null

Configuration settings
Mmu.A_nullPointer = Assert.Desc {
    msg: "A_nullPointer: Pointer is null"
};
 
C SYNOPSIS
 
config Mmu.A_unknownDescType  // module-wide

Assert raised when the descriptor type is not recognized

Configuration settings
Mmu.A_unknownDescType = Assert.Desc {
    msg: "A_unknownDescType: Descriptor type is not recognized"
};
 
C SYNOPSIS
 
config Mmu.defaultAttrs  // module-wide

default descriptor attributes structure

Configuration settings
Mmu.defaultAttrs = Mmu.DescriptorAttrs {
    type: Mmu.DescriptorType_TABLE,
    nsTable: false,
    apTable: 0,
    xnTable: false,
    pxnTable: false,
    noExecute: false,
    privNoExecute: false,
    contiguous: false,
    notGlobal: false,
    accessFlag: true,
    shareable: 0,
    accPerm: 0,
    nonSecure: false,
    attrIndx: 0,
    reserved: 0
};
 
C SYNOPSIS
 
config Mmu.enableMMU  // module-wide

Configuration parameter to enable MMU

Configuration settings
Mmu.enableMMU = Bool true;
 
C SYNOPSIS
 
config Mmu.errata798181  // module-wide

Enable workaround for ARM errata 798181

Configuration settings
Mmu.errata798181 = Bool true;
 
DETAILS
Errata 798181 brief description: Moving a virtual page that is being accessed by an active process can lead to unexpected behavior.
C SYNOPSIS
 
metaonly config Mmu.cachePlatformMemory  // module-wide

Flag to automatically mark platform's code/data/stack memory as cacheable in MMU descriptor table

Configuration settings
Mmu.cachePlatformMemory = Bool true;
 
DETAILS
By default, all memory regions defined in the platform an application is built with are marked as cacheable.
If manual configuration of memory regions is required, set this config parameter to 'false'.
SEE
 
metaonly config Mmu.common$  // module-wide

Common module configuration parameters

Configuration settings
Mmu.common$ = Types.Common$ undefined;
 
DETAILS
All modules have this configuration parameter. Its name contains the '$' character to ensure it does not conflict with configuration parameters declared by the module. This allows new configuration parameters to be added in the future without any chance of breaking existing modules.
 
metaonly config Mmu.rovViewInfo  // module-wide
Configuration settings
Mmu.rovViewInfo = ViewInfo.Instance ViewInfo.create;
 
 
metaonly Mmu.initDescAttrsMeta()  // module-wide

Initializes the descriptor attribute structure

Configuration settings
Mmu.initDescAttrsMeta(Mmu.DescriptorAttrs* descAttrs) returns Void
 
ARGUMENTS
attrs — Pointer to descriptor attribute struct
 
metaonly Mmu.setFirstLevelDescMeta()  // module-wide

Statically sets the descriptor for the virtual address

Configuration settings
Mmu.setFirstLevelDescMeta(Ptr virtualAddr, UInt64 phyAddr, Mmu.DescriptorAttrs attrs) returns Void
 
ARGUMENTS
virtualAddr — The modified virtual address
phyAddr — The physical address
attrs — Pointer to first level descriptor attribute struct
DETAILS
The first level table entry for the virtual address is mapped to either a physical address with the attributes specified or maps to a second level descriptor table. The descriptor table is effective when the MMU is enabled.
If attrs.type is set to Mmu.DescriptorType_TABLE then the physical address which is passed as the second argument to setFirstLevelDescMeta() is ignored and the virtual address (aligned to 1GB) is mapped to the corresponding second level descriptor table.
SEE
 
metaonly Mmu.setMAIRMeta()  // module-wide

Statically sets the memory attribute encoding in the MAIRn register

Configuration settings
Mmu.setMAIRMeta(UInt attrIndx, UInt attr) returns Void
 
ARGUMENTS
attrIndx — Select appropriate MAIR register (0 or 1) and byte offset within selected register
attr — Memory attribute encoding
DETAILS
MAIR0 and MAIR1 provide the memory attribute encodings to the possible attrIndx values in a Long-descriptor format translation table entry for stage 1 translations (see setMAIR for more details).
 
metaonly Mmu.setSecondLevelDescMeta()  // module-wide

Statically sets the descriptor for the virtual address

Configuration settings
Mmu.setSecondLevelDescMeta(Ptr virtualAddr, UInt64 phyAddr, Mmu.DescriptorAttrs attrs) returns Void
 
ARGUMENTS
virtualAddr — The modified virtual address
phyAddr — The physical address
attrs — Pointer to second level descriptor attribute struct
DETAILS
The second level table entry for the virtual address is mapped to the physical address with the attributes specified. The descriptor table is effective when the MMU is enabled.
SEE
generated on Tue, 06 Sep 2016 21:52:36 GMT