The Cortex M3's Nested Vectored Interrupt Controller (NVIC)
supports up to 256 interrupts/exceptions. In practice, most
devices support much fewer (ie the Stellaris family of devices
have only 80 total interrupts defined).
SYS/BIOS Interrupt IDs or interrupt numbers correspond
to an interrupt's position in the interrupt vector table.
ID 0 corresponds to vector 0 which is used by the NVIC
to hold the initial (reset) stack pointer value.
IDs 2-14 are hardwired to exceptions.
ID 15 is the SysTick timer interrupt.
ID's 16-255 are mapped to the NVIC's user interrupts 0-239
which are tied to platform specific interrupt sources.
Zero latency interrupts are distinguished from regular dispatched
interrupts at create time by their priority being greater
than Hwi.disablePriority.
The NVIC interrupt controller is designed for priority based
interrupts.
In general, the NVIC supports priority values of 0 thru 255.
For most TI MCU devices, 8 priorities are supported. A peculiarity
of ARM's NVIC is that, although the priority field is an 8 bit value,
the range of supported priority values are left-justified within this
8 bit field. Consequently, the 8 priority values are not 0 thru 7 as
one might expect, but rather:
A 16 entry boot vector table is placed at address 0x00000000 in
FLASH.
An 80 entry vector table is placed at address 0x20000000 in RAM.
The FLASH boot vector table contains the reset vector and exception
handler vectors used until the RAM based vector table is initialized.
The RAM vector table contains the 16 exception vectors as well as all
the 64 user interrupt vectors.
During system startup, the NVIC Vector Table Offset Registor is
intialized to point to this vector table after the table has been
initialized.
By default, Ducati core 0 places its runtime vector table at address
0x00000400 and core 1 places its runtime vector table at address
0x00000800.
Additionally, a boot vector table is placed at address
0x00000000 which is shared by both cores.
The boot reset vector function determines which core it is being
executed on and jumps to the reset vector contained in its corresponding
runtime vector table.
enum Hwi_MaskingOption |
|
Shorthand interrupt masking options
typedef enum Hwi_MaskingOption {
Hwi_MaskingOption_NONE,
Hwi_MaskingOption_ALL,
Hwi_MaskingOption_SELF,
Hwi_MaskingOption_BITMASK,
Hwi_MaskingOption_LOWER
} Hwi_MaskingOption;
VALUES
MaskingOption_NONE
No interrupts are disabled
MaskingOption_ALL
All interrupts are disabled
MaskingOption_SELF
Only this interrupt is disabled
MaskingOption_BITMASK
User supplies interrupt enable masks
MaskingOption_LOWER
All current and lower priority
interrupts are disabled.
Only a few targets/devices truly
support this masking option. For those
that don't, this setting is treated
the same as MaskingOption_SELF.
typedef Hwi_ExcHandlerFuncPtr |
|
Hwi exception handler function type definition
typedef Void (*Hwi_ExcHandlerFuncPtr)(UInt*,UInt);
typedef Hwi_ExceptionHookFuncPtr |
|
Exception hook function type definition
typedef Hwi_FuncPtr |
|
Hwi create function type definition
typedef Void (*Hwi_FuncPtr)(UArg);
typedef Hwi_Irp |
|
Interrupt Return Pointer
DETAILS
This is the address of the interrupted instruction.
typedef Hwi_VectorFuncPtr |
|
Hwi vector function type definition
typedef Void (*Hwi_VectorFuncPtr)(Void);
struct Hwi_CCR |
|
NVIC Configuration Control Register (CCR)
typedef struct Hwi_CCR {
Bits8 STKALIGN;
// Auto stack alignment in exception
Bits8 BFHFNMIGN;
// All faults ignore BUS Faults
Bits8 DIV_0_TRP;
// Trap on divide by zero
Bits8 UNALIGN_TRP;
// Trap on all unaligned accesses
Bits8 USERSETMPEND;
// Allow user to trigger interrupts
Bits8 NONEBASETHRDENA;
// Allow entering thread mode anytime
} Hwi_CCR;
struct Hwi_ExcContext |
|
Exception Context - Register contents at the time of an exception
typedef struct Hwi_ExcContext {
Ptr threadHandle;
Ptr threadStack;
SizeT threadStackSize;
Ptr r0;
Ptr r1;
Ptr r2;
Ptr r3;
Ptr r4;
Ptr r5;
Ptr r6;
Ptr r7;
Ptr r8;
Ptr r9;
Ptr r10;
Ptr r11;
Ptr r12;
Ptr sp;
Ptr lr;
Ptr pc;
Ptr psr;
Ptr ICSR;
Ptr MMFSR;
Ptr BFSR;
Ptr UFSR;
Ptr HFSR;
Ptr DFSR;
Ptr MMAR;
Ptr BFAR;
Ptr AFSR;
} Hwi_ExcContext;
struct Hwi_HookSet |
|
Hwi hook set type definition
typedef struct Hwi_HookSet {
Void (*registerFxn)(Int);
} Hwi_HookSet;
DETAILS
The functions that make up a hookSet have certain restrictions. They
cannot call any Hwi instance functions other than Hwi_getHookContext()
and Hwi_setHookContext(). For all practical purposes, they should treat
the Hwi_Handle passed to these functions as an opaque handle.
struct Hwi_StackInfo |
|
Structure contains Hwi stack usage info
typedef struct Hwi_StackInfo {
SizeT hwiStackPeak;
SizeT hwiStackSize;
Ptr hwiStackBase;
} Hwi_StackInfo;
DETAILS
Used by getStackInfo() and viewGetStackInfo() functions
config Hwi_A_unsupportedMaskingOption // module-wide |
|
Assert when bad maskSetting parameter provided
extern const Assert_Id Hwi_A_unsupportedMaskingOption;
config Hwi_E_NMI // module-wide |
|
Error raised when NMI exception occurs
config Hwi_E_alreadyDefined // module-wide |
|
Error raised when Hwi is already defined
extern const Error_Id Hwi_E_alreadyDefined;
config Hwi_E_busFault // module-wide |
|
Error raised when bus fault exception occurs
config Hwi_E_debugMon // module-wide |
|
Error raised when debugMon exception occurs
config Hwi_E_exception // module-wide |
|
Error raised when an exception occurs
config Hwi_E_hardFault // module-wide |
|
Error raised when hard fault exception occurs
config Hwi_E_hwiLimitExceeded // module-wide |
|
Error raised when the number of interrupts being created
exceeds the number supported
extern const Error_Id Hwi_E_hwiLimitExceeded;
config Hwi_E_memFault // module-wide |
|
Error raised when memory fault exception occurs
config Hwi_E_noIsr // module-wide |
|
Error raised when an uninitialized interrupt occurs
config Hwi_E_reserved // module-wide |
|
Error raised when reserved exception occurs
config Hwi_E_svCall // module-wide |
|
Error raised when svCall exception occurs
config Hwi_E_usageFault // module-wide |
|
Error raised when usage fault exception occurs
config Hwi_LD_end // module-wide |
|
Issued just after return from Hwi function (with interrupts disabled)
config Hwi_LM_begin // module-wide |
|
Issued just prior to Hwi function invocation (with interrupts disabled)
config Hwi_NUM_INTERRUPTS // module-wide |
|
The Cortex M3 NVIC supports up to 256 interrupts/exceptions
extern const Int Hwi_NUM_INTERRUPTS;
DETAILS
The actual number supported is device specific and provided by
the catalog device specification.
config Hwi_NUM_PRIORITIES // module-wide |
|
The Cortex M3 NVIC supports up to 256 interrupt priorities
extern const Int Hwi_NUM_PRIORITIES;
DETAILS
The actual number supported is device specific and provided by
the catalog device specification.
config Hwi_disablePriority // module-wide |
|
The priority that BASEPRI is set to by Hwi_disable()
extern const UInt Hwi_disablePriority;
DETAILS
All interrupts configured with equal or less priority (equal or
higher number) than disablePriority are disabled by
Hwi_disable.
Interrupts configured with higher priority (smaller number) than
Hwi.disablePriority are non-maskable (ie zero-latency).
The default setting is the second highest interrupt priority
defined for the device (typically '0x20' for devices
which support 8 priority values).
This results in priority 0 (and all
other values in the same priority group, ie 0x00 thru 0x1f)
being the zero-latency, non-maskable interrupt priority.
All other priorities are disabled with Hwi_disable().
config Hwi_dispatcherAutoNestingSupport // module-wide |
|
Include interrupt nesting logic in interrupt dispatcher?
extern const Bool Hwi_dispatcherAutoNestingSupport;
DETAILS
Default is true.
This option provides the user with the ability to optimize
interrupt dispatcher performance when support for interrupt
nesting is not required.
Setting this parameter to false will disable the logic in
the interrupt dispatcher that manipulates interrupt mask
registers and enables and disables interrupts before and
after invoking the user's Hwi function.
Set this parameter to false if you don't need interrupts
enabled during the execution of your Hwi functions.
config Hwi_dispatcherIrpTrackingSupport // module-wide |
|
Controls whether the
dispatcher retains the interrupted thread's return address
extern const Bool Hwi_dispatcherIrpTrackingSupport;
DETAILS
This option is enabled by default.
Setting this parameter to false will disable the logic in
the interrupt dispatcher that keeps track of the interrupt's
return address and provide a small savings in interrupt latency.
The application can get an interrupt's most recent return
address using the
getIrp API.
config Hwi_dispatcherSwiSupport // module-wide |
|
Include Swi scheduling logic in interrupt dispatcher?
extern const Bool Hwi_dispatcherSwiSupport;
DETAILS
Default is inherited from
BIOS.swiEnabled, which is true by default.
This option provides the user with the ability to optimize
interrupt dispatcher performance when it is known that Swis
will not be posted from any of their Hwi threads.
WARNING
Setting this parameter to false will disable the logic in
the interrupt dispatcher that invokes the Swi scheduler
prior to returning from an interrupt.
With this setting, Swis MUST NOT be posted from Hwi functions!
config Hwi_dispatcherTaskSupport // module-wide |
|
Include Task scheduling logic in interrupt dispatcher?
extern const Bool Hwi_dispatcherTaskSupport;
DETAILS
Default is inherited from
BIOS.taskEnabled, which is true by default.
This option provides the user with the ability to optimize
interrupt dispatcher performance when it is known that no
Task scheduling APIs (ie
Semaphore_post()) will be executed from any of their Hwi threads.
Setting this parameter to false will disable the logic in
the interrupt dispatcher that invokes the Task scheduler
prior to returning from an interrupt.
config Hwi_excHandlerFunc // module-wide |
|
Exception handler function pointer
DETAILS
The default is determined by the value of Hwi.enableException.
If the user does NOT set this parameter, then the following default
behavior is followed:
If Hwi.enableException is true, then the internal 'Hwi_excHandlerMax'
function is used. This exception handler saves the exception context
then does a complete exception decode and dump to the console, then
raises an Error. The exception context can be viewed within CCS
in the ROV Hwi module's Exception view.
If Hwi.enableException is false, then the internal 'Hwi_excHandlerMin'
function is used. This exception handler saves the exception context
then raises an Error. The exception context can be viewed within CCS
in the ROV Hwi module's Exception view.
If the user sets this parameter to their own function, then the user's
function will be invoked with the following arguments:
Void myExceptionHandler(UInt *excStack, UInt lr);
Where 'excStack' is the address of the stack containing the
register context at the time of the exception, and 'lr' is the
link register value when the low-level-assembly-coded exception
handler was vectored to.
If this parameter is set to 'null', then an infinite while loop is
entered when an exception occurs. This setting minimizes code and
data footprint but provides no automatic exception decoding.
config Hwi_excHookFunc // module-wide |
|
User Exception hook function
DETAILS
Called just after the exception context has been initialized.
This function will be run on the ISR stack.
This function must run to completion.
It is called without any Task or Swi scheduling protection
and therefore can not call any functions that may cause a Swi or Task
scheduling operation (Swi_post(), Semaphore_post(), Event_post(), etc).
config Hwi_excHookFuncs // module-wide |
|
config Hwi_nullIsrFunc // module-wide |
|
Uninitialized ISR Handler. Default is set to an internal exception handler
config Hwi_priGroup // module-wide |
|
The PRIGROUP setting. Default is 0
extern const UInt Hwi_priGroup;
DETAILS
This value will be written to the PRIGROUP field
within the NVIC's Application Interrupt and Reset Control
Register (Hwi_nvic.AIRCR). It defines how the 8 bit priority
values are interpreted by the hardware.
Valid settings are 0-7.
The default setting of 0 causes bits 7-1 of an interrupt's
priority value to be used as pre-emption priority, while bit 0
is used to determine which of two simultaneous interrupts with
the same pre-emption priority will be serviced first.
For most TI MCU devices, this means that each of the 8 supported
priority values are unique pre-emption priorities and are not
subdivided into priority groups.
extern Hwi_nvic |
|
Physical Nested Vectored Interrupt Controller Device.
Short name is "Hwi_nvic"
Long name is "ti_sysbios_family_arm_m3_Hwi_nvic"
Hwi_NVIC Hwi_nvic; // linked as extern ti_sysbios_family_arm_m3_Hwi_nvic
extern Hwi_vnvic |
|
Virtual Nested Vectored Interrupt Controller structure
written to by both cores for SMP.
Short name is "Hwi_vnvic"
Long name is "ti_sysbios_family_arm_m3_Hwi_vnvic"
Hwi_NVIC Hwi_vnvic; // linked as extern ti_sysbios_family_arm_m3_Hwi_vnvic
Hwi_clearInterrupt() // module-wide |
|
Clear a specific interrupt
Void Hwi_clearInterrupt(UInt intNum);
ARGUMENTS
intNum
interrupt number to clear
DETAILS
Clears a specific interrupt's pending status.
The implementation is family-specific.
Hwi_disable() // module-wide |
|
Disable all non zero-latency interrupts
macro UInt Hwi_disable();
RETURNS
opaque key for use by Hwi_restore()
DETAILS
Hwi_disable disables all non zero-latency hardware interrupts and
returns an
opaque key indicating whether interrupts were globally enabled or
disabled on entry to Hwi_disable().
The actual value of the key is target/device specific and is meant
to be passed to Hwi_restore().
Call Hwi_disable before a portion of a function that needs
to run without interruption. When critical processing is complete, call
Hwi_restore or Hwi_enable to reenable hardware interrupts.
Servicing of interrupts that occur while interrupts are disabled is
postponed until interrupts are reenabled. However, if the same type
of interrupt occurs several times while interrupts are disabled,
the interrupt's function is executed only once when interrupts are
reenabled.
A context switch can occur when calling Hwi_enable or Hwi_restore if
an enabled interrupt occurred while interrupts are disabled.
Hwi_disable may be called from main(). However, since Hwi interrupts
are already disabled in main(), such a call has no effect.
IMPLEMENTATION NOTE
In order to support zero latency interrupts, rather
than setting PRIMASK (which would globally disable all NVIC
interrupts), Hwi_disable() instead writes the value of
Hwi.disablePriority
to the BASEPRI register. In doing so, all interrupts of equal or
lower priority than Hwi.disablePriority are disabled.
CONSTRAINTS
If a Task switching API such as
Semaphore_pend(),
Semaphore_post(),
Task_sleep(), or
Task_yield()
is invoked which results in a context switch while
interrupts are disabled, an embedded call to
Hwi_enable occurs
on the way to the new thread context which unconditionally re-enables
interrupts. Interrupts will remain enabled until a subsequent
Hwi_disable
invocation.
Swis always run with interrupts enabled.
See
Swi_post() for a discussion Swis and
interrupts.
Hwi_disableInterrupt() // module-wide |
|
Disable a specific interrupt
UInt Hwi_disableInterrupt(UInt intNum);
ARGUMENTS
intNum
interrupt number to disable
RETURNS
key to restore previous enable/disable state
DETAILS
Disable a specific interrupt identified by an interrupt number.
Hwi_enable() // module-wide |
|
Globally enable interrupts
RETURNS
opaque key for use by Hwi_restore()
DETAILS
Hwi_enable globally enables hardware interrupts and returns an
opaque key indicating whether interrupts were globally enabled or
disabled on entry to Hwi_enable().
The actual value of the key is target/device specific and is meant
to be passed to Hwi_restore().
This function is
called as part of SYS/BIOS Startup_POST_APP_MAIN phase.
Hardware interrupts are enabled unless a call to Hwi_disable disables
them.
Servicing of interrupts that occur while interrupts are disabled is
postponed until interrupts are reenabled. However, if the same type
of interrupt occurs several times while interrupts are disabled,
the interrupt's function is executed only once when interrupts are
reenabled.
A context switch can occur when calling Hwi_enable or Hwi_restore if
an enabled interrupt occurred while interrupts are disabled.
Any call to Hwi_enable enables interrupts, even if Hwi_disable has
been called several times.
Hwi_enable must not be called from main().
Hwi_enableInterrupt() // module-wide |
|
Enable a specific interrupt
UInt Hwi_enableInterrupt(UInt intNum);
ARGUMENTS
intNum
interrupt number to enable
RETURNS
key to restore previous enable/disable state
DETAILS
Enables a specific interrupt identified by an interrupt number.
Hwi_excSetBuffers() // module-wide |
|
Set the exception context and stack buffer pointers
Void Hwi_excSetBuffers(Ptr excContextBuffer, Ptr excStackBuffer);
ARGUMENTS
excContextBuffer
Address to place ExcContext
excStackBuffer
Address to place ExcStack
Hwi_getCoreStackInfo() // module-wide |
|
Get Hwi stack usage Info for the specified coreId
Bool Hwi_getCoreStackInfo(
IHwi_StackInfo *
stkInfo,
Bool computeStackDepth,
UInt coreId);
ARGUMENTS
stkInfo
pointer to structure of type StackInfo
computeStackDepth
decides whether to compute stack depth
coreId
core whose stack info needs to be retrieved
RETURNS
boolean to indicate a stack overflow
DETAILS
getCoreStackInfo returns the Hwi stack usage info for the specified
coreId to its calling function by filling stack base address,
stack size and stack peak fields in the
StackInfo structure.
This function should be used only in applications built with
ti.sysbios.BIOS.smpEnabled set to true.
getCoreStackInfo accepts three arguments, a pointer to a structure
of type
StackInfo, a boolean and a coreId. If the boolean
is set to true, the function computes the stack depth and fills the
stack peak field in the StackInfo structure. If a stack overflow
is detected, the stack depth is not computed. If the boolean is
set to false, the function only checks for a stack overflow.
The isr stack is always checked for an overflow and a boolean
is returned to indicate whether an overflow occured.
Below is an example of calling getCoreStackInfo() API:
#include <ti/sysbios/BIOS.h>
#include <ti/sysbios/hal/Hwi.h>
#include <ti/sysbios/hal/Core.h>
#include <ti/sysbios/knl/Task.h>
...
Void idleTask()
{
UInt idx;
Hwi_StackInfo stkInfo;
Bool stackOverflow = FALSE;
// Request stack depth for each core's Hwi stack and check for
// overflow
for (idx = 0; idx < Core_numCores; idx++) {
stackOverflow = Hwi_getCoreStackInfo(&stkInfo, TRUE, idx);
// Alternately, we can omit the request for stack depth and
// request only the stack base and stack size (the check for
// stack overflow is always performed):
//
// stackOverflow = Hwi_getCoreStackInfo(&stkInfo, FALSE, idx);
if (stackOverflow) {
// isr Stack Overflow detected
}
}
}
Int main(Int argc, char* argv[])
{
...
BIOS_start();
return (0);
}
Hwi_getHandle() // module-wide |
|
Returns Hwi_handle associated with intNum
ARGUMENTS
intNum
interrupt number
Hwi_getStackInfo() // module-wide |
|
Get Hwi stack usage Info
Bool Hwi_getStackInfo(
IHwi_StackInfo *
stkInfo,
Bool computeStackDepth);
ARGUMENTS
stkInfo
pointer to structure of type StackInfo
computeStackDepth
decides whether to compute stack depth
RETURNS
boolean to indicate a stack overflow
DETAILS
getStackInfo returns the Hwi stack usage info to its calling
function by filling stack base address, stack size and stack
peak fields in the
StackInfo structure.
getStackInfo accepts two arguments, a pointer to a structure
of type
StackInfo and a boolean. If the boolean is set
to true, the function computes the stack depth and fills the
stack peak field in the StackInfo structure. If a stack overflow
is detected, the stack depth is not computed. If the boolean is
set to false, the function only checks for a stack overflow.
The isr stack is always checked for an overflow and a boolean
is returned to indicate whether an overflow occured.
Below is an example of calling getStackInfo() API:
#include <ti/sysbios/BIOS.h>
#include <ti/sysbios/hal/Hwi.h>
#include <ti/sysbios/knl/Swi.h>
#include <ti/sysbios/knl/Task.h>
Swi_Handle swi0;
volatile Bool swiStackOverflow = FALSE;
Void swi0Fxn(UArg arg1, UArg arg2)
{
Hwi_StackInfo stkInfo;
// Request stack depth
swiStackOverflow = Hwi_getStackInfo(&stkInfo, TRUE);
// Alternately, we can omit the request for stack depth and
// request only the stack base and stack size (the check for
// stack overflow is always performed):
//
// swiStackOverflow = Hwi_getStackInfo(&stkInfo, FALSE);
if (swiStackOverflow) {
// isr Stack Overflow detected
}
}
Void idleTask()
{
Swi_post(swi0);
}
Int main(Int argc, char* argv[])
{
swi0 = Swi_create(swi0Fxn, NULL, NULL);
BIOS_start();
return (0);
}
Hwi_post() // module-wide |
|
Generate an interrupt for test purposes
Void Hwi_post(UInt intNum);
ARGUMENTS
intNum
ID of interrupt to generate
Hwi_restore() // module-wide |
|
Globally restore interrupts
macro Void Hwi_restore(UInt key);
ARGUMENTS
key
enable/disable state to restore
DETAILS
Hwi_restore globally restores interrupts to the state determined
by the key argument provided by a previous invocation of Hwi_disable.
A context switch may occur when calling Hwi_restore if Hwi_restore
reenables interrupts and another Hwi occurred while interrupts were
disabled.
Hwi_restore may be called from main(). However, since Hwi_enable
cannot be called from main(), interrupts are always disabled in
main(), and a call to Hwi_restore has no effect.
Hwi_restoreInterrupt() // module-wide |
|
Restore a specific interrupt's enabled/disabled state
Void Hwi_restoreInterrupt(UInt intNum, UInt key);
ARGUMENTS
intNum
interrupt number to restore
key
key returned from enableInt or disableInt
DETAILS
Restores a specific interrupt identified by an interrupt number.
restoreInterrupt is generally used to restore an interrupt to its state
before
disableInterrupt or
enableInterrupt was
invoked
Hwi_setPriority() // module-wide |
|
Set an interrupt's relative priority
Void Hwi_setPriority(UInt intNum, UInt priority);
ARGUMENTS
intNum
ID of interrupt
priority
priority
DETAILS
Valid priorities are 0 - 255. 0 is highest priority.
WARNING
Setting the priority of a dispatched Hwi to a value higher
than
Hwi.disablePriority will make
it become non-maskable by
Hwi_disable().
The behavior of your application after that will be
unpredictable and will likely yield catastrophic results!
Hwi_startup() // module-wide |
|
Initially enable interrupts
DETAILS
Called within BIOS_start
Module-Wide Built-Ins |
|
// Get this module's unique id
Bool Hwi_Module_startupDone();
// Test if this module has completed startup
// The heap from which this module allocates memory
Bool Hwi_Module_hasMask();
// Test whether this module has a diagnostics mask
Bits16 Hwi_Module_getMask();
// Returns the diagnostics mask for this module
Void Hwi_Module_setMask(Bits16 mask);
// Set the diagnostics mask for this module
Instance Object Types |
|
typedef struct Hwi_Object Hwi_Object;
// Opaque internal representation of an instance object
// Client reference to an instance object
typedef struct Hwi_Struct Hwi_Struct;
// Opaque client structure large enough to hold an instance object
// Convert this instance structure pointer into an instance handle
// Convert this instance handle into an instance structure pointer
Instance Config Parameters |
|
typedef struct Hwi_Params {
// Instance config-params structure
// Common per-instance configs
UArg arg;
// ISR function argument. Default is 0
Bool enableInt;
// Enable this interrupt when object is created? Default is true
Int eventId;
// Interrupt event ID (Interrupt Selection Number)
// Interrupt Masking Option. Only MaskingOption_LOWER is supported
Int priority;
// Interrupt priority.
The default is 255 which is the lowest priority
Bool useDispatcher;
// Use the interrupt dispatcher with this interrupt. Default is true
} Hwi_Params;
// Initialize this config-params structure with supplier-specified defaults before instance creation
config Hwi_Params.arg // instance |
|
ISR function argument. Default is 0
config Hwi_Params.enableInt // instance |
|
Enable this interrupt when object is created? Default is true
config Hwi_Params.eventId // instance |
|
Interrupt event ID (Interrupt Selection Number)
DETAILS
Default is -1.
Not all targets/devices support this instance parameter.
On those that don't, this parameter is ignored.
config Hwi_Params.maskSetting // instance |
|
Interrupt Masking Option. Only MaskingOption_LOWER is supported
DETAILS
The NVIC interrupt controller is designed for priority based
interrupts. No support is provided for anything but
Hwi.MaskingOption_LOWER.
config Hwi_Params.priority // instance |
|
Interrupt priority.
The default is 255 which is the lowest priority
DETAILS
The default value of -1 is used as a flag to indicate
the lowest (logical) device-specific priority value.
Not all targets/devices support this instance parameter.
On those that don't, this parameter is ignored.
Priority 0 is the highest priority and by default is
reserved for zero latency interrupts
(see
disablePriority).
Valid priorities values are device dependent and their
nesting behaviors depend on the
priGroup setting.
See the Cortex M3 architecture reference manual for details
on the meanings of these parameters.
config Hwi_Params.useDispatcher // instance |
|
Use the interrupt dispatcher with this interrupt. Default is true
DETAILS
If set to false, the interrupt dispatcher is NOT used. Instead,
the configured Hwi function address is placed directly in the
vector table, which results in the dispatcher being bypassed.
WARNING
Interrupts configured to bupass the dispatcher are not allowed
to call ANY SYS/BIOS APIs that effect thread scheduling. Examples
of API that should no be invoked are:
- Swi_post(),
-
- Semaphore_post(),
-
- Event_post(),
-
- Task_yield()
-
Additionally, although the signature for a non-dispatched interrupt
function is the same as that for a dispatched interrupt
(see
FuncPtr), no argument is actually passed
to the non-dispatched ISR handler.
Runtime Instance Creation |
|
// Allocate and initialize a new instance object and return its handle
// Initialize a new instance object inside the provided structure
ARGUMENTS
intNum
interrupt number
hwiFxn
pointer to ISR function
params
per-instance config params, or NULL to select default values (target-domain only)
eb
active error-handling block, or NULL to select default policy (target-domain only)
DETAILS
A Hwi dispatcher table entry is created and filled with the
function specified by the fxn parameter and the attributes
specified by the params parameter.
If params is NULL, the Hwi's dispatcher properties are assigned a
default set of values. Otherwise, the following properties
are specified by a structure of type Hwi_Params.
- The arg element is a generic argument that is passed to the plugged
function as its only parameter. The default value is 0.
- The enableInt element determines whether the interrupt should be
enabled in the IER by create.
- The maskSetting element defines the dispatcherAutoNestingSupport
behavior of the interrupt.
Hwi_create returns a pointer to the created Hwi object.
Instance Deletion |
|
// Finalize and free this previously allocated instance object, setting the referenced handle to NULL
// Finalize the instance object inside the provided structure
Hwi_getFunc() // instance |
|
Get Hwi function and arg
ARGUMENTS
handle
handle of a previously-created Hwi instance object
arg
pointer for returning hwi's ISR function argument
RETURNS
hwi's ISR function
Hwi_getHookContext() // instance |
|
Get hook instance's context for a Hwi
Ptr Hwi_getHookContext(
Hwi_Handle handle,
Int id);
ARGUMENTS
handle
handle of a previously-created Hwi instance object
RETURNS
hook instance's context for hwi
Hwi_getIrp() // instance |
|
Get address of interrupted instruction
ARGUMENTS
handle
handle of a previously-created Hwi instance object
RETURNS
most current IRP of a Hwi
Hwi_reconfig() // instance |
|
Reconfigure a dispatched interrupt
ARGUMENTS
handle
handle of a previously-created Hwi instance object
Hwi_setFunc() // instance |
|
Overwrite Hwi function and arg
ARGUMENTS
handle
handle of a previously-created Hwi instance object
fxn
pointer to ISR function
arg
argument to ISR function
DETAILS
Replaces a Hwi object's hwiFxn function originally
provided in
create.
Hwi_setHookContext() // instance |
|
Set hook instance's context for a Hwi
Void Hwi_setHookContext(
Hwi_Handle handle,
Int id,
Ptr hookContext);
ARGUMENTS
handle
handle of a previously-created Hwi instance object
id
hook instance's ID
hookContext
value to write to context
Instance Convertors |
|
// unconditionally move one level up the inheritance hierarchy
// conditionally move one level down the inheritance hierarchy; NULL upon failure
Instance Built-Ins |
|
Int Hwi_Object_count();
// The number of statically-created instance objects
// The handle of the i-th statically-created instance object (array == NULL)
// The handle of the first dynamically-created instance object, or NULL
// The handle of the next dynamically-created instance object, or NULL
// The heap used to allocate dynamically-created instance objects
// The label associated with this instance object
// The name of this instance object
enum Hwi.MaskingOption |
|
Shorthand interrupt masking options
values of type Hwi.MaskingOption
const Hwi.MaskingOption_NONE;
const Hwi.MaskingOption_ALL;
const Hwi.MaskingOption_SELF;
const Hwi.MaskingOption_BITMASK;
const Hwi.MaskingOption_LOWER;
VALUES
MaskingOption_NONE
No interrupts are disabled
MaskingOption_ALL
All interrupts are disabled
MaskingOption_SELF
Only this interrupt is disabled
MaskingOption_BITMASK
User supplies interrupt enable masks
MaskingOption_LOWER
All current and lower priority
interrupts are disabled.
Only a few targets/devices truly
support this masking option. For those
that don't, this setting is treated
the same as MaskingOption_SELF.
C SYNOPSIS
struct Hwi.CCR |
|
NVIC Configuration Control Register (CCR)
var obj = new Hwi.CCR;
obj.STKALIGN = Bits8 ...
// Auto stack alignment in exception
obj.BFHFNMIGN = Bits8 ...
// All faults ignore BUS Faults
obj.DIV_0_TRP = Bits8 ...
// Trap on divide by zero
obj.UNALIGN_TRP = Bits8 ...
// Trap on all unaligned accesses
obj.USERSETMPEND = Bits8 ...
// Allow user to trigger interrupts
obj.NONEBASETHRDENA = Bits8 ...
// Allow entering thread mode anytime
C SYNOPSIS
struct Hwi.ExcContext |
|
Exception Context - Register contents at the time of an exception
var obj = new Hwi.ExcContext;
obj.threadHandle = Ptr ...
obj.threadStack = Ptr ...
obj.threadStackSize = SizeT ...
obj.r0 = Ptr ...
obj.r1 = Ptr ...
obj.r2 = Ptr ...
obj.r3 = Ptr ...
obj.r4 = Ptr ...
obj.r5 = Ptr ...
obj.r6 = Ptr ...
obj.r7 = Ptr ...
obj.r8 = Ptr ...
obj.r9 = Ptr ...
obj.r10 = Ptr ...
obj.r11 = Ptr ...
obj.r12 = Ptr ...
obj.sp = Ptr ...
obj.lr = Ptr ...
obj.pc = Ptr ...
obj.psr = Ptr ...
obj.ICSR = Ptr ...
obj.MMFSR = Ptr ...
obj.BFSR = Ptr ...
obj.UFSR = Ptr ...
obj.HFSR = Ptr ...
obj.DFSR = Ptr ...
obj.MMAR = Ptr ...
obj.BFAR = Ptr ...
obj.AFSR = Ptr ...
C SYNOPSIS
struct Hwi.HookSet |
|
Hwi hook set type definition
var obj = new Hwi.HookSet;
obj.registerFxn = Void(*)(Int) ...
DETAILS
The functions that make up a hookSet have certain restrictions. They
cannot call any Hwi instance functions other than Hwi_getHookContext()
and Hwi_setHookContext(). For all practical purposes, they should treat
the Hwi_Handle passed to these functions as an opaque handle.
C SYNOPSIS
struct Hwi.StackInfo |
|
Structure contains Hwi stack usage info
var obj = new Hwi.StackInfo;
obj.hwiStackPeak = SizeT ...
obj.hwiStackSize = SizeT ...
obj.hwiStackBase = Ptr ...
DETAILS
Used by getStackInfo() and viewGetStackInfo() functions
C SYNOPSIS
config Hwi.A_unsupportedMaskingOption // module-wide |
|
Assert when bad maskSetting parameter provided
msg: "A_unsupportedMaskingOption: unsupported maskSetting."
};
C SYNOPSIS
config Hwi.E_NMI // module-wide |
|
Error raised when NMI exception occurs
C SYNOPSIS
config Hwi.E_alreadyDefined // module-wide |
|
Error raised when Hwi is already defined
msg: "E_alreadyDefined: Hwi already defined: intr# %d"
};
C SYNOPSIS
config Hwi.E_busFault // module-wide |
|
Error raised when bus fault exception occurs
msg: "E_busFault: %s, address: %08x"
};
C SYNOPSIS
config Hwi.E_debugMon // module-wide |
|
Error raised when debugMon exception occurs
C SYNOPSIS
config Hwi.E_exception // module-wide |
|
Error raised when an exception occurs
msg: "E_exception: id = %d, pc = %08x.\nTo see more exception detail, set ti.sysbios.family.arm.m3.Hwi.enableException = true or,\nexamine the Exception view for the ti.sysbios.family.arm.m3.Hwi module using ROV."
};
C SYNOPSIS
config Hwi.E_hardFault // module-wide |
|
Error raised when hard fault exception occurs
msg: "E_hardFault: %s"
};
C SYNOPSIS
config Hwi.E_hwiLimitExceeded // module-wide |
|
Error raised when the number of interrupts being created
exceeds the number supported
msg: "E_hwiLimitExceeded: Too many interrupts defined"
};
C SYNOPSIS
config Hwi.E_memFault // module-wide |
|
Error raised when memory fault exception occurs
msg: "E_memFault: %s, address: %08x"
};
C SYNOPSIS
config Hwi.E_noIsr // module-wide |
|
Error raised when an uninitialized interrupt occurs
msg: "E_noIsr: id = %d, pc = %08x"
};
C SYNOPSIS
config Hwi.E_reserved // module-wide |
|
Error raised when reserved exception occurs
msg: "E_reserved: %s %d"
};
C SYNOPSIS
config Hwi.E_svCall // module-wide |
|
Error raised when svCall exception occurs
msg: "E_svCall: svNum = %d"
};
C SYNOPSIS
config Hwi.E_usageFault // module-wide |
|
Error raised when usage fault exception occurs
msg: "E_usageFault: %s"
};
C SYNOPSIS
config Hwi.LD_end // module-wide |
|
Issued just after return from Hwi function (with interrupts disabled)
msg: "LD_end: hwi: 0x%x"
};
C SYNOPSIS
config Hwi.LM_begin // module-wide |
|
Issued just prior to Hwi function invocation (with interrupts disabled)
msg: "LM_begin: hwi: 0x%x, func: 0x%x, preThread: %d, intNum: %d, irp: 0x%x"
};
C SYNOPSIS
config Hwi.NUM_INTERRUPTS // module-wide |
|
The Cortex M3 NVIC supports up to 256 interrupts/exceptions
Hwi.NUM_INTERRUPTS = Int undefined;
DETAILS
The actual number supported is device specific and provided by
the catalog device specification.
C SYNOPSIS
config Hwi.NUM_PRIORITIES // module-wide |
|
The Cortex M3 NVIC supports up to 256 interrupt priorities
Hwi.NUM_PRIORITIES = Int undefined;
DETAILS
The actual number supported is device specific and provided by
the catalog device specification.
C SYNOPSIS
config Hwi.disablePriority // module-wide |
|
The priority that BASEPRI is set to by Hwi_disable()
Hwi.disablePriority = UInt undefined;
DETAILS
All interrupts configured with equal or less priority (equal or
higher number) than disablePriority are disabled by
Hwi_disable.
Interrupts configured with higher priority (smaller number) than
Hwi.disablePriority are non-maskable (ie zero-latency).
The default setting is the second highest interrupt priority
defined for the device (typically '0x20' for devices
which support 8 priority values).
This results in priority 0 (and all
other values in the same priority group, ie 0x00 thru 0x1f)
being the zero-latency, non-maskable interrupt priority.
All other priorities are disabled with Hwi_disable().
C SYNOPSIS
config Hwi.dispatcherAutoNestingSupport // module-wide |
|
Include interrupt nesting logic in interrupt dispatcher?
Hwi.dispatcherAutoNestingSupport = Bool true;
DETAILS
Default is true.
This option provides the user with the ability to optimize
interrupt dispatcher performance when support for interrupt
nesting is not required.
Setting this parameter to false will disable the logic in
the interrupt dispatcher that manipulates interrupt mask
registers and enables and disables interrupts before and
after invoking the user's Hwi function.
Set this parameter to false if you don't need interrupts
enabled during the execution of your Hwi functions.
C SYNOPSIS
config Hwi.dispatcherIrpTrackingSupport // module-wide |
|
Controls whether the
dispatcher retains the interrupted thread's return address
Hwi.dispatcherIrpTrackingSupport = Bool true;
DETAILS
This option is enabled by default.
Setting this parameter to false will disable the logic in
the interrupt dispatcher that keeps track of the interrupt's
return address and provide a small savings in interrupt latency.
The application can get an interrupt's most recent return
address using the
getIrp API.
C SYNOPSIS
config Hwi.dispatcherSwiSupport // module-wide |
|
Include Swi scheduling logic in interrupt dispatcher?
Hwi.dispatcherSwiSupport = Bool undefined;
DETAILS
Default is inherited from
BIOS.swiEnabled, which is true by default.
This option provides the user with the ability to optimize
interrupt dispatcher performance when it is known that Swis
will not be posted from any of their Hwi threads.
WARNING
Setting this parameter to false will disable the logic in
the interrupt dispatcher that invokes the Swi scheduler
prior to returning from an interrupt.
With this setting, Swis MUST NOT be posted from Hwi functions!
C SYNOPSIS
config Hwi.dispatcherTaskSupport // module-wide |
|
Include Task scheduling logic in interrupt dispatcher?
Hwi.dispatcherTaskSupport = Bool undefined;
DETAILS
Default is inherited from
BIOS.taskEnabled, which is true by default.
This option provides the user with the ability to optimize
interrupt dispatcher performance when it is known that no
Task scheduling APIs (ie
Semaphore_post()) will be executed from any of their Hwi threads.
Setting this parameter to false will disable the logic in
the interrupt dispatcher that invokes the Task scheduler
prior to returning from an interrupt.
C SYNOPSIS
config Hwi.excHandlerFunc // module-wide |
|
Exception handler function pointer
DETAILS
The default is determined by the value of Hwi.enableException.
If the user does NOT set this parameter, then the following default
behavior is followed:
If Hwi.enableException is true, then the internal 'Hwi_excHandlerMax'
function is used. This exception handler saves the exception context
then does a complete exception decode and dump to the console, then
raises an Error. The exception context can be viewed within CCS
in the ROV Hwi module's Exception view.
If Hwi.enableException is false, then the internal 'Hwi_excHandlerMin'
function is used. This exception handler saves the exception context
then raises an Error. The exception context can be viewed within CCS
in the ROV Hwi module's Exception view.
If the user sets this parameter to their own function, then the user's
function will be invoked with the following arguments:
Void myExceptionHandler(UInt *excStack, UInt lr);
Where 'excStack' is the address of the stack containing the
register context at the time of the exception, and 'lr' is the
link register value when the low-level-assembly-coded exception
handler was vectored to.
If this parameter is set to 'null', then an infinite while loop is
entered when an exception occurs. This setting minimizes code and
data footprint but provides no automatic exception decoding.
C SYNOPSIS
config Hwi.excHookFunc // module-wide |
|
User Exception hook function
DETAILS
Called just after the exception context has been initialized.
This function will be run on the ISR stack.
This function must run to completion.
It is called without any Task or Swi scheduling protection
and therefore can not call any functions that may cause a Swi or Task
scheduling operation (Swi_post(), Semaphore_post(), Event_post(), etc).
C SYNOPSIS
config Hwi.excHookFuncs // module-wide |
|
C SYNOPSIS
config Hwi.nullIsrFunc // module-wide |
|
Uninitialized ISR Handler. Default is set to an internal exception handler
Hwi.nullIsrFunc = Void(*)(Void) undefined;
C SYNOPSIS
config Hwi.priGroup // module-wide |
|
The PRIGROUP setting. Default is 0
DETAILS
This value will be written to the PRIGROUP field
within the NVIC's Application Interrupt and Reset Control
Register (Hwi_nvic.AIRCR). It defines how the 8 bit priority
values are interpreted by the hardware.
Valid settings are 0-7.
The default setting of 0 causes bits 7-1 of an interrupt's
priority value to be used as pre-emption priority, while bit 0
is used to determine which of two simultaneous interrupts with
the same pre-emption priority will be serviced first.
For most TI MCU devices, this means that each of the 8 supported
priority values are unique pre-emption priorities and are not
subdivided into priority groups.
C SYNOPSIS
metaonly config Hwi.busFaultFunc // module-wide |
|
Bus Fault Handler. Default is set to an internal exception handler
Hwi.busFaultFunc = Void(*)(Void) undefined;
metaonly config Hwi.common$ // module-wide |
|
Common module configuration parameters
DETAILS
All modules have this configuration parameter. Its name
contains the '$' character to ensure it does not conflict with
configuration parameters declared by the module. This allows
new configuration parameters to be added in the future without
any chance of breaking existing modules.
metaonly config Hwi.debugMonFunc // module-wide |
|
Debug Mon Handler. Default is set to an internal exception handler
Hwi.debugMonFunc = Void(*)(Void) undefined;
metaonly config Hwi.dispatchTableSize // module-wide |
|
Size (in number of interrupts) of the table used by the interrupt
dispatcher to locate the corresponding Hwi object. By default,
Hwi.dispatchTableSize will be internally set
to the number of interrupts supported by the device
Hwi.dispatchTableSize = UInt undefined;
DETAILS
When the Hwi dispatch table size is equal to the number of interrupts
supported
NUM_INTERRUPTS by the device, a linear-indexed
dispatch table mechanism is used that will consume 4 bytes of RAM
for each interrupt supported.
If the dispatch table size is set to a number less than the number
of interrupts supported by the device, then a non linear-indexed
dispatch table mechanism is employed that uses 12 bytes of RAM for
each interrupt supported.
Consequently, for applications that use less than 1/3 of the total
number of interrupts supported by the device, setting this parameter
to the number of interrupts ACTUALLY USED will result in less RAM
memory being used than otherwise.
For applications that use very few interrupts, this can be a significant RAM memory savings.</p>
metaonly config Hwi.enableException // module-wide |
|
Enable full exception decoding
Hwi.enableException = Bool true;
DETAILS
When this is enabled, the exception handler will fully
decode an exception and dump the registers to the
system console.
metaonly config Hwi.excContextBuffer // module-wide |
|
User Exception Context Buffer Address
Hwi.excContextBuffer = Ptr undefined;
DETAILS
By default, when an exception occurs, an
ExcContext
structure is allocated on the ISR stack and filled in within the
exception handler.
If
excContextBuffer is initialized by the user, the
ExcContext structure will be placed at that address instead.
The buffer must be large enough to contain an
ExcContext
structure.
metaonly config Hwi.excContextBuffers // module-wide |
|
Hwi.excContextBuffers = Ptr[] undefined;
metaonly config Hwi.excStackBuffer // module-wide |
|
User Exception Stack Buffer Address
Hwi.excStackBuffer = Ptr undefined;
DETAILS
By default, when an exception occurs, a pointer to the base address
of the stack being used by the thread causing the exception is placed
If
excStackBuffer is initialized by the user, the
stack contents of the thread causing the exception will be
copied to that address instead.
The buffer must be large enough to contain the largest task stack
or ISR stack defined in the application.
metaonly config Hwi.excStackBuffers // module-wide |
|
Hwi.excStackBuffers = Ptr[] undefined;
metaonly config Hwi.hardFaultFunc // module-wide |
|
Hard Fault Handler. Default is set to an internal exception handler
Hwi.hardFaultFunc = Void(*)(Void) undefined;
metaonly config Hwi.intAffinity // module-wide |
|
Hwi.intAffinity = UInt8[] undefined;
metaonly config Hwi.memFaultFunc // module-wide |
|
Hard Mem Handler. Default is set to an internal exception handler
Hwi.memFaultFunc = Void(*)(Void) undefined;
metaonly config Hwi.nmiFunc // module-wide |
|
NMI Handler. Default is set to an internal exception handler
Hwi.nmiFunc = Void(*)(Void) undefined;
metaonly config Hwi.nvicCCR // module-wide |
|
NVIC CCR register settings
STKALIGN: 1,
BFHFNMIGN: 0,
DIV_0_TRP: 0,
UNALIGN_TRP: 0,
USERSETMPEND: 0,
NONEBASETHRDENA: 0
};
DETAILS
These setting are written to Hwi_nvic.CCR at startup time.
See the Cortex M3 architecture reference manual for details
on the meanings of these parameters.
metaonly config Hwi.reservedFunc // module-wide |
|
Reserved Exception Handler. Default is set to an internal exception handler
Hwi.reservedFunc = Void(*)(Void) undefined;
metaonly config Hwi.resetFunc // module-wide |
|
Reset Handler. Default is c_int00
Hwi.resetFunc = Void(*)(Void) undefined;
metaonly config Hwi.resetVectorAddress // module-wide |
|
Reset vector table address. Default is 0x00000000
Hwi.resetVectorAddress = Ptr 0x00000000;
DETAILS
This parameter is the address of the vector table used
at system reset time. Typically this is placed at 0x00000000.
If the Hwi.resetVectorAddress has a different value than
the
Hwi.vectorTableAddress
then two vector tables are generated, one at the Hwi.resetVectorAddress
and another at the
Hwi.vectorTableAddress.
After the initial boot code has been executed at startup, the NVIC's
Vector Table Offset Register will be programmed to point to the
vector table at the
Hwi.vectorTableAddress.
is created and placed in the ".resetVecs" section.
metaonly config Hwi.svCallFunc // module-wide |
|
SVCall Handler. Default is set to an internal exception handler
Hwi.svCallFunc = Void(*)(Void) undefined;
metaonly config Hwi.usageFaultFunc // module-wide |
|
Usage Fault Handler. Default is set to an internal exception handler
Hwi.usageFaultFunc = Void(*)(Void) undefined;
metaonly config Hwi.vectorTableAddress // module-wide |
|
Location of the Runtime Interrupt Vector Table.
Default is device dependent
Hwi.vectorTableAddress = Ptr 0x00000000;
DETAILS
This parameter allows the user to override the default placement
of the runtime interrupt vector table.
The NVIC's Vector Table Offset
Register (VTOR) is also programmed to this value.
Some systems require the runtime vector table to be placed at
an address
other than 0 but still need a copy of the two M3 boot vectors
(SP and reset PC), located there. To achieve this, a separate
parameter
resetVectorAdress is provided. If the
resetVectorAddress has a different value then the vectorTableAddress
then a separate vector table is generated and placed at that
address.
The vector table must be placed at an address at or lower than
0x3FFFFC00 and must be aligned on an even 64 word boundary.
metaonly Hwi.addHookSet() // module-wide |
|
addHookSet is used in a config file to add a hook set (defined
by struct HookSet)
ARGUMENTS
hook
structure of type HookSet
DETAILS
HookSet structure elements may be omitted, in which case those
elements will not exist.
Instance Config Parameters |
|
var params = new Hwi.Params;
// Instance config-params object
params.arg = UArg 0;
// ISR function argument. Default is 0
params.enableInt = Bool true;
// Enable this interrupt when object is created? Default is true
params.eventId = Int -1;
// Interrupt event ID (Interrupt Selection Number)
// Interrupt Masking Option. Only MaskingOption_LOWER is supported
params.priority = Int 255;
// Interrupt priority.
The default is 255 which is the lowest priority
params.useDispatcher = Bool true;
// Use the interrupt dispatcher with this interrupt. Default is true
config Hwi.Params.arg // instance |
|
ISR function argument. Default is 0
var params = new Hwi.Params;
...
params.arg = UArg 0;
C SYNOPSIS
config Hwi.Params.enableInt // instance |
|
Enable this interrupt when object is created? Default is true
var params = new Hwi.Params;
...
params.enableInt = Bool true;
C SYNOPSIS
config Hwi.Params.eventId // instance |
|
Interrupt event ID (Interrupt Selection Number)
var params = new Hwi.Params;
...
params.eventId = Int -1;
DETAILS
Default is -1.
Not all targets/devices support this instance parameter.
On those that don't, this parameter is ignored.
C SYNOPSIS
config Hwi.Params.maskSetting // instance |
|
Interrupt Masking Option. Only MaskingOption_LOWER is supported
var params = new Hwi.Params;
...
DETAILS
The NVIC interrupt controller is designed for priority based
interrupts. No support is provided for anything but
Hwi.MaskingOption_LOWER.
C SYNOPSIS
config Hwi.Params.priority // instance |
|
Interrupt priority.
The default is 255 which is the lowest priority
var params = new Hwi.Params;
...
params.priority = Int 255;
DETAILS
The default value of -1 is used as a flag to indicate
the lowest (logical) device-specific priority value.
Not all targets/devices support this instance parameter.
On those that don't, this parameter is ignored.
Priority 0 is the highest priority and by default is
reserved for zero latency interrupts
(see
disablePriority).
Valid priorities values are device dependent and their
nesting behaviors depend on the
priGroup setting.
See the Cortex M3 architecture reference manual for details
on the meanings of these parameters.
C SYNOPSIS
config Hwi.Params.useDispatcher // instance |
|
Use the interrupt dispatcher with this interrupt. Default is true
var params = new Hwi.Params;
...
params.useDispatcher = Bool true;
DETAILS
If set to false, the interrupt dispatcher is NOT used. Instead,
the configured Hwi function address is placed directly in the
vector table, which results in the dispatcher being bypassed.
WARNING
Interrupts configured to bupass the dispatcher are not allowed
to call ANY SYS/BIOS APIs that effect thread scheduling. Examples
of API that should no be invoked are:
- Swi_post(),
-
- Semaphore_post(),
-
- Event_post(),
-
- Task_yield()
-
Additionally, although the signature for a non-dispatched interrupt
function is the same as that for a dispatched interrupt
(see
FuncPtr), no argument is actually passed
to the non-dispatched ISR handler.
C SYNOPSIS
Static Instance Creation |
|
// Allocate instance config-params
params.config = ...
// Assign individual configs
var inst = Hwi.create(Int intNum, Void(*)(UArg) hwiFxn, params);
// Create an instance-object
ARGUMENTS
intNum
interrupt number
hwiFxn
pointer to ISR function
params
per-instance config params, or NULL to select default values (target-domain only)
eb
active error-handling block, or NULL to select default policy (target-domain only)
DETAILS
A Hwi dispatcher table entry is created and filled with the
function specified by the fxn parameter and the attributes
specified by the params parameter.
If params is NULL, the Hwi's dispatcher properties are assigned a
default set of values. Otherwise, the following properties
are specified by a structure of type Hwi_Params.
- The arg element is a generic argument that is passed to the plugged
function as its only parameter. The default value is 0.
- The enableInt element determines whether the interrupt should be
enabled in the IER by create.
- The maskSetting element defines the dispatcherAutoNestingSupport
behavior of the interrupt.
Hwi_create returns a pointer to the created Hwi object.