#include <rf_prop_cmd.h>
Data Fields | |
struct { | |
uint8_t bEnaRssi:1 | |
If 1, enable RSSI as a criterion. More... | |
uint8_t bEnaCorr:1 | |
If 1, enable correlation as a criterion. More... | |
uint8_t operation:1 | |
0: Busy if either RSSI or correlation indicates Busy 1: Busy if both RSSI and correlation indicates Busy More... | |
uint8_t busyOp:1 | |
0: Continue carrier sense on channel Busy 1: End carrier sense on channel Busy For an RX command, the receiver will continue when carrier sense ends, but it will then not end if channel goes Idle More... | |
uint8_t idleOp:1 | |
0: Continue on channel Idle 1: End on channel Idle More... | |
uint8_t timeoutRes:1 | |
0: Timeout with channel state Invalid treated as Busy 1: Timeout with channel state Invalid treated as Idle More... | |
} | csConf |
int8_t | rssiThr |
RSSI threshold. More... | |
uint8_t | numRssiIdle |
Number of consecutive RSSI measurements below the threshold needed before the channel is declared Idle. More... | |
uint8_t | numRssiBusy |
Number of consecutive RSSI measurements above the threshold needed before the channel is declared Busy. More... | |
uint16_t | corrPeriod |
Number of RAT ticks for a correlation observation periods. More... | |
struct { | |
uint8_t numCorrInv:4 | |
Number of subsequent correlation tops with maximum corrPeriod RAT ticks between them needed to go from Idle to Invalid. More... | |
uint8_t numCorrBusy:4 | |
Number of subsequent correlation tops with maximum corrPeriod RAT ticks between them needed to go from Invalid to Busy. More... | |
} | corrConfig |
struct { | |
uint8_t triggerType:4 | |
The type of trigger. More... | |
uint8_t bEnaCmd:1 | |
0: No alternative trigger command 1: CMD_TRIGGER can be used as an alternative trigger More... | |
uint8_t triggerNo:2 | |
The trigger number of the CMD_TRIGGER command that triggers this action. More... | |
uint8_t pastTrig:1 | |
0: A trigger in the past is never triggered, or for start of commands, give an error 1: A trigger in the past is triggered as soon as possible More... | |
} | csEndTrigger |
Trigger classifier for ending the carrier sense. More... | |
ratmr_t | csEndTime |
Time used together with csEndTrigger for ending the operation. More... | |
Definition at line 77 of file rf_prop_cmd.h.
uint8_t rfc_carrierSense_s::bEnaCmd |
0: No alternative trigger command
1: CMD_TRIGGER can be used as an alternative trigger
Definition at line 105 of file rf_prop_cmd.h.
uint8_t rfc_carrierSense_s::bEnaCorr |
If 1, enable correlation as a criterion.
Definition at line 80 of file rf_prop_cmd.h.
uint8_t rfc_carrierSense_s::bEnaRssi |
If 1, enable RSSI as a criterion.
Definition at line 79 of file rf_prop_cmd.h.
uint8_t rfc_carrierSense_s::busyOp |
0: Continue carrier sense on channel Busy
1: End carrier sense on channel Busy
For an RX command, the receiver will continue when carrier sense ends, but it will then not end if channel goes Idle
Definition at line 83 of file rf_prop_cmd.h.
struct { ... } rfc_carrierSense_s::corrConfig |
uint16_t rfc_carrierSense_s::corrPeriod |
Number of RAT ticks for a correlation observation periods.
Definition at line 96 of file rf_prop_cmd.h.
struct { ... } rfc_carrierSense_s::csConf |
ratmr_t rfc_carrierSense_s::csEndTime |
Time used together with csEndTrigger
for ending the operation.
Definition at line 111 of file rf_prop_cmd.h.
struct { ... } rfc_carrierSense_s::csEndTrigger |
Trigger classifier for ending the carrier sense.
uint8_t rfc_carrierSense_s::idleOp |
0: Continue on channel Idle
1: End on channel Idle
Definition at line 86 of file rf_prop_cmd.h.
uint8_t rfc_carrierSense_s::numCorrBusy |
Number of subsequent correlation tops with maximum corrPeriod
RAT ticks between them needed to go from Invalid to Busy.
Definition at line 100 of file rf_prop_cmd.h.
uint8_t rfc_carrierSense_s::numCorrInv |
Number of subsequent correlation tops with maximum corrPeriod
RAT ticks between them needed to go from Idle to Invalid.
Definition at line 98 of file rf_prop_cmd.h.
uint8_t rfc_carrierSense_s::numRssiBusy |
Number of consecutive RSSI measurements above the threshold needed before the channel is declared Busy.
Definition at line 94 of file rf_prop_cmd.h.
uint8_t rfc_carrierSense_s::numRssiIdle |
Number of consecutive RSSI measurements below the threshold needed before the channel is declared Idle.
Definition at line 92 of file rf_prop_cmd.h.
uint8_t rfc_carrierSense_s::operation |
0: Busy if either RSSI or correlation indicates Busy
1: Busy if both RSSI and correlation indicates Busy
Definition at line 81 of file rf_prop_cmd.h.
uint8_t rfc_carrierSense_s::pastTrig |
0: A trigger in the past is never triggered, or for start of commands, give an error
1: A trigger in the past is triggered as soon as possible
Definition at line 108 of file rf_prop_cmd.h.
int8_t rfc_carrierSense_s::rssiThr |
RSSI threshold.
Definition at line 91 of file rf_prop_cmd.h.
uint8_t rfc_carrierSense_s::timeoutRes |
0: Timeout with channel state Invalid treated as Busy
1: Timeout with channel state Invalid treated as Idle
Definition at line 88 of file rf_prop_cmd.h.
uint8_t rfc_carrierSense_s::triggerNo |
The trigger number of the CMD_TRIGGER command that triggers this action.
Definition at line 107 of file rf_prop_cmd.h.
uint8_t rfc_carrierSense_s::triggerType |
The type of trigger.
Definition at line 104 of file rf_prop_cmd.h.