#include <rf_ble_cmd.h>
Data Fields | |
uint8_t | nTxConnectReq |
Number of transmitted CONNECT_REQ packets. More... | |
uint8_t | nRxAdvOk |
Number of ADV*_IND packets received with CRC OK and not ignored. More... | |
uint16_t | nRxAdvIgnored |
Number of ADV*_IND packets received with CRC OK, but ignored. More... | |
uint16_t | nRxAdvNok |
Number of ADV*_IND packets received with CRC error. More... | |
uint8_t | nRxAdvBufFull |
Number of ADV*_IND packets received that did not fit in Rx queue. More... | |
int8_t | lastRssi |
The RSSI of the last received packet. More... | |
ratmr_t | timeStamp |
Time stamp of the received ADV*_IND packet that caused transmission of CONNECT_REQ. More... | |
Definition at line 1037 of file rf_ble_cmd.h.
int8_t rfc_bleInitiatorOutput_s::lastRssi |
The RSSI of the last received packet.
Definition at line 1043 of file rf_ble_cmd.h.
uint8_t rfc_bleInitiatorOutput_s::nRxAdvBufFull |
Number of ADV*_IND packets received that did not fit in Rx queue.
Definition at line 1042 of file rf_ble_cmd.h.
uint16_t rfc_bleInitiatorOutput_s::nRxAdvIgnored |
Number of ADV*_IND packets received with CRC OK, but ignored.
Definition at line 1040 of file rf_ble_cmd.h.
uint16_t rfc_bleInitiatorOutput_s::nRxAdvNok |
Number of ADV*_IND packets received with CRC error.
Definition at line 1041 of file rf_ble_cmd.h.
uint8_t rfc_bleInitiatorOutput_s::nRxAdvOk |
Number of ADV*_IND packets received with CRC OK and not ignored.
Definition at line 1039 of file rf_ble_cmd.h.
uint8_t rfc_bleInitiatorOutput_s::nTxConnectReq |
Number of transmitted CONNECT_REQ packets.
Definition at line 1038 of file rf_ble_cmd.h.
ratmr_t rfc_bleInitiatorOutput_s::timeStamp |
Time stamp of the received ADV*_IND packet that caused transmission of CONNECT_REQ.
Definition at line 1044 of file rf_ble_cmd.h.