CC26xx Driver Library
vims.c
Go to the documentation of this file.
1 /******************************************************************************
2 * Filename: vims.c
3 * Revised: 2015-09-21 15:46:11 +0200 (Mon, 21 Sep 2015)
4 * Revision: 44630
5 *
6 * Description: Driver for the VIMS.
7 *
8 * Copyright (c) 2015, Texas Instruments Incorporated
9 * All rights reserved.
10 *
11 * Redistribution and use in source and binary forms, with or without
12 * modification, are permitted provided that the following conditions are met:
13 *
14 * 1) Redistributions of source code must retain the above copyright notice,
15 * this list of conditions and the following disclaimer.
16 *
17 * 2) Redistributions in binary form must reproduce the above copyright notice,
18 * this list of conditions and the following disclaimer in the documentation
19 * and/or other materials provided with the distribution.
20 *
21 * 3) Neither the name of the ORGANIZATION nor the names of its contributors may
22 * be used to endorse or promote products derived from this software without
23 * specific prior written permission.
24 *
25 * THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS "AS IS"
26 * AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT LIMITED TO, THE
27 * IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR A PARTICULAR PURPOSE
28 * ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT HOLDER OR CONTRIBUTORS BE
29 * LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, SPECIAL, EXEMPLARY, OR
30 * CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT LIMITED TO, PROCUREMENT OF
31 * SUBSTITUTE GOODS OR SERVICES; LOSS OF USE, DATA, OR PROFITS; OR BUSINESS
32 * INTERRUPTION) HOWEVER CAUSED AND ON ANY THEORY OF LIABILITY, WHETHER IN
33 * CONTRACT, STRICT LIABILITY, OR TORT (INCLUDING NEGLIGENCE OR OTHERWISE)
34 * ARISING IN ANY WAY OUT OF THE USE OF THIS SOFTWARE, EVEN IF ADVISED OF THE
35 * POSSIBILITY OF SUCH DAMAGE.
36 *
37 ******************************************************************************/
38 
39 #include <driverlib/vims.h>
40 
41 //*****************************************************************************
42 //
43 // Handle support for DriverLib in ROM:
44 // This section will undo prototype renaming made in the header file
45 //
46 //*****************************************************************************
47 #if !defined(DOXYGEN)
48  #undef VIMSConfigure
49  #define VIMSConfigure NOROM_VIMSConfigure
50  #undef VIMSModeSet
51  #define VIMSModeSet NOROM_VIMSModeSet
52  #undef VIMSModeGet
53  #define VIMSModeGet NOROM_VIMSModeGet
54  #undef VIMSModeSafeSet
55  #define VIMSModeSafeSet NOROM_VIMSModeSafeSet
56 #endif
57 
58 //*****************************************************************************
59 //
60 // Configures the VIMS.
61 //
62 //*****************************************************************************
63 void
64 VIMSConfigure(uint32_t ui32Base, bool bRoundRobin, bool bPrefetch)
65 {
66  uint32_t ui32Reg;
67 
68  //
69  // Check the arguments.
70  //
71  ASSERT(VIMSBaseValid(ui32Base));
72 
73  ui32Reg = HWREG(ui32Base + VIMS_O_CTL);
74  ui32Reg &= ~(VIMS_CTL_PREF_EN | VIMS_CTL_ARB_CFG);
75  if(bRoundRobin)
76  {
77  ui32Reg |= VIMS_CTL_ARB_CFG;
78  }
79  if(bPrefetch)
80  {
81  ui32Reg |= VIMS_CTL_PREF_EN;
82  }
83 
84  //
85  // Set the Arbitration and prefetch mode.
86  //
87  HWREG(ui32Base + VIMS_O_CTL) = ui32Reg;
88 }
89 
90 //*****************************************************************************
91 //
92 // Set the operational mode of the VIMS
93 //
94 //*****************************************************************************
95 void
96 VIMSModeSet(uint32_t ui32Base, uint32_t ui32Mode)
97 {
98  uint32_t ui32Reg;
99 
100  //
101  // Check the arguments.
102  //
103  ASSERT(VIMSBaseValid(ui32Base));
104 
105  ASSERT((ui32Mode == VIMS_MODE_DISABLED) ||
106  (ui32Mode == VIMS_MODE_ENABLED) ||
107  (ui32Mode == VIMS_MODE_OFF));
108 
109  //
110  // Set the mode.
111  //
112  ui32Reg = HWREG(ui32Base + VIMS_O_CTL);
113  ui32Reg &= ~VIMS_CTL_MODE_M;
114  ui32Reg |= (ui32Mode & VIMS_CTL_MODE_M);
115 
116  HWREG(ui32Base + VIMS_O_CTL) = ui32Reg;
117 }
118 
119 //*****************************************************************************
120 //
121 // Get the current operational mode of the VIMS.
122 //
123 //*****************************************************************************
124 uint32_t
125 VIMSModeGet(uint32_t ui32Base)
126 {
127  uint32_t ui32Reg;
128 
129  //
130  // Check the arguments.
131  //
132  ASSERT(VIMSBaseValid(ui32Base));
133 
134  ui32Reg = HWREG(ui32Base + VIMS_O_STAT);
135  if(ui32Reg & VIMS_STAT_MODE_CHANGING)
136  {
137  return (VIMS_MODE_CHANGING);
138  }
139  else
140  {
141  return (ui32Reg & VIMS_STAT_MODE_M);
142  }
143 }
144 
145 //*****************************************************************************
146 //
147 // Safe setting of new VIMS mode
148 // - Function might be blocking
149 // - Can be called for any mode change (also if actually not changing mode)
150 //
151 //*****************************************************************************
152 void
153 VIMSModeSafeSet( uint32_t ui32Base, uint32_t ui32NewMode, bool blocking )
154 {
155  uint32_t currentMode;
156 
157  //
158  // Check the arguments.
159  //
160  ASSERT(VIMSBaseValid(ui32Base));
161  ASSERT((ui32NewMode == VIMS_MODE_DISABLED) ||
162  (ui32NewMode == VIMS_MODE_ENABLED) ||
163  (ui32NewMode == VIMS_MODE_OFF));
164 
165  //
166  // Make sure that only the mode bits are set in the input parameter
167  // (done just for security since it is critical to the code flow)
168  //
169  ui32NewMode &= VIMS_CTL_MODE_M;
170 
171  //
172  // Wait for any pending change to complete and get current VIMS mode
173  // (This is a blocking point but will typically only be a blocking point
174  // only if mode is changed multiple times with blocking=0)
175  //
176  do {
177  currentMode = VIMSModeGet( ui32Base );
178  } while ( currentMode == VIMS_MODE_CHANGING );
179 
180  //
181  // First check that it actually is a mode change request
182  //
183  if ( ui32NewMode != currentMode ) {
184  //
185  // Due to a hw-problem it is strongly recommended to go via VIMS_MODE_OFF
186  // when leaving VIMS_MODE_ENABLED (=VIMS_CTL_MODE_CACHE)
187  // (And no need to go via OFF, if OFF is the final state and will be set later)
188  //
189  if (( currentMode == VIMS_CTL_MODE_CACHE ) &&
190  ( ui32NewMode != VIMS_CTL_MODE_OFF ) )
191  {
192  VIMSModeSet( ui32Base, VIMS_MODE_OFF );
193 
194  while ( HWREGBITW( VIMS_BASE + VIMS_O_STAT, VIMS_STAT_MODE_CHANGING_BITN )) {
195  // Do nothing - wait for change to complete.
196  // (Needed blocking point but it takes only some few cycles)
197  }
198  }
199  //
200  // Set new mode
201  //
202  VIMSModeSet( ui32Base, ui32NewMode );
203 
204  //
205  // Wait for final mode change to complete - if blocking is requested
206  //
207  if ( blocking ) {
208  while ( HWREGBITW( VIMS_BASE + VIMS_O_STAT, VIMS_STAT_MODE_CHANGING_BITN )) {
209  // Do nothing - wait for change to complete.
210  }
211  }
212  }
213 }
void VIMSModeSet(uint32_t ui32Base, uint32_t ui32Mode)
Set the operational mode of the VIMS.
Definition: vims.c:96
#define VIMS_MODE_ENABLED
Definition: vims.h:98
void VIMSModeSafeSet(uint32_t ui32Base, uint32_t ui32NewMode, bool blocking)
Set the operational mode of the VIMS in a safe sequence.
Definition: vims.c:153
uint32_t VIMSModeGet(uint32_t ui32Base)
Get the current operational mode of the VIMS.
Definition: vims.c:125
#define ASSERT(expr)
Definition: debug.h:74
#define VIMS_MODE_DISABLED
Definition: vims.h:97
#define VIMS_MODE_CHANGING
Definition: vims.h:95
#define VIMS_MODE_OFF
Definition: vims.h:99
void VIMSConfigure(uint32_t ui32Base, bool bRoundRobin, bool bPrefetch)
Configures the VIMS.
Definition: vims.c:64