CC26xx Driver Library
ioc.h
Go to the documentation of this file.
1 /******************************************************************************
2 * Filename: ioc.h
3 * Revised: 2015-11-17 14:14:34 +0100 (Tue, 17 Nov 2015)
4 * Revision: 45115
5 *
6 * Description: Defines and prototypes for the IO Controller.
7 *
8 * Copyright (c) 2015, Texas Instruments Incorporated
9 * All rights reserved.
10 *
11 * Redistribution and use in source and binary forms, with or without
12 * modification, are permitted provided that the following conditions are met:
13 *
14 * 1) Redistributions of source code must retain the above copyright notice,
15 * this list of conditions and the following disclaimer.
16 *
17 * 2) Redistributions in binary form must reproduce the above copyright notice,
18 * this list of conditions and the following disclaimer in the documentation
19 * and/or other materials provided with the distribution.
20 *
21 * 3) Neither the name of the ORGANIZATION nor the names of its contributors may
22 * be used to endorse or promote products derived from this software without
23 * specific prior written permission.
24 *
25 * THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS "AS IS"
26 * AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT LIMITED TO, THE
27 * IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR A PARTICULAR PURPOSE
28 * ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT HOLDER OR CONTRIBUTORS BE
29 * LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, SPECIAL, EXEMPLARY, OR
30 * CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT LIMITED TO, PROCUREMENT OF
31 * SUBSTITUTE GOODS OR SERVICES; LOSS OF USE, DATA, OR PROFITS; OR BUSINESS
32 * INTERRUPTION) HOWEVER CAUSED AND ON ANY THEORY OF LIABILITY, WHETHER IN
33 * CONTRACT, STRICT LIABILITY, OR TORT (INCLUDING NEGLIGENCE OR OTHERWISE)
34 * ARISING IN ANY WAY OUT OF THE USE OF THIS SOFTWARE, EVEN IF ADVISED OF THE
35 * POSSIBILITY OF SUCH DAMAGE.
36 *
37 ******************************************************************************/
38 
39 //*****************************************************************************
40 //
45 //
46 //*****************************************************************************
47 
48 #ifndef __IOC_H__
49 #define __IOC_H__
50 
51 //*****************************************************************************
52 //
53 // If building with a C++ compiler, make all of the definitions in this header
54 // have a C binding.
55 //
56 //*****************************************************************************
57 #ifdef __cplusplus
58 extern "C"
59 {
60 #endif
61 
62 #include <stdbool.h>
63 #include <stdint.h>
64 #include <inc/hw_types.h>
65 #include <inc/hw_memmap.h>
66 #include <inc/hw_ioc.h>
67 #include <inc/hw_ints.h>
68 #include <driverlib/interrupt.h>
69 #include <driverlib/debug.h>
70 #include <driverlib/gpio.h>
71 
72 //*****************************************************************************
73 //
74 // Support for DriverLib in ROM:
75 // This section renames all functions that are not "static inline", so that
76 // calling these functions will default to implementation in flash. At the end
77 // of this file a second renaming will change the defaults to implementation in
78 // ROM for available functions.
79 //
80 // To force use of the implementation in flash, e.g. for debugging:
81 // - Globally: Define DRIVERLIB_NOROM at project level
82 // - Per function: Use prefix "NOROM_" when calling the function
83 //
84 //*****************************************************************************
85 #if !defined(DOXYGEN)
86  #define IOCPortConfigureSet NOROM_IOCPortConfigureSet
87  #define IOCPortConfigureGet NOROM_IOCPortConfigureGet
88  #define IOCIOShutdownSet NOROM_IOCIOShutdownSet
89  #define IOCIOModeSet NOROM_IOCIOModeSet
90  #define IOCIOIntSet NOROM_IOCIOIntSet
91  #define IOCIOPortPullSet NOROM_IOCIOPortPullSet
92  #define IOCIOHystSet NOROM_IOCIOHystSet
93  #define IOCIOInputSet NOROM_IOCIOInputSet
94  #define IOCIOSlewCtrlSet NOROM_IOCIOSlewCtrlSet
95  #define IOCIODrvStrengthSet NOROM_IOCIODrvStrengthSet
96  #define IOCIOPortIdSet NOROM_IOCIOPortIdSet
97  #define IOCIntEnable NOROM_IOCIntEnable
98  #define IOCIntDisable NOROM_IOCIntDisable
99  #define IOCPinTypeGpioInput NOROM_IOCPinTypeGpioInput
100  #define IOCPinTypeGpioOutput NOROM_IOCPinTypeGpioOutput
101  #define IOCPinTypeUart NOROM_IOCPinTypeUart
102  #define IOCPinTypeSsiMaster NOROM_IOCPinTypeSsiMaster
103  #define IOCPinTypeSsiSlave NOROM_IOCPinTypeSsiSlave
104  #define IOCPinTypeI2c NOROM_IOCPinTypeI2c
105  #define IOCPinTypeAux NOROM_IOCPinTypeAux
106 #endif
107 
108 //*****************************************************************************
109 //
110 // Number of IOs (max. total of 32)
111 //
112 //*****************************************************************************
113 #define NUM_IO_MAX 32
114 
115 //*****************************************************************************
116 //
117 // The following fields are IO Id for the IOC module
118 //
119 //*****************************************************************************
120 #define IOID_0 0x00000000 // IO Id 0
121 #define IOID_1 0x00000001 // IO Id 1
122 #define IOID_2 0x00000002 // IO Id 2
123 #define IOID_3 0x00000003 // IO Id 3
124 #define IOID_4 0x00000004 // IO Id 4
125 #define IOID_5 0x00000005 // IO Id 5
126 #define IOID_6 0x00000006 // IO Id 6
127 #define IOID_7 0x00000007 // IO Id 7
128 #define IOID_8 0x00000008 // IO Id 8
129 #define IOID_9 0x00000009 // IO Id 9
130 #define IOID_10 0x0000000A // IO Id 10
131 #define IOID_11 0x0000000B // IO Id 11
132 #define IOID_12 0x0000000C // IO Id 12
133 #define IOID_13 0x0000000D // IO Id 13
134 #define IOID_14 0x0000000E // IO Id 14
135 #define IOID_15 0x0000000F // IO Id 15
136 #define IOID_16 0x00000010 // IO Id 16
137 #define IOID_17 0x00000011 // IO Id 17
138 #define IOID_18 0x00000012 // IO Id 18
139 #define IOID_19 0x00000013 // IO Id 19
140 #define IOID_20 0x00000014 // IO Id 20
141 #define IOID_21 0x00000015 // IO Id 21
142 #define IOID_22 0x00000016 // IO Id 22
143 #define IOID_23 0x00000017 // IO Id 23
144 #define IOID_24 0x00000018 // IO Id 24
145 #define IOID_25 0x00000019 // IO Id 25
146 #define IOID_26 0x0000001A // IO Id 26
147 #define IOID_27 0x0000001B // IO Id 27
148 #define IOID_28 0x0000001C // IO Id 28
149 #define IOID_29 0x0000001D // IO Id 29
150 #define IOID_30 0x0000001E // IO Id 30
151 #define IOID_31 0x0000001F // IO Id 31
152 #define IOID_UNUSED 0xFFFFFFFF // Unused IO Id
153 
154 #define IOC_IOID_MASK 0x000000FF // IOC IO Id bit mask
155 
156 //*****************************************************************************
157 //
158 // Number of IO ports
159 //
160 //*****************************************************************************
161 #define NUM_IO_PORTS 56
162 
163 //*****************************************************************************
164 //
165 // IOC Peripheral Port Mapping
166 //
167 //*****************************************************************************
168 #define IOC_PORT_GPIO 0x00000000 // Default general purpose IO usage
169 #define IOC_PORT_AON_CLK32K 0x00000007 // AON External 32kHz clock
170 #define IOC_PORT_AUX_IO 0x00000008 // AUX IO Pin
171 #define IOC_PORT_MCU_SSI0_RX 0x00000009 // MCU SSI0 Receive Pin
172 #define IOC_PORT_MCU_SSI0_TX 0x0000000A // MCU SSI0 Transmit Pin
173 #define IOC_PORT_MCU_SSI0_FSS 0x0000000B // MCU SSI0 FSS Pin
174 #define IOC_PORT_MCU_SSI0_CLK 0x0000000C // MCU SSI0 Clock Pin
175 #define IOC_PORT_MCU_I2C_MSSDA 0x0000000D // MCU I2C Data Pin
176 #define IOC_PORT_MCU_I2C_MSSCL 0x0000000E // MCU I2C Clock Pin
177 #define IOC_PORT_MCU_UART0_RX 0x0000000F // MCU UART0 Receive Pin
178 #define IOC_PORT_MCU_UART0_TX 0x00000010 // MCU UART0 Transmit Pin
179 #define IOC_PORT_MCU_UART0_CTS 0x00000011 // MCU UART0 Clear To Send Pin
180 #define IOC_PORT_MCU_UART0_RTS 0x00000012 // MCU UART0 Request To Send Pin
181 #define IOC_PORT_MCU_PORT_EVENT0 0x00000017 // MCU PORT EVENT 0
182 #define IOC_PORT_MCU_PORT_EVENT1 0x00000018 // MCU PORT EVENT 1
183 #define IOC_PORT_MCU_PORT_EVENT2 0x00000019 // MCU PORT EVENT 2
184 #define IOC_PORT_MCU_PORT_EVENT3 0x0000001A // MCU PORT EVENT 3
185 #define IOC_PORT_MCU_PORT_EVENT4 0x0000001B // MCU PORT EVENT 4
186 #define IOC_PORT_MCU_PORT_EVENT5 0x0000001C // MCU PORT EVENT 5
187 #define IOC_PORT_MCU_PORT_EVENT6 0x0000001D // MCU PORT EVENT 6
188 #define IOC_PORT_MCU_PORT_EVENT7 0x0000001E // MCU PORT EVENT 7
189 #define IOC_PORT_MCU_SWV 0x00000020 // Serial Wire Viewer
190 #define IOC_PORT_MCU_SSI1_RX 0x00000021 // MCU SSI1 Receive Pin
191 #define IOC_PORT_MCU_SSI1_TX 0x00000022 // MCU SSI1 Transmit Pin
192 #define IOC_PORT_MCU_SSI1_FSS 0x00000023 // MCU SSI1 FSS Pin
193 #define IOC_PORT_MCU_SSI1_CLK 0x00000024 // MCU SSI1 Clock Pin
194 #define IOC_PORT_MCU_I2S_AD0 0x00000025 // MCU I2S Data Pin 0
195 #define IOC_PORT_MCU_I2S_AD1 0x00000026 // MCU I2S Data Pin 1
196 #define IOC_PORT_MCU_I2S_WCLK 0x00000027 // MCU I2S Frame/Word Clock
197 #define IOC_PORT_MCU_I2S_BCLK 0x00000028 // MCU I2S Bit Clock
198 #define IOC_PORT_MCU_I2S_MCLK 0x00000029 // MCU I2S Master clock 2
199 #define IOC_PORT_RFC_TRC 0x0000002E // RF Core Tracer
200 #define IOC_PORT_RFC_GPO0 0x0000002F // RC Core Data Out Pin 0
201 #define IOC_PORT_RFC_GPO1 0x00000030 // RC Core Data Out Pin 1
202 #define IOC_PORT_RFC_GPO2 0x00000031 // RC Core Data Out Pin 2
203 #define IOC_PORT_RFC_GPO3 0x00000032 // RC Core Data Out Pin 3
204 #define IOC_PORT_RFC_GPI0 0x00000033 // RC Core Data In Pin 0
205 #define IOC_PORT_RFC_GPI1 0x00000034 // RC Core Data In Pin 1
206 
207 //*****************************************************************************
208 //
209 // Defines for enabling/disabling an IO
210 //
211 //*****************************************************************************
212 #define IOC_SLEW_ENABLE 0x00001000
213 #define IOC_SLEW_DISABLE 0x00000000
214 #define IOC_INPUT_ENABLE 0x20000000
215 #define IOC_INPUT_DISABLE 0x00000000
216 #define IOC_HYST_ENABLE 0x40000000
217 #define IOC_HYST_DISABLE 0x00000000
218 
219 //*****************************************************************************
220 //
221 // Values that can be used to set the shutdown mode of an IO
222 //
223 //*****************************************************************************
224 #define IOC_NO_WAKE_UP 0x00000000
225 #define IOC_WAKE_ON_LOW 0x10000000
226 #define IOC_WAKE_ON_HIGH 0x18000000
227 
228 //*****************************************************************************
229 //
230 // Values that can be used to set the IO Mode of an IO
231 //
232 //*****************************************************************************
233 #define IOC_IOMODE_NORMAL 0x00000000 // Normal Input/Output
234 #define IOC_IOMODE_INV 0x01000000 // Inverted Input/Output
235 #define IOC_IOMODE_OPEN_DRAIN_NORMAL \
236  0x04000000 // Open Drain, Normal Input/Output
237 #define IOC_IOMODE_OPEN_DRAIN_INV \
238  0x05000000 // Open Drain, Inverted
239  // Input/Output
240 #define IOC_IOMODE_OPEN_SRC_NORMAL \
241  0x06000000 // Open Source, Normal Input/Output
242 #define IOC_IOMODE_OPEN_SRC_INV \
243  0x07000000 // Open Source, Inverted
244  // Input/Output
245 
246 //*****************************************************************************
247 //
248 // Values that can be used to set the edge detection on an IO
249 //
250 //*****************************************************************************
251 #define IOC_NO_EDGE 0x00000000 // No edge detection
252 #define IOC_FALLING_EDGE 0x00010000 // Edge detection on falling edge
253 #define IOC_RISING_EDGE 0x00020000 // Edge detection on rising edge
254 #define IOC_BOTH_EDGES 0x00030000 // Edge detection on both edges
255 #define IOC_INT_ENABLE 0x00040000 // Enable interrupt on edge detect
256 #define IOC_INT_DISABLE 0x00000000 // Disable interrupt on edge detect
257 #define IOC_INT_M 0x00070000 // Int config mask
258 
259 //*****************************************************************************
260 //
261 // Values that be used to set pull on an IO
262 //
263 //*****************************************************************************
264 #define IOC_NO_IOPULL 0x00006000 // No IO pull
265 #define IOC_IOPULL_UP 0x00004000 // Pull up
266 #define IOC_IOPULL_DOWN 0x00002000 // Pull down
267 #define IOC_IOPULL_M 0x00006000 // Pull config mask
268 #define IOC_IOPULL_M 0x00006000
269 
270 //*****************************************************************************
271 //
272 // Values that can be used to select the drive strength of an IO
273 //
274 //*****************************************************************************
275 #define IOC_CURRENT_2MA 0x00000000 // 2mA drive strength
276 #define IOC_CURRENT_4MA 0x00000400 // 4mA drive strength
277 #define IOC_CURRENT_8MA 0x00000800 // 4 or 8mA drive strength
278 
279 #define IOC_STRENGTH_AUTO 0x00000000 // Automatic Drive Strength
280  // (2/4/8 mA @ VVDS)
281 #define IOC_STRENGTH_MAX 0x00000300 // Maximum Drive Strength
282  // (2/4/8 mA @ 1.8V)
283 #define IOC_STRENGTH_MED 0x00000200 // Medium Drive Strength
284  // (2/4/8 mA @ 2.5V)
285 #define IOC_STRENGTH_MIN 0x00000100 // Minimum Drive Strength
286  // (2/4/8 mA @ 3.3V)
287 //*****************************************************************************
288 //
289 // Defines for standard IO setup
290 //
291 //*****************************************************************************
292 #define IOC_STD_INPUT (IOC_CURRENT_2MA | IOC_STRENGTH_AUTO | \
293  IOC_NO_IOPULL | IOC_SLEW_DISABLE | \
294  IOC_HYST_DISABLE | IOC_NO_EDGE | \
295  IOC_INT_DISABLE | IOC_IOMODE_NORMAL | \
296  IOC_NO_WAKE_UP | IOC_INPUT_ENABLE )
297 #define IOC_STD_OUTPUT (IOC_CURRENT_2MA | IOC_STRENGTH_AUTO | \
298  IOC_NO_IOPULL | IOC_SLEW_DISABLE | \
299  IOC_HYST_DISABLE | IOC_NO_EDGE | \
300  IOC_INT_DISABLE | IOC_IOMODE_NORMAL | \
301  IOC_NO_WAKE_UP | IOC_INPUT_DISABLE )
302 
303 //*****************************************************************************
304 //
305 // API Functions and prototypes
306 //
307 //*****************************************************************************
308 
309 //*****************************************************************************
310 //
417 //
418 //*****************************************************************************
419 extern void IOCPortConfigureSet(uint32_t ui32IOId, uint32_t ui32PortId,
420  uint32_t ui32IOConfig);
421 
422 //*****************************************************************************
423 //
438 //
439 //*****************************************************************************
440 extern uint32_t IOCPortConfigureGet(uint32_t ui32IOId);
441 
442 //*****************************************************************************
443 //
458 //
459 //*****************************************************************************
460 extern void IOCIOShutdownSet(uint32_t ui32IOId, uint32_t ui32IOShutdown);
461 
462 
463 //*****************************************************************************
464 //
482 //
483 //*****************************************************************************
484 extern void IOCIOModeSet(uint32_t ui32IOId, uint32_t ui32IOMode);
485 
486 //*****************************************************************************
487 //
506 //
507 //*****************************************************************************
508 extern void IOCIOIntSet(uint32_t ui32IOId, uint32_t ui32Int,
509  uint32_t ui32EdgeDet);
510 
511 //*****************************************************************************
512 //
527 //
528 //*****************************************************************************
529 extern void IOCIOPortPullSet(uint32_t ui32IOId, uint32_t ui32Pull);
530 
531 //*****************************************************************************
532 //
546 //
547 //*****************************************************************************
548 extern void IOCIOHystSet(uint32_t ui32IOId, uint32_t ui32Hysteresis);
549 
550 //*****************************************************************************
551 //
565 //
566 //*****************************************************************************
567 extern void IOCIOInputSet(uint32_t ui32IOId, uint32_t ui32Input);
568 
569 //*****************************************************************************
570 //
584 //
585 //*****************************************************************************
586 extern void IOCIOSlewCtrlSet(uint32_t ui32IOId, uint32_t ui32SlewEnable);
587 
588 //*****************************************************************************
589 //
622 //
623 //*****************************************************************************
624 extern void IOCIODrvStrengthSet(uint32_t ui32IOId, uint32_t ui32IOCurrent,
625  uint32_t ui32DrvStrength);
626 
627 //*****************************************************************************
628 //
679 //
680 //*****************************************************************************
681 extern void IOCIOPortIdSet(uint32_t ui32IOId, uint32_t ui32PortId);
682 
683 //*****************************************************************************
684 //
699 //
700 //*****************************************************************************
701 __STATIC_INLINE void
702 IOCIntRegister(void (*pfnHandler)(void))
703 {
704  //
705  // Register the interrupt handler.
706  //
707  IntRegister(INT_AON_GPIO_EDGE, pfnHandler);
708 
709  //
710  // Enable the IO edge interrupt.
711  //
712  IntEnable(INT_AON_GPIO_EDGE);
713 }
714 
715 //*****************************************************************************
716 //
726 //
727 //*****************************************************************************
728 __STATIC_INLINE void
730 {
731  //
732  // Disable the interrupts.
733  //
734  IntDisable(INT_AON_GPIO_EDGE);
735 
736  //
737  // Unregister the interrupt handler.
738  //
739  IntUnregister(INT_AON_GPIO_EDGE);
740 }
741 
742 //*****************************************************************************
743 //
753 //
754 //*****************************************************************************
755 extern void IOCIntEnable(uint32_t ui32IOId);
756 
757 //*****************************************************************************
758 //
771 //
772 //*****************************************************************************
773 extern void IOCIntDisable(uint32_t ui32IOId);
774 
775 //*****************************************************************************
776 //
804 //
805 //*****************************************************************************
806 __STATIC_INLINE void
807 IOCIntClear(uint32_t ui32IOId)
808 {
809  //
810  // Check the arguments.
811  //
812  ASSERT(ui32IOId <= IOID_31);
813 
814  //
815  // Clear the requested interrupt source by clearing the event.
816  //
817  GPIO_clearEventDio(ui32IOId);
818 }
819 
820 //*****************************************************************************
821 //
830 //
831 //*****************************************************************************
832 __STATIC_INLINE uint32_t
833 IOCIntStatus(uint32_t ui32IOId)
834 {
835  //
836  // Check the arguments.
837  //
838  ASSERT(ui32IOId <= IOID_31);
839 
840  //
841  // Get the event status.
842  //
843  return (GPIO_getEventDio(ui32IOId));
844 }
845 
846 
847 //*****************************************************************************
848 //
872 //
873 //*****************************************************************************
874 extern void IOCPinTypeGpioInput(uint32_t ui32IOId);
875 
876 //*****************************************************************************
877 //
901 //
902 //*****************************************************************************
903 extern void IOCPinTypeGpioOutput(uint32_t ui32IOId);
904 
905 //*****************************************************************************
906 //
940 //
941 //*****************************************************************************
942 extern void IOCPinTypeUart(uint32_t ui32Base, uint32_t ui32Rx,
943  uint32_t ui32Tx, uint32_t ui32Cts,
944  uint32_t ui32Rts);
945 
946 //*****************************************************************************
947 //
973 //
974 //*****************************************************************************
975 extern void IOCPinTypeSsiMaster(uint32_t ui32Base, uint32_t ui32Rx,
976  uint32_t ui32Tx, uint32_t ui32Fss,
977  uint32_t ui32Clk);
978 
979 //*****************************************************************************
980 //
1002 //
1003 //*****************************************************************************
1004 extern void IOCPinTypeSsiSlave(uint32_t ui32Base, uint32_t ui32Rx,
1005  uint32_t ui32Tx, uint32_t ui32Fss,
1006  uint32_t ui32Clk);
1007 
1008 //*****************************************************************************
1009 //
1025 //
1026 //*****************************************************************************
1027 extern void IOCPinTypeI2c(uint32_t ui32Base, uint32_t ui32Data,
1028  uint32_t ui32Clk);
1029 
1030 
1031 //*****************************************************************************
1032 //
1049 //
1050 //*****************************************************************************
1051 extern void IOCPinTypeAux(uint32_t ui32IOId);
1052 
1053 //*****************************************************************************
1054 //
1055 // Support for DriverLib in ROM:
1056 // Redirect to implementation in ROM when available.
1057 //
1058 //*****************************************************************************
1059 #if !defined(DRIVERLIB_NOROM) && !defined(DOXYGEN)
1060  #include <driverlib/rom.h>
1061  #ifdef ROM_IOCPortConfigureSet
1062  #undef IOCPortConfigureSet
1063  #define IOCPortConfigureSet ROM_IOCPortConfigureSet
1064  #endif
1065  #ifdef ROM_IOCPortConfigureGet
1066  #undef IOCPortConfigureGet
1067  #define IOCPortConfigureGet ROM_IOCPortConfigureGet
1068  #endif
1069  #ifdef ROM_IOCIOShutdownSet
1070  #undef IOCIOShutdownSet
1071  #define IOCIOShutdownSet ROM_IOCIOShutdownSet
1072  #endif
1073  #ifdef ROM_IOCIOModeSet
1074  #undef IOCIOModeSet
1075  #define IOCIOModeSet ROM_IOCIOModeSet
1076  #endif
1077  #ifdef ROM_IOCIOIntSet
1078  #undef IOCIOIntSet
1079  #define IOCIOIntSet ROM_IOCIOIntSet
1080  #endif
1081  #ifdef ROM_IOCIOPortPullSet
1082  #undef IOCIOPortPullSet
1083  #define IOCIOPortPullSet ROM_IOCIOPortPullSet
1084  #endif
1085  #ifdef ROM_IOCIOHystSet
1086  #undef IOCIOHystSet
1087  #define IOCIOHystSet ROM_IOCIOHystSet
1088  #endif
1089  #ifdef ROM_IOCIOInputSet
1090  #undef IOCIOInputSet
1091  #define IOCIOInputSet ROM_IOCIOInputSet
1092  #endif
1093  #ifdef ROM_IOCIOSlewCtrlSet
1094  #undef IOCIOSlewCtrlSet
1095  #define IOCIOSlewCtrlSet ROM_IOCIOSlewCtrlSet
1096  #endif
1097  #ifdef ROM_IOCIODrvStrengthSet
1098  #undef IOCIODrvStrengthSet
1099  #define IOCIODrvStrengthSet ROM_IOCIODrvStrengthSet
1100  #endif
1101  #ifdef ROM_IOCIOPortIdSet
1102  #undef IOCIOPortIdSet
1103  #define IOCIOPortIdSet ROM_IOCIOPortIdSet
1104  #endif
1105  #ifdef ROM_IOCIntEnable
1106  #undef IOCIntEnable
1107  #define IOCIntEnable ROM_IOCIntEnable
1108  #endif
1109  #ifdef ROM_IOCIntDisable
1110  #undef IOCIntDisable
1111  #define IOCIntDisable ROM_IOCIntDisable
1112  #endif
1113  #ifdef ROM_IOCPinTypeGpioInput
1114  #undef IOCPinTypeGpioInput
1115  #define IOCPinTypeGpioInput ROM_IOCPinTypeGpioInput
1116  #endif
1117  #ifdef ROM_IOCPinTypeGpioOutput
1118  #undef IOCPinTypeGpioOutput
1119  #define IOCPinTypeGpioOutput ROM_IOCPinTypeGpioOutput
1120  #endif
1121  #ifdef ROM_IOCPinTypeUart
1122  #undef IOCPinTypeUart
1123  #define IOCPinTypeUart ROM_IOCPinTypeUart
1124  #endif
1125  #ifdef ROM_IOCPinTypeSsiMaster
1126  #undef IOCPinTypeSsiMaster
1127  #define IOCPinTypeSsiMaster ROM_IOCPinTypeSsiMaster
1128  #endif
1129  #ifdef ROM_IOCPinTypeSsiSlave
1130  #undef IOCPinTypeSsiSlave
1131  #define IOCPinTypeSsiSlave ROM_IOCPinTypeSsiSlave
1132  #endif
1133  #ifdef ROM_IOCPinTypeI2c
1134  #undef IOCPinTypeI2c
1135  #define IOCPinTypeI2c ROM_IOCPinTypeI2c
1136  #endif
1137  #ifdef ROM_IOCPinTypeAux
1138  #undef IOCPinTypeAux
1139  #define IOCPinTypeAux ROM_IOCPinTypeAux
1140  #endif
1141 #endif
1142 
1143 //*****************************************************************************
1144 //
1145 // Mark the end of the C bindings section for C++ compilers.
1146 //
1147 //*****************************************************************************
1148 #ifdef __cplusplus
1149 }
1150 #endif
1151 
1152 #endif // __IOC_H__
1153 
1154 //*****************************************************************************
1155 //
1159 //
1160 //*****************************************************************************
static uint32_t GPIO_getEventDio(uint32_t dioNumber)
Gets the event status of a specific DIO.
Definition: gpio.h:584
void IOCIntDisable(uint32_t ui32IOId)
Disables individual IO edge interrupt sources.
Definition: ioc.c:474
void IOCIOSlewCtrlSet(uint32_t ui32IOId, uint32_t ui32SlewEnable)
Enable/disable the slew control on an IO port.
Definition: ioc.c:347
void IOCPinTypeSsiMaster(uint32_t ui32Base, uint32_t ui32Rx, uint32_t ui32Tx, uint32_t ui32Fss, uint32_t ui32Clk)
Configure a set of IOs for standard SSI peripheral master control.
Definition: ioc.c:590
void IOCPinTypeI2c(uint32_t ui32Base, uint32_t ui32Data, uint32_t ui32Clk)
Configure a set of IOs for standard I2C peripheral control.
Definition: ioc.c:714
void IOCIOShutdownSet(uint32_t ui32IOId, uint32_t ui32IOShutdown)
Set wake-up on an IO port.
Definition: ioc.c:150
static void GPIO_clearEventDio(uint32_t dioNumber)
Clears the IO event status of a specific DIO.
Definition: gpio.h:644
void IOCPinTypeSsiSlave(uint32_t ui32Base, uint32_t ui32Rx, uint32_t ui32Tx, uint32_t ui32Fss, uint32_t ui32Clk)
Configure a set of IOs for standard SSI peripheral slave control.
Definition: ioc.c:652
void IOCIOHystSet(uint32_t ui32IOId, uint32_t ui32Hysteresis)
Configure hysteresis on and IO port.
Definition: ioc.c:285
void IOCIOInputSet(uint32_t ui32IOId, uint32_t ui32Input)
Enable/disable IO port as input.
Definition: ioc.c:316
void IOCIntEnable(uint32_t ui32IOId)
Enables individual IO edge detect interrupt.
Definition: ioc.c:445
static uint32_t IOCIntStatus(uint32_t ui32IOId)
Returns the status of the IO interrupts.
Definition: ioc.h:833
void IOCIODrvStrengthSet(uint32_t ui32IOId, uint32_t ui32IOCurrent, uint32_t ui32DrvStrength)
Configure the drive strength source and current mode of an IO port.
Definition: ioc.c:378
void IOCPinTypeAux(uint32_t ui32IOId)
Configure an IO for AUX control.
Definition: ioc.c:746
void IOCIOIntSet(uint32_t ui32IOId, uint32_t ui32Int, uint32_t ui32EdgeDet)
Setup interrupt detection on an IO Port.
Definition: ioc.c:218
#define ASSERT(expr)
Definition: debug.h:74
uint32_t IOCPortConfigureGet(uint32_t ui32IOId)
Get the configuration of an IO port.
Definition: ioc.c:124
void IOCPortConfigureSet(uint32_t ui32IOId, uint32_t ui32PortId, uint32_t ui32IOConfig)
Set the configuration of an IO port.
Definition: ioc.c:96
void IOCPinTypeGpioOutput(uint32_t ui32IOId)
Setup an IO for standard GPIO output.
Definition: ioc.c:527
static void IOCIntUnregister(void)
Unregisters an interrupt handler for a IO edge interrupt.
Definition: ioc.h:729
void IOCIOPortIdSet(uint32_t ui32IOId, uint32_t ui32PortId)
Setup the Port ID for this IO.
Definition: ioc.c:415
void IOCPinTypeGpioInput(uint32_t ui32IOId)
Setup an IO for standard GPIO input.
Definition: ioc.c:503
void IntUnregister(uint32_t ui32Interrupt)
Unregisters the function to be called when an interrupt occurs.
Definition: interrupt.c:200
static void IOCIntClear(uint32_t ui32IOId)
Clears the IO edge interrupt source.
Definition: ioc.h:807
#define IOID_31
Definition: ioc.h:151
void IOCPinTypeUart(uint32_t ui32Base, uint32_t ui32Rx, uint32_t ui32Tx, uint32_t ui32Cts, uint32_t ui32Rts)
Configure a set of IOs for standard UART peripheral control.
Definition: ioc.c:551
void IOCIOModeSet(uint32_t ui32IOId, uint32_t ui32IOMode)
Set the IO Mode of an IO Port.
Definition: ioc.c:183
void IntDisable(uint32_t ui32Interrupt)
Disables an interrupt.
Definition: interrupt.c:378
void IntRegister(uint32_t ui32Interrupt, void(*pfnHandler)(void))
Registers a function to be called when an interrupt occurs.
Definition: interrupt.c:152
static void IOCIntRegister(void(*pfnHandler)(void))
Register an interrupt handler for an IO edge interrupt.
Definition: ioc.h:702
void IOCIOPortPullSet(uint32_t ui32IOId, uint32_t ui32Pull)
Set the pull on an IO port.
Definition: ioc.c:253
void IntEnable(uint32_t ui32Interrupt)
Enables an interrupt.
Definition: interrupt.c:318