![]() |
![]() |
TI-RTOS Drivers
tidrivers_tivac_2_16_01_13
|
SPITivaDMA Hardware attributes. More...
#include <SPITivaDMA.h>
Data Fields | |
SPIBaseAddrType | baseAddr |
unsigned int | intNum |
uint32_t | intPriority |
uint32_t * | scratchBufPtr |
uint32_t | defaultTxBufValue |
uint32_t | rxChannelIndex |
uint32_t | txChannelIndex |
void(* | channelMappingFxn )(SPIDataType) |
uint32_t | rxChannelMappingFxnArg |
uint32_t | txChannelMappingFxnArg |
SPITivaDMA Hardware attributes.
These fields, with the exception of intPriority, are used by driverlib APIs and therefore must be populated by driverlib macro definitions. For TivaWare these definitions are found in:
intPriority is the SPI peripheral's interrupt priority, as defined by the underlying OS. It is passed unmodified to the underlying OS's interrupt handler creation code, so you need to refer to the OS documentation for usage. For example, for SYS/BIOS applications, refer to the ti.sysbios.family.arm.m3.Hwi documentation for SYS/BIOS usage of interrupt priorities. If the driver uses the ti.drivers.ports interface instead of making OS calls directly, then the HwiP port handles the interrupt priority in an OS specific way. In the case of the SYS/BIOS port, intPriority is passed unmodified to Hwi_create().
A sample structure is shown below:
SPIBaseAddrType SPITivaDMA_HWAttrs::baseAddr |
SSI Peripheral's base address
unsigned int SPITivaDMA_HWAttrs::intNum |
SSI TivaDMA Peripheral's interrupt vector
uint32_t SPITivaDMA_HWAttrs::intPriority |
SPITivaDMA Peripheral's interrupt priority
uint32_t* SPITivaDMA_HWAttrs::scratchBufPtr |
Address of a scratch buffer of size uint32_t
uint32_t SPITivaDMA_HWAttrs::defaultTxBufValue |
Default TX value if txBuf == NULL
uint32_t SPITivaDMA_HWAttrs::rxChannelIndex |
uDMA controlTable channel index
uint32_t SPITivaDMA_HWAttrs::txChannelIndex |
uDMA controlTable channel index
void(* SPITivaDMA_HWAttrs::channelMappingFxn) (SPIDataType) |
uDMA mapping function that maps the SPI trigger to the DMA channel
uint32_t SPITivaDMA_HWAttrs::rxChannelMappingFxnArg |
uDMA MappingFxn arg to map the Tx channel
uint32_t SPITivaDMA_HWAttrs::txChannelMappingFxnArg |
uDMA MappingFxn arg to map the Rx channel