![]() |
![]() |
TI-RTOS Drivers
tidrivers_tivac_2_16_01_13
|
![]() |
Macros | |
#define | PWM_STATUS_SUCCESS 0 |
Successful status code returned by PWM_control(). More... | |
#define | PWM_STATUS_ERROR -1 |
Generic error status code returned by PWM_control(). More... | |
#define | PWM_STATUS_UNDEFINEDCMD -2 |
An error status code returned by PWM_control() for undefined command codes. More... | |
PWM_STATUS_* macros are general status codes returned by PWM_control()
PWMTimerTiva_STATUS_* macros are command codes only defined in the PWMTimerTiva.h driver implementation and need to:
PWMTiva_STATUS_* macros are command codes only defined in the PWMTiva.h driver implementation and need to:
#define PWM_STATUS_SUCCESS 0 |
Successful status code returned by PWM_control().
PWM_control() returns PWM_STATUS_SUCCESS if the control code was executed successfully.
#define PWM_STATUS_ERROR -1 |
Generic error status code returned by PWM_control().
PWM_control() returns PWM_STATUS_ERROR if the control code was not executed successfully.
#define PWM_STATUS_UNDEFINEDCMD -2 |
An error status code returned by PWM_control() for undefined command codes.
PWM_control() returns PWM_STATUS_UNDEFINEDCMD if the control code is not recognized by the driver implementation.