![]() |
![]() |
TI-RTOS Drivers
tidrivers_msp43x_2_16_01_13
|
SPIMSP432DMA Hardware attributes These fields, with the exception of intPriority, are used by driverlib APIs and therefore must be populated by driverlib macro definitions. For MSP430Ware these definitions are found in: More...
#include <SPIMSP432DMA.h>
Data Fields | |
uint32_t | baseAddr |
uint16_t | bitOrder |
uint8_t | clockSource |
uint8_t | defaultTxBufValue |
uint8_t | dmaIntNum |
uint32_t | intPriority |
uint32_t | rxDMAChannelIndex |
uint32_t | txDMAChannelIndex |
SPIMSP432DMA Hardware attributes These fields, with the exception of intPriority, are used by driverlib APIs and therefore must be populated by driverlib macro definitions. For MSP430Ware these definitions are found in:
intPriority is the SPI peripheral's interrupt priority, as defined by the underlying OS. It is passed unmodified to the underlying OS's interrupt handler creation code, so you need to refer to the OS documentation for usage. For example, for SYS/BIOS applications, refer to the ti.sysbios.family.arm.m3.Hwi documentation for SYS/BIOS usage of interrupt priorities. If the driver uses the ti.drivers.ports interface instead of making OS calls directly, then the HwiP port handles the interrupt priority in an OS specific way. In the case of the SYS/BIOS port, intPriority is passed unmodified to Hwi_create().
A sample structure is shown below:
uint32_t SPIMSP432DMA_HWAttrs::baseAddr |
EUSCI_B_SPI Peripheral's base address
uint16_t SPIMSP432DMA_HWAttrs::bitOrder |
EUSCI_B_SPI Bit order
uint8_t SPIMSP432DMA_HWAttrs::clockSource |
EUSCI_B_SPI Clock source
uint8_t SPIMSP432DMA_HWAttrs::defaultTxBufValue |
uint8_t SPIMSP432DMA_HWAttrs::dmaIntNum |
Default TX value if txBuf == NULL DMA interrupt number
uint32_t SPIMSP432DMA_HWAttrs::intPriority |
DMA interrupt priority
uint32_t SPIMSP432DMA_HWAttrs::rxDMAChannelIndex |
DMA rxDMAChannel for Rx data
uint32_t SPIMSP432DMA_HWAttrs::txDMAChannelIndex |
DMA txDMAChannel for Tx data