![]() |
![]() |
TI-RTOS Drivers
tidrivers_msp43x_2_16_01_13
|
![]() |
Macros | |
#define | UART_STATUS_SUCCESS 0 |
Successful status code returned by UART_control(). More... | |
#define | UART_STATUS_ERROR -1 |
Generic error status code returned by UART_control(). More... | |
#define | UART_STATUS_UNDEFINEDCMD -2 |
An error status code returned by UART_control() for undefined command codes. More... | |
UART_STATUS_* macros are general status codes returned by UART_control()
UARTEUSCIA_STATUS_* macros are command codes only defined in the UARTEUSCIA.h driver implementation and need to:
UARTMSP432_STATUS_* macros are command codes only defined in the UARTMSP432.h driver implementation and need to:
UARTUSCIA_STATUS_* macros are command codes only defined in the UARTUSCIA.h driver implementation and need to:
#define UART_STATUS_SUCCESS 0 |
Successful status code returned by UART_control().
UART_control() returns UART_STATUS_SUCCESS if the control code was executed successfully.
#define UART_STATUS_ERROR -1 |
Generic error status code returned by UART_control().
UART_control() returns UART_STATUS_ERROR if the control code was not executed successfully.
#define UART_STATUS_UNDEFINEDCMD -2 |
An error status code returned by UART_control() for undefined command codes.
UART_control() returns UART_STATUS_UNDEFINEDCMD if the control code is not recognized by the driver implementation.