![]() |
![]() |
TI-RTOS Drivers
tidrivers_msp43x_2_16_01_13
|
USBMSCHFatFs driver interface.
============================================================================
The USBMSCHFatFs header file should be included in an application as follows:
The USBMSCHFatFs driver is a driver designed to hook into FatFs. It implements a set of functions that FatFs needs to call to perform basic block data transfers.
This driver is designed to work with the USB Library. Because it is running in host mode, we need to add protection when accessing the USB Library. A gate was added to prevent the task servicing the USB library to preempt any other task accessing the USB Library.
Once the driver has been opened, the application may used the FatFs APIs or the standard C runtime file I/O calls (fopen, fclose, etc...). Once the driver has been closed, ensure the application does NOT make any file I/O calls.
This module serves as the main interface for TI-RTOS applications. Its purpose is to redirect the module's APIs to specific peripheral implementations which are specified using a pointer to a USBMSCHFatFs_FxnTable.
The USBMSCHFatFs driver interface module is joined (at link time) to a NULL-terminated array of USBMSCHFatFs_Config data structures named USBMSCHFatFs_config. USBMSCHFatFs_config is implemented in the application with each entry being an instance of a USBMSCHFatFs peripheral. Each entry in USBMSCHFatFs_config contains a:
The USBMSCHFatFs driver interface produces log statements if instrumentation is enabled.
Diagnostics Mask | Log details |
---|---|
Diags_USER1 | basic operations performed |
Diags_USER2 | detailed operations performed |
#include <stddef.h>
#include <stdint.h>
#include <stdbool.h>
Go to the source code of this file.
Data Structures | |
struct | USBMSCHFatFs_Params |
USBMSCHFatFs Parameters. More... | |
struct | USBMSCHFatFs_FxnTable |
The definition of a USBMSCHFatFs function table that contains the required set of functions to control a specific USBMSCHFatFs driver implementation. More... | |
struct | USBMSCHFatFs_Config |
USBMSCHFatFs Global configuration. More... | |
Macros | |
#define | USBMSCHFatFs_CMD_RESERVED 32 |
#define | USBMSCHFatFs_STATUS_RESERVED -32 |
#define | USBMSCHFatFs_STATUS_SUCCESS 0 |
Successful status code returned by USBMSCHFatFs_control(). More... | |
#define | USBMSCHFatFs_STATUS_ERROR -1 |
Generic error status code returned by USBMSCHFatFs_control(). More... | |
#define | USBMSCHFatFs_STATUS_UNDEFINEDCMD -2 |
An error status code returned by USBMSCHFatFs_control() for undefined command codes. More... | |
Typedefs | |
typedef struct USBMSCHFatFs_Config * | USBMSCHFatFs_Handle |
USBMSCHFatFs Handler. More... | |
typedef struct USBMSCHFatFs_Params | USBMSCHFatFs_Params |
USBMSCHFatFs Parameters. More... | |
typedef void(* | USBMSCHFatFs_InitFxn) (USBMSCHFatFs_Handle handle) |
A function pointer to a driver specific implementation of USBMSCHFatFs_init(). More... | |
typedef USBMSCHFatFs_Handle(* | USBMSCHFatFs_OpenFxn) (USBMSCHFatFs_Handle handle, unsigned char drv, USBMSCHFatFs_Params *params) |
A function pointer to a driver specific implementation of USBMSCHFatFs_open(). More... | |
typedef void(* | USBMSCHFatFs_CloseFxn) (USBMSCHFatFs_Handle handle) |
A function pointer to a driver specific implementation of USBMSCHFatFs_close(). More... | |
typedef int(* | USBMSCHFatFs_ControlFxn) (USBMSCHFatFs_Handle handle, unsigned int cmd, void *arg) |
A function pointer to a driver specific implementation of USBMSCHFatFs_control(). More... | |
typedef bool(* | USBMSCHFatFs_waitForconnectFxn) (USBMSCHFatFs_Handle handle, unsigned int timeout) |
A function pointer to a driver specific implementation of USBMSCHFatFs_waitForConnect(). More... | |
typedef struct USBMSCHFatFs_FxnTable | USBMSCHFatFs_FxnTable |
The definition of a USBMSCHFatFs function table that contains the required set of functions to control a specific USBMSCHFatFs driver implementation. More... | |
typedef struct USBMSCHFatFs_Config | USBMSCHFatFs_Config |
USBMSCHFatFs Global configuration. More... | |
Functions | |
void | USBMSCHFatFs_close (USBMSCHFatFs_Handle handle) |
Function to closes a given USBMSCHFatFs peripheral specified by the USBMSCHFatFs handle. This function unmounts the file system mounted by USBMSCHFatFs_open and unregisters the USBMSCHFatFs driver from BIOS' FatFs module. More... | |
int | USBMSCHFatFs_control (USBMSCHFatFs_Handle handle, unsigned int cmd, void *arg) |
Function performs implementation specific features on a given USBMSCHFatFs_Handle. More... | |
void | USBMSCHFatFs_init (void) |
Function to initialize the USBMSCHFatFs module. More... | |
USBMSCHFatFs_Handle | USBMSCHFatFs_open (unsigned int index, unsigned char drv, USBMSCHFatFs_Params *params) |
This function registers the USBMSCHFatFs driver with BIOS' FatFs module and mounts the FatFs file system. More... | |
void | USBMSCHFatFs_Params_init (USBMSCHFatFs_Params *params) |
Function to initialize the USBMSCHFatFs_Params structure to its defaults. More... | |
bool | USBMSCHFatFs_waitForConnect (USBMSCHFatFs_Handle handle, unsigned int timeout) |
Function blocks task execution while no USB drive is enumerated. After the USBMSCHFatFs driver has been opened this functino is used to determine when a USB drive is has been enumerated. More... | |
typedef struct USBMSCHFatFs_Config* USBMSCHFatFs_Handle |
USBMSCHFatFs Handler.
typedef struct USBMSCHFatFs_Params USBMSCHFatFs_Params |
USBMSCHFatFs Parameters.
USBMSCHFatFs parameters are used to with the USBMSCHFatFs_open() call. Default values for these parameters are set using USBMSCHFatFs_Params_init().
typedef void(* USBMSCHFatFs_InitFxn) (USBMSCHFatFs_Handle handle) |
A function pointer to a driver specific implementation of USBMSCHFatFs_init().
typedef USBMSCHFatFs_Handle(* USBMSCHFatFs_OpenFxn) (USBMSCHFatFs_Handle handle, unsigned char drv, USBMSCHFatFs_Params *params) |
A function pointer to a driver specific implementation of USBMSCHFatFs_open().
typedef void(* USBMSCHFatFs_CloseFxn) (USBMSCHFatFs_Handle handle) |
A function pointer to a driver specific implementation of USBMSCHFatFs_close().
typedef int(* USBMSCHFatFs_ControlFxn) (USBMSCHFatFs_Handle handle, unsigned int cmd, void *arg) |
A function pointer to a driver specific implementation of USBMSCHFatFs_control().
typedef bool(* USBMSCHFatFs_waitForconnectFxn) (USBMSCHFatFs_Handle handle, unsigned int timeout) |
A function pointer to a driver specific implementation of USBMSCHFatFs_waitForConnect().
typedef struct USBMSCHFatFs_FxnTable USBMSCHFatFs_FxnTable |
The definition of a USBMSCHFatFs function table that contains the required set of functions to control a specific USBMSCHFatFs driver implementation.
typedef struct USBMSCHFatFs_Config USBMSCHFatFs_Config |
USBMSCHFatFs Global configuration.
The USBMSCHFatFs_Config structure contains a set of pointers used to characterize the USBMSCHFatFs driver implementation.
This structure needs to be defined before calling USBMSCHFatFs_init() and it must not be changed thereafter.
void USBMSCHFatFs_close | ( | USBMSCHFatFs_Handle | handle | ) |
Function to closes a given USBMSCHFatFs peripheral specified by the USBMSCHFatFs handle. This function unmounts the file system mounted by USBMSCHFatFs_open and unregisters the USBMSCHFatFs driver from BIOS' FatFs module.
handle | A USBMSCHFatFs_Handle returned from USBMSCHFatFs_open |
int USBMSCHFatFs_control | ( | USBMSCHFatFs_Handle | handle, |
unsigned int | cmd, | ||
void * | arg | ||
) |
Function performs implementation specific features on a given USBMSCHFatFs_Handle.
Commands for USBMSCHFatFs_control can originate from USBMSCHFatFs.h or from implementation specific USBMSCHFatFs*.h (USBMSCHFatFsTiva.h, etc.. ) files. While commands from USBMSCHFatFs.h are API portable across driver implementations, not all implementations may support all these commands. Conversely, commands from driver implementation specific USBMSCHFatFs*.h files add unique driver capabilities but are not API portable across all USBMSCHFatFs driver implementations.
Commands supported by USBMSCHFatFs.h follow a USBMSCHFatFs_CMD_<cmd> naming convention.
Commands supported by USBMSCHFatFs*.h follow a USBMSCHFatFs*_CMD_<cmd> naming convention.
Each control command defines arg differently. The types of arg are documented with each command.
See USBMSCHFatFs_control command codes for command codes.
See USBMSCHFatFs_control return status codes for status codes.
handle | A USBMSCHFatFs handle returned from USBMSCHFatFs_open() |
cmd | USBMSCHFatFs.h or USBMSCHFatFs*.h commands. |
arg | An optional R/W (read/write) command argument accompanied with cmd |
void USBMSCHFatFs_init | ( | void | ) |
Function to initialize the USBMSCHFatFs module.
USBMSCHFatFs_Handle USBMSCHFatFs_open | ( | unsigned int | index, |
unsigned char | drv, | ||
USBMSCHFatFs_Params * | params | ||
) |
This function registers the USBMSCHFatFs driver with BIOS' FatFs module and mounts the FatFs file system.
index | Logical peripheral number for the USBMSCHFatFs indexed into the USBMSCHFatFs_config table |
drv | Drive number to be associated with the USBMSCHFatFs FatFs driver |
params | Pointer to an parameter block, if NULL it will use default values. All the fields in this structure are RO (read-only). |
void USBMSCHFatFs_Params_init | ( | USBMSCHFatFs_Params * | params | ) |
Function to initialize the USBMSCHFatFs_Params structure to its defaults.
params | An pointer to USBMSCHFatFs_Params structure for initialization |
Defaults values are: servicePriority = Task_numPriorities - 1;
bool USBMSCHFatFs_waitForConnect | ( | USBMSCHFatFs_Handle | handle, |
unsigned int | timeout | ||
) |
Function blocks task execution while no USB drive is enumerated. After the USBMSCHFatFs driver has been opened this functino is used to determine when a USB drive is has been enumerated.
handle | A USBMSCHFatFs handle |
timeout | Timeout period in system ticks for the task to block |