![]() |
![]() |
TI-RTOS Drivers
tidrivers_c2000_2_16_01_13
|
EMACTiva Driver.
============================================================================
The EMACTiva header file should be included in an application as follows:
Refer to EMAC.h for a complete description of APIs.
The EMACTiva driver produces log statements using the instrumented library. The following masks are used:
#include <stdint.h>
#include <ti/sysbios/knl/Swi.h>
#include <ti/ndk/inc/stkmain.h>
Go to the source code of this file.
Data Structures | |
struct | EMACTiva_HWAttrs |
EMACTiva Hardware attributes. More... | |
struct | EMACTiva_Object |
EMACTiva Object. More... | |
Macros | |
#define | _INCLUDE_NIMU_CODE |
Typedefs | |
typedef struct EMACTiva_HWAttrs | EMACTiva_HWAttrs |
EMACTiva Hardware attributes. More... | |
typedef struct EMACTiva_Object | EMACTiva_Object |
EMACTiva Object. More... | |
Functions | |
void | EMACTiva_init (uint32_t index) |
This function sets the EMACTiva driver. More... | |
bool | EMACTiva_isLinkUp (uint32_t index) |
This function returns if the link is up. More... | |
int | EMACTiva_NIMUInit (STKEVENT_Handle hEvent) |
This function is needed in the NIMUDeviceTable that is required by the NDK. More... | |
Variables | |
const EMAC_FxnTable | EMACTiva_fxnTable |
EMACTiva function table. More... | |
#define _INCLUDE_NIMU_CODE |
typedef struct EMACTiva_HWAttrs EMACTiva_HWAttrs |
EMACTiva Hardware attributes.
intPriority is the EMAC peripheral's interrupt priority, as defined by the underlying OS. It is passed unmodified to the underlying OS's interrupt handler creation code, so you need to refer to the OS documentation for usage. For example, for SYS/BIOS applications, refer to the ti.sysbios.family.arm.m3.Hwi documentation for SYS/BIOS usage of interrupt priorities. If the driver uses the ti.drivers.ports interface instead of making OS calls directly, then the HwiP port handles the interrupt priority in an OS specific way. In the case of the SYS/BIOS port, intPriority is passed unmodified to Hwi_create().
typedef struct EMACTiva_Object EMACTiva_Object |
EMACTiva Object.
This structure should not be directly accessed. It is specified here to allow the application to supply the needed memory to the EMACTiva module.
void EMACTiva_init | ( | uint32_t | index | ) |
This function sets the EMACTiva driver.
This function must be called before the NDK stack thread is started.
The EMAC_config structure must be present and initialized before this function is called.
bool EMACTiva_isLinkUp | ( | uint32_t | index | ) |
This function returns if the link is up.
int EMACTiva_NIMUInit | ( | STKEVENT_Handle | hEvent | ) |
This function is needed in the NIMUDeviceTable that is required by the NDK.
const EMAC_FxnTable EMACTiva_fxnTable |
EMACTiva function table.