![]() |
![]() |
Functions | |
_extern int | MLDTestGroup (NETIF_DEVICE *ptr_device, IP6N multicast_address) |
_extern int | MLDJoinGroup (NETIF_DEVICE *ptr_device, IP6N multicast_address) |
_extern int | MLDLeaveGroup (NETIF_DEVICE *ptr_device, IP6N multicast_address) |
_extern int MLDJoinGroup | ( | NETIF_DEVICE * | ptr_device, | |
IP6N | multicast_address | |||
) |
Description
This function is used to join a multicast group over a specific interface.
This is for *internal* NDK Stack Usage.
[in] | ptr_device | The pointer to the NIMU Network Interface object over which the multicast address is being joined. |
[in] | multicast_address | IPv6 Multicast address being joined. |
0 | - Success | |
<0 | - Error |
_extern int MLDLeaveGroup | ( | NETIF_DEVICE * | ptr_device, | |
IP6N | multicast_address | |||
) |
Description
This function is used to leave a multicast group over a specific interface.
This is for *internal* NDK Stack Usage.
[in] | ptr_device | The pointer to the NIMU Network Interface object over which the multicast address is being left. |
[in] | multicast_address | IPv6 Multicast address being left. |
0 | - Success | |
<0 | - Error |
_extern int MLDTestGroup | ( | NETIF_DEVICE * | ptr_device, | |
IP6N | multicast_address | |||
) |
Description
This function is called from the IPv6 Stack receive handler to verify if the address specified here has been joined or not?
This is for *internal* NDK Stack Usage.
[in] | ptr_device | Pointer to the Network Interface object on which the IPv6 packet was rxed. |
[in] | multicast_address | This is the IPAddress from the Destination field of the IPv6 Packet. |
1 | - Multicast Group has been joined | |
0 | - The group has not been joined. |