![]() |
![]() |
Functions | |
HANDLE | IPv6GetRoute (IP6N DstIP) |
int | IPv6TxPacket (PBM_Pkt *pPkt, UINT32 Flags) |
HANDLE IPv6GetRoute | ( | IP6N | DstIP | ) |
Description
The function is used to get an IPv6 route matching the destination IP Address. The function increments the reference counter for the ROUTE6 object.
This is for *internal* NDK Stack Usage.
[in] | DstIP | IPv6 Destination IP address we are trying to find a route for. |
Success | - Handle of the Route6 object to be used. | |
Error | - 0 |
int IPv6TxPacket | ( | PBM_Pkt * | pPkt, | |
UINT32 | Flags | |||
) |
Description
The function is used to transmit an IPv6 packet.
This is for *internal* NDK Stack Usage.
[in] | pPkt | Pointer to the IPv6 packet which needs to be transmitted |
[in] | Flags | Flags which need to be worked out. (Placeholder) |
Success | - 0 | |
Error | - <0 |