#include <rf_ble_cmd.h>
Data Fields | |
dataQueue_t * | pRxQ |
Pointer to receive queue. More... | |
struct { | |
uint8_t bAutoFlushIgnored:1 | |
If 1, automatically remove ignored packets from Rx queue. More... | |
uint8_t bAutoFlushCrcErr:1 | |
If 1, automatically remove packets with CRC error from Rx queue. More... | |
uint8_t bAutoFlushEmpty:1 | |
If 1, automatically remove empty packets from Rx queue. More... | |
uint8_t bIncludeLenByte:1 | |
If 1, include the received length byte in the stored packet; otherwise discard it. More... | |
uint8_t bIncludeCrc:1 | |
If 1, include the received CRC field in the stored packet; otherwise discard it. More... | |
uint8_t bAppendRssi:1 | |
If 1, append an RSSI byte to the packet in the Rx queue. More... | |
uint8_t bAppendStatus:1 | |
If 1, append a status byte to the packet in the Rx queue. More... | |
uint8_t bAppendTimestamp:1 | |
If 1, append a timestamp to the packet in the Rx queue. More... | |
} | rxConfig |
Configuration bits for the receive queue entries. More... | |
struct { | |
uint8_t scanFilterPolicy:1 | |
The advertiser filter policy, as defined in Volume 2, Part E, Section 7.8.10 of the Bluetooth 4.0 spec. More... | |
uint8_t bActiveScan:1 | |
0: Passive scan 1: Active scan More... | |
uint8_t deviceAddrType:1 | |
The type of the device address – public (0) or random (1) More... | |
uint8_t __pad0__:1 | |
uint8_t bStrictLenFilter:1 | |
1: Discard messages with illegal length More... | |
uint8_t bAutoWlIgnore:1 | |
1: Automatically set ignore bit in white list More... | |
uint8_t bEndOnRpt:1 | |
1: End scanner operation after each reported ADV*_IND and potentially SCAN_RSP More... | |
uint8_t rpaMode:1 | |
Resolvable private address mode 0: Normal operation 1: Use white list for a received RPA regardless of filter policy. More... | |
} | scanConfig |
uint16_t | randomState |
State for pseudo-random number generation used in backoff procedure. More... | |
uint16_t | backoffCount |
Parameter backoffCount used in backoff procedure, cf. Bluetooth 4.0 spec. More... | |
struct { | |
uint8_t logUpperLimit:4 | |
Binary logarithm of parameter upperLimit used in scanner backoff procedure. More... | |
uint8_t bLastSucceeded:1 | |
1 if the last SCAN_RSP was successfully received and upperLimit not changed More... | |
uint8_t bLastFailed:1 | |
1 if reception of the last SCAN_RSP failed and upperLimit was not changed More... | |
} | backoffPar |
uint8_t | scanReqLen |
Size of scan request data. More... | |
uint8_t * | pScanReqData |
Pointer to buffer containing SCAN_REQ data. More... | |
uint16_t * | pDeviceAddress |
Pointer to device address used for this device. More... | |
rfc_bleWhiteListEntry_t * | pWhiteList |
Pointer to white list. More... | |
uint16_t | __dummy0 |
struct { | |
uint8_t triggerType:4 | |
The type of trigger. More... | |
uint8_t bEnaCmd:1 | |
0: No alternative trigger command 1: CMD_TRIGGER can be used as an alternative trigger More... | |
uint8_t triggerNo:2 | |
The trigger number of the CMD_TRIGGER command that triggers this action. More... | |
uint8_t pastTrig:1 | |
0: A trigger in the past is never triggered, or for start of commands, give an error 1: A trigger in the past is triggered as soon as possible More... | |
} | timeoutTrigger |
Trigger that causes the device to stop receiving as soon as allowed. More... | |
struct { | |
uint8_t triggerType:4 | |
The type of trigger. More... | |
uint8_t bEnaCmd:1 | |
0: No alternative trigger command 1: CMD_TRIGGER can be used as an alternative trigger More... | |
uint8_t triggerNo:2 | |
The trigger number of the CMD_TRIGGER command that triggers this action. More... | |
uint8_t pastTrig:1 | |
0: A trigger in the past is never triggered, or for start of commands, give an error 1: A trigger in the past is triggered as soon as possible More... | |
} | endTrigger |
Trigger that causes the device to stop receiving as soon as allowed. More... | |
ratmr_t | timeoutTime |
Time used together with timeoutTrigger that causes the device to stop receiving as soon as allowed, ending with BLE_DONE_RXTIMEOUT. More... | |
ratmr_t | endTime |
Time used together with endTrigger that causes the device to stop receiving as soon as allowed, ending with BLE_DONE_ENDED. More... | |
Definition at line 736 of file rf_ble_cmd.h.
uint16_t rfc_bleScannerPar_s::__dummy0 |
Definition at line 775 of file rf_ble_cmd.h.
uint8_t rfc_bleScannerPar_s::__pad0__ |
Definition at line 754 of file rf_ble_cmd.h.
uint16_t rfc_bleScannerPar_s::backoffCount |
Parameter backoffCount used in backoff procedure, cf. Bluetooth 4.0 spec.
Definition at line 763 of file rf_ble_cmd.h.
struct { ... } rfc_bleScannerPar_s::backoffPar |
uint8_t rfc_bleScannerPar_s::bActiveScan |
0: Passive scan
1: Active scan
Definition at line 751 of file rf_ble_cmd.h.
uint8_t rfc_bleScannerPar_s::bAppendRssi |
If 1, append an RSSI byte to the packet in the Rx queue.
Definition at line 744 of file rf_ble_cmd.h.
uint8_t rfc_bleScannerPar_s::bAppendStatus |
If 1, append a status byte to the packet in the Rx queue.
Definition at line 745 of file rf_ble_cmd.h.
uint8_t rfc_bleScannerPar_s::bAppendTimestamp |
If 1, append a timestamp to the packet in the Rx queue.
Definition at line 746 of file rf_ble_cmd.h.
uint8_t rfc_bleScannerPar_s::bAutoFlushCrcErr |
If 1, automatically remove packets with CRC error from Rx queue.
Definition at line 740 of file rf_ble_cmd.h.
uint8_t rfc_bleScannerPar_s::bAutoFlushEmpty |
If 1, automatically remove empty packets from Rx queue.
Definition at line 741 of file rf_ble_cmd.h.
uint8_t rfc_bleScannerPar_s::bAutoFlushIgnored |
If 1, automatically remove ignored packets from Rx queue.
Definition at line 739 of file rf_ble_cmd.h.
uint8_t rfc_bleScannerPar_s::bAutoWlIgnore |
1: Automatically set ignore bit in white list
Definition at line 756 of file rf_ble_cmd.h.
uint8_t rfc_bleScannerPar_s::bEnaCmd |
0: No alternative trigger command
1: CMD_TRIGGER can be used as an alternative trigger
Definition at line 778 of file rf_ble_cmd.h.
uint8_t rfc_bleScannerPar_s::bEndOnRpt |
1: End scanner operation after each reported ADV*_IND and potentially SCAN_RSP
Definition at line 757 of file rf_ble_cmd.h.
uint8_t rfc_bleScannerPar_s::bIncludeCrc |
If 1, include the received CRC field in the stored packet; otherwise discard it.
Definition at line 743 of file rf_ble_cmd.h.
uint8_t rfc_bleScannerPar_s::bIncludeLenByte |
If 1, include the received length byte in the stored packet; otherwise discard it.
Definition at line 742 of file rf_ble_cmd.h.
uint8_t rfc_bleScannerPar_s::bLastFailed |
1 if reception of the last SCAN_RSP failed and upperLimit
was not changed
Definition at line 768 of file rf_ble_cmd.h.
uint8_t rfc_bleScannerPar_s::bLastSucceeded |
1 if the last SCAN_RSP was successfully received and upperLimit
not changed
Definition at line 766 of file rf_ble_cmd.h.
uint8_t rfc_bleScannerPar_s::bStrictLenFilter |
1: Discard messages with illegal length
Definition at line 755 of file rf_ble_cmd.h.
uint8_t rfc_bleScannerPar_s::deviceAddrType |
The type of the device address – public (0) or random (1)
Definition at line 753 of file rf_ble_cmd.h.
ratmr_t rfc_bleScannerPar_s::endTime |
Time used together with endTrigger
that causes the device to stop receiving as soon as allowed, ending with BLE_DONE_ENDED.
Definition at line 794 of file rf_ble_cmd.h.
struct { ... } rfc_bleScannerPar_s::endTrigger |
Trigger that causes the device to stop receiving as soon as allowed.
uint8_t rfc_bleScannerPar_s::logUpperLimit |
Binary logarithm of parameter upperLimit used in scanner backoff procedure.
Definition at line 765 of file rf_ble_cmd.h.
uint8_t rfc_bleScannerPar_s::pastTrig |
0: A trigger in the past is never triggered, or for start of commands, give an error
1: A trigger in the past is triggered as soon as possible
Definition at line 781 of file rf_ble_cmd.h.
uint16_t* rfc_bleScannerPar_s::pDeviceAddress |
Pointer to device address used for this device.
Definition at line 773 of file rf_ble_cmd.h.
dataQueue_t* rfc_bleScannerPar_s::pRxQ |
Pointer to receive queue.
Definition at line 737 of file rf_ble_cmd.h.
uint8_t* rfc_bleScannerPar_s::pScanReqData |
Pointer to buffer containing SCAN_REQ data.
Definition at line 772 of file rf_ble_cmd.h.
rfc_bleWhiteListEntry_t* rfc_bleScannerPar_s::pWhiteList |
Pointer to white list.
Definition at line 774 of file rf_ble_cmd.h.
uint16_t rfc_bleScannerPar_s::randomState |
State for pseudo-random number generation used in backoff procedure.
Definition at line 762 of file rf_ble_cmd.h.
uint8_t rfc_bleScannerPar_s::rpaMode |
Resolvable private address mode
0: Normal operation
1: Use white list for a received RPA regardless of filter policy.
Definition at line 758 of file rf_ble_cmd.h.
struct { ... } rfc_bleScannerPar_s::rxConfig |
Configuration bits for the receive queue entries.
struct { ... } rfc_bleScannerPar_s::scanConfig |
uint8_t rfc_bleScannerPar_s::scanFilterPolicy |
The advertiser filter policy, as defined in Volume 2, Part E, Section 7.8.10 of the Bluetooth 4.0 spec.
Definition at line 749 of file rf_ble_cmd.h.
uint8_t rfc_bleScannerPar_s::scanReqLen |
Size of scan request data.
Definition at line 771 of file rf_ble_cmd.h.
ratmr_t rfc_bleScannerPar_s::timeoutTime |
Time used together with timeoutTrigger
that causes the device to stop receiving as soon as allowed, ending with BLE_DONE_RXTIMEOUT.
Definition at line 792 of file rf_ble_cmd.h.
struct { ... } rfc_bleScannerPar_s::timeoutTrigger |
Trigger that causes the device to stop receiving as soon as allowed.
uint8_t rfc_bleScannerPar_s::triggerNo |
The trigger number of the CMD_TRIGGER command that triggers this action.
Definition at line 780 of file rf_ble_cmd.h.
uint8_t rfc_bleScannerPar_s::triggerType |
The type of trigger.
Definition at line 777 of file rf_ble_cmd.h.