#include <rf_ble_cmd.h>
Data Fields | |
struct { | |
uint8_t channel:6 | |
The channel on which the packet was received, provided channel is in the range 0–39; otherwise 0x3F. More... | |
uint8_t bIgnore:1 | |
1 if the packet is marked as ignored, 0 otherwise More... | |
uint8_t bCrcErr:1 | |
1 if the packet was received with CRC error, 0 otherwise More... | |
} | status |
Definition at line 1077 of file rf_ble_cmd.h.
uint8_t rfc_bleRxStatus_s::bCrcErr |
1 if the packet was received with CRC error, 0 otherwise
Definition at line 1082 of file rf_ble_cmd.h.
uint8_t rfc_bleRxStatus_s::bIgnore |
1 if the packet is marked as ignored, 0 otherwise
Definition at line 1081 of file rf_ble_cmd.h.
uint8_t rfc_bleRxStatus_s::channel |
The channel on which the packet was received, provided channel is in the range 0–39; otherwise 0x3F.
Definition at line 1079 of file rf_ble_cmd.h.
struct { ... } rfc_bleRxStatus_s::status |