CC13xx Driver Library
rfc_CMD_PROP_TX_s Struct Reference

#include <rf_prop_cmd.h>

Data Fields

uint16_t commandNo
 The command ID number 0x3801. More...
 
uint16_t status
 An integer telling the status of the command. This value is updated by the radio CPU during operation and may be read by the system CPU at any time. More...
 
rfc_radioOp_tpNextOp
 Pointer to the next operation to run after this operation is done. More...
 
ratmr_t startTime
 Absolute or relative start time (depending on the value of startTrigger) More...
 
struct {
   uint8_t   triggerType:4
 The type of trigger. More...
 
   uint8_t   bEnaCmd:1
 0: No alternative trigger command
1: CMD_TRIGGER can be used as an alternative trigger More...
 
   uint8_t   triggerNo:2
 The trigger number of the CMD_TRIGGER command that triggers this action. More...
 
   uint8_t   pastTrig:1
 0: A trigger in the past is never triggered, or for start of commands, give an error
1: A trigger in the past is triggered as soon as possible More...
 
startTrigger
 Identification of the trigger that starts the operation. More...
 
struct {
   uint8_t   rule:4
 Condition for running next command: Rule for how to proceed. More...
 
   uint8_t   nSkip:4
 Number of skips if the rule involves skipping. More...
 
condition
 
struct {
   uint8_t   bFsOff:1
 0: Keep frequency synth on after command
1: Turn frequency synth off after command More...
 
   uint8_t   __pad0__:2
 
   uint8_t   bUseCrc:1
 0: Do not append CRC
1: Append CRC More...
 
   uint8_t   bVarLen:1
 0: Fixed length
1: Transmit length as first byte More...
 
pktConf
 
uint8_t pktLen
 Packet length. More...
 
uint32_t syncWord
 Sync word to transmit. More...
 
uint8_t * pPkt
 Pointer to packet. More...
 

Detailed Description

Definition at line 119 of file rf_prop_cmd.h.

Field Documentation

uint8_t rfc_CMD_PROP_TX_s::__pad0__

Definition at line 141 of file rf_prop_cmd.h.

uint8_t rfc_CMD_PROP_TX_s::bEnaCmd

0: No alternative trigger command
1: CMD_TRIGGER can be used as an alternative trigger

Definition at line 128 of file rf_prop_cmd.h.

uint8_t rfc_CMD_PROP_TX_s::bFsOff

0: Keep frequency synth on after command
1: Turn frequency synth off after command

Definition at line 139 of file rf_prop_cmd.h.

uint8_t rfc_CMD_PROP_TX_s::bUseCrc

0: Do not append CRC
1: Append CRC

Definition at line 142 of file rf_prop_cmd.h.

uint8_t rfc_CMD_PROP_TX_s::bVarLen

0: Fixed length
1: Transmit length as first byte

Definition at line 144 of file rf_prop_cmd.h.

uint16_t rfc_CMD_PROP_TX_s::commandNo

The command ID number 0x3801.

Definition at line 120 of file rf_prop_cmd.h.

struct { ... } rfc_CMD_PROP_TX_s::condition
uint8_t rfc_CMD_PROP_TX_s::nSkip

Number of skips if the rule involves skipping.

Definition at line 136 of file rf_prop_cmd.h.

uint8_t rfc_CMD_PROP_TX_s::pastTrig

0: A trigger in the past is never triggered, or for start of commands, give an error
1: A trigger in the past is triggered as soon as possible

Definition at line 131 of file rf_prop_cmd.h.

struct { ... } rfc_CMD_PROP_TX_s::pktConf
uint8_t rfc_CMD_PROP_TX_s::pktLen

Packet length.

Definition at line 147 of file rf_prop_cmd.h.

rfc_radioOp_t* rfc_CMD_PROP_TX_s::pNextOp

Pointer to the next operation to run after this operation is done.

Definition at line 124 of file rf_prop_cmd.h.

uint8_t* rfc_CMD_PROP_TX_s::pPkt

Pointer to packet.

Definition at line 149 of file rf_prop_cmd.h.

uint8_t rfc_CMD_PROP_TX_s::rule

Condition for running next command: Rule for how to proceed.

Definition at line 135 of file rf_prop_cmd.h.

ratmr_t rfc_CMD_PROP_TX_s::startTime

Absolute or relative start time (depending on the value of startTrigger)

Definition at line 125 of file rf_prop_cmd.h.

struct { ... } rfc_CMD_PROP_TX_s::startTrigger

Identification of the trigger that starts the operation.

uint16_t rfc_CMD_PROP_TX_s::status

An integer telling the status of the command. This value is updated by the radio CPU during operation and may be read by the system CPU at any time.

Definition at line 121 of file rf_prop_cmd.h.

uint32_t rfc_CMD_PROP_TX_s::syncWord

Sync word to transmit.

Definition at line 148 of file rf_prop_cmd.h.

uint8_t rfc_CMD_PROP_TX_s::triggerNo

The trigger number of the CMD_TRIGGER command that triggers this action.

Definition at line 130 of file rf_prop_cmd.h.

uint8_t rfc_CMD_PROP_TX_s::triggerType

The type of trigger.

Definition at line 127 of file rf_prop_cmd.h.