![]() |
![]() |
TI-RTOS Drivers
tidrivers_tivac_2_16_00_08
|
GPIO device specific driver configuration structure. More...
#include <GPIOTiva.h>
Data Fields | |
GPIO_PinConfig * | pinConfigs |
GPIO_CallbackFxn * | callbacks |
uint32_t | numberOfPinConfigs |
uint32_t | numberOfCallbacks |
uint32_t | intPriority |
GPIO device specific driver configuration structure.
GPIO_PinConfig* GPIOTiva_Config::pinConfigs |
Pointer to the board's PinConfig array
GPIO_CallbackFxn* GPIOTiva_Config::callbacks |
Pointer to the board's callback array
uint32_t GPIOTiva_Config::numberOfPinConfigs |
Number of pin configs defined
uint32_t GPIOTiva_Config::numberOfCallbacks |
Number of callbacks defined
uint32_t GPIOTiva_Config::intPriority |
Interrupt priority used for call back interrupts.
intPriority is the interrupt priority, as defined by the underlying OS. It is passed unmodified to the underlying OS's interrupt handler creation code, so you need to refer to the OS documentation for usage. For example, for SYS/BIOS applications, refer to the ti.sysbios.family.arm.m3.Hwi documentation for SYS/BIOS usage of interrupt priorities. If the driver uses the ti.drivers.ports interface instead of making OS calls directly, then the HwiP port handles the interrupt priority in an OS specific way. In the case of the SYS/BIOS port, intPriority is passed unmodified to Hwi_create().
Setting ~0 will configure the lowest possible priority