![]() |
![]() |
TI-RTOS Drivers
tidrivers_c2000_2_16_00_08
|
EMACTiva Hardware attributes. More...
#include <EMACTiva.h>
Data Fields | |
unsigned int | intNum |
unsigned int | intPriority |
uint8_t * | macAddress |
EMACTiva Hardware attributes.
intPriority is the EMAC peripheral's interrupt priority, as defined by the underlying OS. It is passed unmodified to the underlying OS's interrupt handler creation code, so you need to refer to the OS documentation for usage. For example, for SYS/BIOS applications, refer to the ti.sysbios.family.arm.m3.Hwi documentation for SYS/BIOS usage of interrupt priorities. If the driver uses the ti.drivers.ports interface instead of making OS calls directly, then the HwiP port handles the interrupt priority in an OS specific way. In the case of the SYS/BIOS port, intPriority is passed unmodified to Hwi_create().
unsigned int EMACTiva_HWAttrs::intNum |
Interrupt Vector Id
unsigned int EMACTiva_HWAttrs::intPriority |
Interrupt priority
uint8_t* EMACTiva_HWAttrs::macAddress |
Pointer to MAC address