Functions | |
void | SockCleanPcb (uint SockProt, IPN IPAddress) |
void SockCleanPcb | ( | uint | SockProt, | |
IPN | IPAddress | |||
) |
Description
The function cycles through all the socket entries for the specified protocol family and closes any socket which matches the IP Address specified. The function was added to ensure that when an IP address is modified then any sockets which are using the OLD IP Address should be closed.
This is for *internal* NDK Stack Usage.
[in] | SockProt | Socket Family |
[in] | IPAddress | OLD IP Address to which a socket might be bound to and which needs to be cleaned. |
Not | Applicable |