Functions | |
_extern SOCKET | accept (SOCKET s, PSA pName, int *plen) |
_extern int | bind (SOCKET s, PSA pName, int len) |
_extern int | connect (SOCKET s, PSA pName, int len) |
_extern int | getpeername (SOCKET s, PSA pName, int *plen) |
_extern int | getsockname (SOCKET s, PSA pName, int *plen) |
_extern int | getsockopt (SOCKET s, int level, int op, void *pbuf, int *pbufsize) |
_extern int | listen (SOCKET s, int maxcon) |
_extern int | recv (SOCKET s, void *pbuf, int size, int flags) |
_extern int | recvfrom (SOCKET s, void *pbuf, int size, int flags, PSA pName, int *plen) |
_extern int | recvnc (SOCKET s, void **ppbuf, int flags, HANDLE *pHandle) |
_extern int | recvncfrom (SOCKET s, void **ppbuf, int flags, PSA pName, int *plen, HANDLE *pHandle) |
_extern int | send (SOCKET s, void *pbuf, int size, int flags) |
_extern int | sendto (SOCKET s, void *pbuf, int size, int flags, PSA pName, int len) |
_extern int | setsockopt (SOCKET s, int level, int op, void *pbuf, int bufsize) |
_extern int | shutdown (SOCKET s, int how) |
_extern SOCKET | socket (int domain, int type, int protocol) |
_extern int | getsendncbuff (SOCKET s, UINT32 bufSize, void **phBuf, HANDLE *phPkt) |
_extern int | sendnc (SOCKET s, void *pbuf, int size, HANDLE hPkt, int flags) |
_extern int | pipe (HANDLE *pfd1, HANDLE *pfd2) |
_extern SOCKET accept | ( | SOCKET | s, | |
PSA | pName, | |||
int * | plen | |||
) |
Description
This function extracts the first pending connection request in the socket queue and spawns a new socket to accept the incoming connection request. This function call is valid only for connection-oriented socket types like TCP.
[in] | s | Handle to local bound socket that is waiting/listening on any incoming connections. The argument s is a socket that has been created using "socket" function call, bound to a local address using "bind" and listening for connections with "listen" function calls. |
[in] | pName | Handle to the sockaddr structure that holds the peer host's address and port information. |
[in] | plen | Holds the length of the sockaddr structure being passed as argument to this function. |
[out] | pName | Handle to the sockaddr structure that holds the connected peer's address and port information. The exact format of this is based on the address family. Valid only when this function returns success. |
[out] | plen | Holds the length of the connected peer's sockaddr structure. The exact length depends on the address family of the socket created. Valid only when the function returns success. |
Success | - Handle to the new socket created | |
Error | - INVALID_SOCKET |
_extern int bind | ( | SOCKET | s, | |
PSA | pName, | |||
int | len | |||
) |
Description
This function assigns a name to an unnamed socket. When a socket is created using "socket()" call, it exists in a name space (address family) but has no name assigned. The bind() function requests that name be assigned to the socket.
[in] | s | Handle to a socket obtained using "socket" function call. |
[in] | pName | Handle to the sockaddr structure that holds the local address and port information that needs to be assigned to the socket. |
[in] | len | Holds the length of the sockaddr structure being passed as argument to this function. This in turn depends on the address family of the socket. |
Success | - 0 | |
Error | - -1 |
_extern int connect | ( | SOCKET | s, | |
PSA | pName, | |||
int | len | |||
) |
Description
This function establishes a logical connection from the socket specified by s to the foreign name (address) specified by pName.
[in] | s | Handle to a socket obtained using "socket" function call. |
[in] | pName | Handle to the sockaddr structure that holds the remote host's address and port information to which the socket needs to connect to. For UDP/SOCK_DGRAM socket pName specifies the address to which packets would be sent by default or can be received from. For TCP/SOCK_STREAM socket this call attempts to make a connection to the socket that is bound to address specified by pName. |
[in] | len | Holds the length of the sockaddr structure being passed as argument to this function. This in turn depends on the address family of the socket. |
Success | - 0 | |
Error | - -1 |
_extern int getpeername | ( | SOCKET | s, | |
PSA | pName, | |||
int * | plen | |||
) |
Description
The getpeername() function retrieves the peer address of the specified socket, store this address in the sockaddr structure pointed to by the pName argument, and store the length of this address in plen argument.
[in] | s | Handle to a socket obtained using "socket" function call. |
[out] | pName | Handle to the sockaddr structure that holds the remote host's address and port information to which the socket is connected to. Valid only when this function returns success. |
[out] | plen | Holds the length of the sockaddr structure being passed as result from this function. Valid only when this function returns success. |
Success | - 0 | |
Error | - -1 |
_extern int getsendncbuff | ( | SOCKET | s, | |
UINT32 | bufSize, | |||
void ** | phBuf, | |||
HANDLE * | phPkt | |||
) |
Description
This function allocates bufSize bytes memory for the data buffer and required memory for the packet buffer to hold this data. On successful memory allocation, it initializes the phBuf and phPkt pointers with the data buffer and packet buffer handles. The data buffer obtained from this API can be used by the application to fill in required data. The application then would need to use the data buffer and packet buffer handles in its call to sendnc() API to send the packet out without any copy on transmit path by the stack. The packet and data buffers are freed up automatically once the packet transmission is completed in the ethernet driver. However, if for some reason the application would like to free the buffer and packet obtained using this call, it can to do so by passing the packet buffer handle to sendncfree() API call and it would free up both the packet and data buffers.
This API is currently only supported for AF_RAWETH family sockets.
[in] | s | Handle to a socket obtained using "socket" function call. |
[in] | bufSize | Size of data buffer to allocate memory for. |
[in] | phBuf | Pointer to data buffer handle in which the application can fill in the required data to send using sendnc() API. |
[in] | phPkt | Pointer to the packet buffer handle which holds the data buffer in turn. |
Success | - 0 | |
Error | - -1 |
_extern int getsockname | ( | SOCKET | s, | |
PSA | pName, | |||
int * | plen | |||
) |
Description
The getsockname() function retrieves the local address of the specified socket, store this address in the sockaddr structure pointed to by the pName argument, and store the length of this address in plen argument.
[in] | s | Handle to a socket obtained using "socket" function call. |
[out] | pName | Handle to the sockaddr structure that holds the local host's address and port information to which the socket is bound to. Valid only when this function returns success. |
[out] | plen | Holds the length of the sockaddr structure being passed as result from this function. Valid only when this function returns success. |
Success | - 0 | |
Error | - -1 |
_extern int getsockopt | ( | SOCKET | s, | |
int | level, | |||
int | op, | |||
void * | pbuf, | |||
int * | pbufsize | |||
) |
Description
This function returns the options associated with a socket.
[in] | s | Socket handle |
[in] | level | Option level (SOL_SOCKET, IPPROTO_IP, IPPROTO_IPV6,IPPROTO_TCP) |
[in] | op | Socket option to get |
[in] | pbuf | Pointer to memory buffer |
[in] | pbufsize | Pointer to size of memory buffer |
Success | - 0 | |
Error | - -1 |
_extern int listen | ( | SOCKET | s, | |
int | maxcon | |||
) |
Description
This function enables the socket to wait for any incoming connection requests. It also configures the size of the pending connection request queue of the socket. This call is applicable only for connection oriented sockets (SOCK_STREAM/TCP).
[in] | s | Handle to a socket obtained using "socket" function call. |
[in] | maxcon | Specifies the maximum length of the queue of pending connections. |
Success | - 0 | |
Error | - -1 |
_extern int pipe | ( | HANDLE * | pfdret1, | |
HANDLE * | pfdret2 | |||
) |
Description
Creates a pre-connected full duplex pipe. The returned file descriptors can be used with all the fd file descriptor functions, as well as the send() and recv() socket functions.
[in] | pfdret1 | Pointer to file descriptor to first end of pipe. |
[in] | pfdret2 | Pointer to file descriptor to second end of pipe. |
Success | - 0 | |
Error | - -1 |
_extern int recv | ( | SOCKET | s, | |
void * | pbuf, | |||
int | size, | |||
int | flags | |||
) |
Description
This function is used to read data received on a specified socket.
[in] | s | Handle to a socket obtained using "socket" function call. |
[in] | pbuf | Specifies the buffer to which the data has to be copied to. |
[in] | size | Specifies the maximum size of the buffer. |
[in] | flags | Options flags |
Success | - Number of bytes of data received successfully | |
Error | - -1 |
_extern int recvfrom | ( | SOCKET | s, | |
void * | pbuf, | |||
int | size, | |||
int | flags, | |||
PSA | pName, | |||
int * | plen | |||
) |
Description
This function attempts to receive data from a socket. It is normally called with unconnected, non-connection oriented sockets. The data is placed into the buffer specified by pbuf, up to a maximum length specified by size. The options in flags can be used to change the default behavior of the operation. The name (address) of the sender is written to pName.
[in] | s | Handle to a socket obtained using "socket" function call. |
[in] | pbuf | Specifies the buffer to which the data has to be copied to. |
[in] | size | Specifies the maximum size of the buffer. |
[in] | flags | Options flags |
[out] | pName | Pointer to place name (address) of sender |
[out] | plen | Pointer to size of pName |
Success | - Number of bytes of data received successfully | |
Error | - -1 |
_extern int recvnc | ( | SOCKET | s, | |
void ** | ppbuf, | |||
int | flags, | |||
HANDLE * | phFrag | |||
) |
Description
This function is used to read data received on a specified socket without copying. This is supported only on IPv4/AF_INET family and Raw ethernet/AF_RAWETH sockets.
[in] | s | Handle to a socket obtained using "socket" function call. |
[out] | ppbuf | Pointer to receive data buffer pointer. |
[in] | flags | Options flags |
[out] | phFrag | Pointer to receive buffer handle. |
Success | - Number of bytes of data received successfully | |
Error | - -1 |
_extern int recvncfrom | ( | SOCKET | s, | |
void ** | ppbuf, | |||
int | flags, | |||
PSA | pName, | |||
int * | plen, | |||
HANDLE * | phFrag | |||
) |
Description
This function attempts to receive data from a socket. It is normally called with unconnected, non-connection oriented sockets. A pointer to data is returned in ppbuf. A system handle used to free the buffer is returned in phFrag. Both of these pointers must be valid. The name (address) of the sender is written to pName. This function is only valid for IPv4/AF_INET family sockets.
[in] | s | Handle to a socket obtained using "socket" function call. |
[out] | ppbuf | Pointer to receive data buffer pointer. |
[in] | flags | Options flags |
[out] | pName | Pointer to place name (address) of sender |
[out] | plen | Pointer to size of pName |
[out] | phFrag | Pointer to receive buffer handle. |
Success | - Number of bytes of data received successfully | |
Error | - -1 |
_extern int send | ( | SOCKET | s, | |
void * | pbuf, | |||
int | size, | |||
int | flags | |||
) |
Description
This function attempts to send data on a socket. It is used on connected sockets only. The data to send is contained in the buffer specified by pbuf, with a length specified by size. The options in flags can be used to change the default behavior of the operation. The functions returns the length of the data transmitted on successful completion.
[in] | s | Handle to a socket obtained using "socket" function call. |
[in] | pbuf | Data buffer holding data to transmit |
[in] | size | Size of data. |
[in] | flags | Options flags |
Success | - Number of bytes of data sent successfully | |
Error | - -1 |
_extern int sendnc | ( | SOCKET | s, | |
void * | pbuf, | |||
int | size, | |||
HANDLE | hPkt, | |||
int | flags | |||
) |
Description
This function attempts to send data on a socket without copy. The data to send is contained in the buffer specified by pbuf, with a length specified by size. Also, a valid handle to the packet buffer hPkt needs to be specified. This packet handle and the buffer pointer should have been obtained from getsendncbuf() call before calling this API. The options in flags can be used to change the default behavior of the operation. The functions returns the length of the data transmitted on successful completion.
This API is currently only supported for AF_RAWETH family sockets.
[in] | s | Handle to a socket obtained using "socket" function call. |
[in] | pbuf | Data buffer holding data to transmit |
[in] | size | Size of data. |
[in] | hPkt | packet handle obtained previously from getsendncbuf() call. |
[in] | flags | Options flags |
Success | - Number of bytes of data sent successfully | |
Error | - -1 |
_extern int sendto | ( | SOCKET | s, | |
void * | pbuf, | |||
int | size, | |||
int | flags, | |||
PSA | pName, | |||
int | len | |||
) |
Description
This function attempts to send data on a socket to a specified destination. It is used on unconnected, non-connection oriented \ sockets only. The data to send is contained in the buffer specified by pbuf, with a length specified by size. The options in flags can be used to change the default behavior of the operation.
[in] | s | Handle to a socket obtained using "socket" function call. |
[in] | pbuf | Data buffer holding data to transmit |
[in] | size | Size of data. |
[in] | flags | Options flags |
[out] | pName | Pointer to name (address) of destination |
[out] | len | size of pName |
Success | - Number of bytes of data sent successfully | |
Error | - -1 |
_extern int setsockopt | ( | SOCKET | s, | |
int | level, | |||
int | op, | |||
void * | pbuf, | |||
int | bufsize | |||
) |
Description
This function sets the option values associated with a socket.
[in] | s | Socket handle |
[in] | level | Option level (SOL_SOCKET, IPPROTO_IP, IPPROTO_IPV6,IPPROTO_TCP) |
[in] | op | Socket option to set |
[in] | pbuf | Pointer to memory buffer |
[in] | bufsize | Size of memory buffer pointed to by pbuf |
Success | - 0 | |
Error | - -1 |
_extern int shutdown | ( | SOCKET | s, | |
int | how | |||
) |
Description
This function causes all or part of a full-duplex connection on the socket associated with a socket to be shut down. If how is SHUT_RD (0), further receives will be disallowed. If how is SHUT_WR (1), further sends will be disallowed. If how is SHUT_RDWR (2), further sends and receives will be disallowed.
[in] | s | Handle to a socket obtained using "socket" function call. |
[in] | how | Manner of shutdown. |
Success | - 0 | |
Error | - -1 |
_extern SOCKET socket | ( | int | domain, | |
int | type, | |||
int | protocol | |||
) |
Description
This function creates a socket, an endpoint for communication and returns the socket in the form of a file descriptor.
[in] | domain | Socket domain/family. Valid values are AF_INET/AF_INET6. |
[in] | type | Socket type (SOCK_DGRAM, SOCK_STREAM, SOCK_RAW). |
[in] | protocol | Socket protocol (Normally IPPROTO_TCP or IPPROTO_UDP, but can be anything when type is set to SOCK_RAW) |
Success | - socket handle | |
Error | - INVALID_SOCKET |