CC26xx Driver Library
rfc_bleScannerOutput_s Struct Reference

#include <rf_ble_cmd.h>

Data Fields

uint16_t nTxScanReq
 Number of transmitted SCAN_REQ packets. More...
 
uint16_t nBackedOffScanReq
 Number of SCAN_REQ packets not sent due to backoff procedure. More...
 
uint16_t nRxAdvOk
 Number of ADV*_IND packets received with CRC OK and not ignored. More...
 
uint16_t nRxAdvIgnored
 Number of ADV*_IND packets received with CRC OK, but ignored. More...
 
uint16_t nRxAdvNok
 Number of ADV*_IND packets received with CRC error. More...
 
uint16_t nRxScanRspOk
 Number of SCAN_RSP packets received with CRC OK and not ignored. More...
 
uint16_t nRxScanRspIgnored
 Number of SCAN_RSP packets received with CRC OK, but ignored. More...
 
uint16_t nRxScanRspNok
 Number of SCAN_RSP packets received with CRC error. More...
 
uint8_t nRxAdvBufFull
 Number of ADV*_IND packets received that did not fit in Rx queue. More...
 
uint8_t nRxScanRspBufFull
 Number of SCAN_RSP packets received that did not fit in Rx queue. More...
 
int8_t lastRssi
 The RSSI of the last received packet. More...
 
uint8_t __dummy0
 
ratmr_t timeStamp
 Time stamp of the last successfully received ADV*_IND packet that was not ignored. More...
 

Detailed Description

Definition at line 993 of file rf_ble_cmd.h.

Field Documentation

uint8_t rfc_bleScannerOutput_s::__dummy0

Definition at line 1005 of file rf_ble_cmd.h.

int8_t rfc_bleScannerOutput_s::lastRssi

The RSSI of the last received packet.

Definition at line 1004 of file rf_ble_cmd.h.

uint16_t rfc_bleScannerOutput_s::nBackedOffScanReq

Number of SCAN_REQ packets not sent due to backoff procedure.

Definition at line 995 of file rf_ble_cmd.h.

uint8_t rfc_bleScannerOutput_s::nRxAdvBufFull

Number of ADV*_IND packets received that did not fit in Rx queue.

Definition at line 1002 of file rf_ble_cmd.h.

uint16_t rfc_bleScannerOutput_s::nRxAdvIgnored

Number of ADV*_IND packets received with CRC OK, but ignored.

Definition at line 997 of file rf_ble_cmd.h.

uint16_t rfc_bleScannerOutput_s::nRxAdvNok

Number of ADV*_IND packets received with CRC error.

Definition at line 998 of file rf_ble_cmd.h.

uint16_t rfc_bleScannerOutput_s::nRxAdvOk

Number of ADV*_IND packets received with CRC OK and not ignored.

Definition at line 996 of file rf_ble_cmd.h.

uint8_t rfc_bleScannerOutput_s::nRxScanRspBufFull

Number of SCAN_RSP packets received that did not fit in Rx queue.

Definition at line 1003 of file rf_ble_cmd.h.

uint16_t rfc_bleScannerOutput_s::nRxScanRspIgnored

Number of SCAN_RSP packets received with CRC OK, but ignored.

Definition at line 1000 of file rf_ble_cmd.h.

uint16_t rfc_bleScannerOutput_s::nRxScanRspNok

Number of SCAN_RSP packets received with CRC error.

Definition at line 1001 of file rf_ble_cmd.h.

uint16_t rfc_bleScannerOutput_s::nRxScanRspOk

Number of SCAN_RSP packets received with CRC OK and not ignored.

Definition at line 999 of file rf_ble_cmd.h.

uint16_t rfc_bleScannerOutput_s::nTxScanReq

Number of transmitted SCAN_REQ packets.

Definition at line 994 of file rf_ble_cmd.h.

ratmr_t rfc_bleScannerOutput_s::timeStamp

Time stamp of the last successfully received ADV*_IND packet that was not ignored.

Definition at line 1006 of file rf_ble_cmd.h.