CC26xx Driver Library
rfc_bleMasterSlavePar_s Struct Reference

#include <rf_ble_cmd.h>

Data Fields

dataQueue_tpRxQ
 Pointer to receive queue. More...
 
dataQueue_tpTxQ
 Pointer to transmit queue. More...
 
struct {
   uint8_t   bAutoFlushIgnored:1
 If 1, automatically remove ignored packets from Rx queue. More...
 
   uint8_t   bAutoFlushCrcErr:1
 If 1, automatically remove packets with CRC error from Rx queue. More...
 
   uint8_t   bAutoFlushEmpty:1
 If 1, automatically remove empty packets from Rx queue. More...
 
   uint8_t   bIncludeLenByte:1
 If 1, include the received length byte in the stored packet; otherwise discard it. More...
 
   uint8_t   bIncludeCrc:1
 If 1, include the received CRC field in the stored packet; otherwise discard it. More...
 
   uint8_t   bAppendRssi:1
 If 1, append an RSSI byte to the packet in the Rx queue. More...
 
   uint8_t   bAppendStatus:1
 If 1, append a status byte to the packet in the Rx queue. More...
 
   uint8_t   bAppendTimestamp:1
 If 1, append a timestamp to the packet in the Rx queue. More...
 
rxConfig
 Configuration bits for the receive queue entries. More...
 
struct {
   uint8_t   lastRxSn:1
 The SN bit of the header of the last packet received with CRC OK. More...
 
   uint8_t   lastTxSn:1
 The SN bit of the header of the last transmitted packet. More...
 
   uint8_t   nextTxSn:1
 The SN bit of the header of the next packet to transmit. More...
 
   uint8_t   bFirstPkt:1
 For slave: 0 if a packet has been transmitted on the connection, 1 otherwise. More...
 
   uint8_t   bAutoEmpty:1
 1 if the last transmitted packet was an auto-empty packet More...
 
   uint8_t   bLlCtrlTx:1
 1 if the last transmitted packet was an LL control packet (LLID = 11) More...
 
   uint8_t   bLlCtrlAckRx:1
 1 if the last received packet was the ACK of an LL control packet More...
 
   uint8_t   bLlCtrlAckPending:1
 1 if the last successfully received packet was an LL control packet which has not yet been ACK'ed More...
 
seqStat
 
uint8_t maxNack
 Maximum number of NACKs received before operation ends. 0: No limit. More...
 
uint8_t maxPkt
 Maximum number of packets transmitted in the operation before it ends. 0: No limit. More...
 
uint32_t accessAddress
 Access address used on the connection. More...
 
uint8_t crcInit0
 CRC initialization value used on the connection – least significant byte. More...
 
uint8_t crcInit1
 CRC initialization value used on the connection – middle byte. More...
 
uint8_t crcInit2
 CRC initialization value used on the connection – most significant byte. More...
 

Detailed Description

Definition at line 544 of file rf_ble_cmd.h.

Field Documentation

uint32_t rfc_bleMasterSlavePar_s::accessAddress

Access address used on the connection.

Definition at line 569 of file rf_ble_cmd.h.

uint8_t rfc_bleMasterSlavePar_s::bAppendRssi

If 1, append an RSSI byte to the packet in the Rx queue.

Definition at line 553 of file rf_ble_cmd.h.

uint8_t rfc_bleMasterSlavePar_s::bAppendStatus

If 1, append a status byte to the packet in the Rx queue.

Definition at line 554 of file rf_ble_cmd.h.

uint8_t rfc_bleMasterSlavePar_s::bAppendTimestamp

If 1, append a timestamp to the packet in the Rx queue.

Definition at line 555 of file rf_ble_cmd.h.

uint8_t rfc_bleMasterSlavePar_s::bAutoEmpty

1 if the last transmitted packet was an auto-empty packet

Definition at line 562 of file rf_ble_cmd.h.

uint8_t rfc_bleMasterSlavePar_s::bAutoFlushCrcErr

If 1, automatically remove packets with CRC error from Rx queue.

Definition at line 549 of file rf_ble_cmd.h.

uint8_t rfc_bleMasterSlavePar_s::bAutoFlushEmpty

If 1, automatically remove empty packets from Rx queue.

Definition at line 550 of file rf_ble_cmd.h.

uint8_t rfc_bleMasterSlavePar_s::bAutoFlushIgnored

If 1, automatically remove ignored packets from Rx queue.

Definition at line 548 of file rf_ble_cmd.h.

uint8_t rfc_bleMasterSlavePar_s::bFirstPkt

For slave: 0 if a packet has been transmitted on the connection, 1 otherwise.

Definition at line 561 of file rf_ble_cmd.h.

uint8_t rfc_bleMasterSlavePar_s::bIncludeCrc

If 1, include the received CRC field in the stored packet; otherwise discard it.

Definition at line 552 of file rf_ble_cmd.h.

uint8_t rfc_bleMasterSlavePar_s::bIncludeLenByte

If 1, include the received length byte in the stored packet; otherwise discard it.

Definition at line 551 of file rf_ble_cmd.h.

uint8_t rfc_bleMasterSlavePar_s::bLlCtrlAckPending

1 if the last successfully received packet was an LL control packet which has not yet been ACK'ed

Definition at line 565 of file rf_ble_cmd.h.

uint8_t rfc_bleMasterSlavePar_s::bLlCtrlAckRx

1 if the last received packet was the ACK of an LL control packet

Definition at line 564 of file rf_ble_cmd.h.

uint8_t rfc_bleMasterSlavePar_s::bLlCtrlTx

1 if the last transmitted packet was an LL control packet (LLID = 11)

Definition at line 563 of file rf_ble_cmd.h.

uint8_t rfc_bleMasterSlavePar_s::crcInit0

CRC initialization value used on the connection – least significant byte.

Definition at line 570 of file rf_ble_cmd.h.

uint8_t rfc_bleMasterSlavePar_s::crcInit1

CRC initialization value used on the connection – middle byte.

Definition at line 571 of file rf_ble_cmd.h.

uint8_t rfc_bleMasterSlavePar_s::crcInit2

CRC initialization value used on the connection – most significant byte.

Definition at line 572 of file rf_ble_cmd.h.

uint8_t rfc_bleMasterSlavePar_s::lastRxSn

The SN bit of the header of the last packet received with CRC OK.

Definition at line 558 of file rf_ble_cmd.h.

uint8_t rfc_bleMasterSlavePar_s::lastTxSn

The SN bit of the header of the last transmitted packet.

Definition at line 559 of file rf_ble_cmd.h.

uint8_t rfc_bleMasterSlavePar_s::maxNack

Maximum number of NACKs received before operation ends. 0: No limit.

Definition at line 567 of file rf_ble_cmd.h.

uint8_t rfc_bleMasterSlavePar_s::maxPkt

Maximum number of packets transmitted in the operation before it ends. 0: No limit.

Definition at line 568 of file rf_ble_cmd.h.

uint8_t rfc_bleMasterSlavePar_s::nextTxSn

The SN bit of the header of the next packet to transmit.

Definition at line 560 of file rf_ble_cmd.h.

dataQueue_t* rfc_bleMasterSlavePar_s::pRxQ

Pointer to receive queue.

Definition at line 545 of file rf_ble_cmd.h.

dataQueue_t* rfc_bleMasterSlavePar_s::pTxQ

Pointer to transmit queue.

Definition at line 546 of file rf_ble_cmd.h.

struct { ... } rfc_bleMasterSlavePar_s::rxConfig

Configuration bits for the receive queue entries.

struct { ... } rfc_bleMasterSlavePar_s::seqStat