#include <rf_common_cmd.h>
Data Fields | |
uint16_t | commandNo |
The command ID number 0x0805. More... | |
uint16_t | status |
An integer telling the status of the command. This value is updated by the radio CPU during operation and may be read by the system CPU at any time. More... | |
rfc_radioOp_t * | pNextOp |
Pointer to the next operation to run after this operation is done. More... | |
ratmr_t | startTime |
Absolute or relative start time (depending on the value of startTrigger ) More... | |
struct { | |
uint8_t triggerType:4 | |
The type of trigger. More... | |
uint8_t bEnaCmd:1 | |
0: No alternative trigger command 1: CMD_TRIGGER can be used as an alternative trigger More... | |
uint8_t triggerNo:2 | |
The trigger number of the CMD_TRIGGER command that triggers this action. More... | |
uint8_t pastTrig:1 | |
0: A trigger in the past is never triggered, or for start of commands, give an error 1: A trigger in the past is triggered as soon as possible More... | |
} | startTrigger |
Identification of the trigger that starts the operation. More... | |
struct { | |
uint8_t rule:4 | |
Condition for running next command: Rule for how to proceed. More... | |
uint8_t nSkip:4 | |
Number of skips if the rule involves skipping. More... | |
} | condition |
struct { | |
uint16_t endianness:1 | |
0: Least significant bit first 1: Most significant bit first More... | |
uint16_t numHdrBits:6 | |
Number of bits in the header. More... | |
uint16_t bFsOff:1 | |
0: Keep frequency synth on after command 1: Turn frequency synth off after command More... | |
uint16_t bUseCrc:1 | |
0: No CRC 1: The last bytes of the packet are a CRC More... | |
uint16_t bCrcIncSw:1 | |
0: Do not include sync word in CRC calculation 1: Include sync word in CRC calculation More... | |
uint16_t bCrcIncHdr:1 | |
0: Do not include header in CRC calculation 1: Include header in CRC calculation More... | |
uint16_t bReportCrc:1 | |
0: Do not write CRC to receive buffer 1: Write received CRC to receive buffer More... | |
uint16_t endType:1 | |
0: Packet is received to the end if end trigger happens after sync is obtained 1: Packet reception is stopped if end trigger happens More... | |
uint16_t bDualSw:1 | |
0: Single sync word 1: Dual sync word. More... | |
} | pktConfig |
uint32_t | syncWord |
Sync word to receive. More... | |
uint32_t | syncWord2 |
Secondary sync word to receive if pktConfig.bDualSw = 1. More... | |
struct { | |
uint16_t numLenBits:4 | |
Number of bits in the length field. More... | |
uint16_t lenFieldPos:5 | |
Bit position of the first bit in the length field. More... | |
uint16_t lenOffset:7 | |
Signed number to add to the received length field. More... | |
} | lenConfig |
uint16_t | maxLen |
Maximum number of bytes in the received packet (including header, excluding CRC) More... | |
uint8_t * | pRecPkt |
Pointer to buffer for received packet. NULL: Do not store the contents. More... | |
ratmr_t | endTime |
Time to end the operation. More... | |
struct { | |
uint8_t triggerType:4 | |
The type of trigger. More... | |
uint8_t bEnaCmd:1 | |
0: No alternative trigger command 1: CMD_TRIGGER can be used as an alternative trigger More... | |
uint8_t triggerNo:2 | |
The trigger number of the CMD_TRIGGER command that triggers this action. More... | |
uint8_t pastTrig:1 | |
0: A trigger in the past is never triggered, or for start of commands, give an error 1: A trigger in the past is triggered as soon as possible More... | |
} | endTrigger |
Trigger classifier for ending the operation. More... | |
int8_t | rssi |
RSSI of received packet. More... | |
uint16_t | recLen |
Number of bytes written to receive buffer. More... | |
ratmr_t | timeStamp |
Time stamp of received packet. More... | |
uint16_t | nRxOk |
Counter of number of received packets with CRC OK and first sync word. More... | |
uint16_t | nRxNok |
Counter of number of received packets with CRC error and first sync word. More... | |
uint16_t | nRx2Ok |
Counter of number of received packets with CRC OK and second sync word; may safely be omitted if pktConfig.bDualSw is 0. More... | |
uint16_t | nRx2Nok |
Counter of number of received packets with CRC error and second sync word; may safely be omitted if pktConfig.bDualSw is 0. More... | |
Definition at line 279 of file rf_common_cmd.h.
uint16_t rfc_CMD_RX_s::bCrcIncHdr |
0: Do not include header in CRC calculation
1: Include header in CRC calculation
Definition at line 308 of file rf_common_cmd.h.
uint16_t rfc_CMD_RX_s::bCrcIncSw |
0: Do not include sync word in CRC calculation
1: Include sync word in CRC calculation
Definition at line 306 of file rf_common_cmd.h.
uint16_t rfc_CMD_RX_s::bDualSw |
0: Single sync word
1: Dual sync word.
Definition at line 314 of file rf_common_cmd.h.
uint8_t rfc_CMD_RX_s::bEnaCmd |
0: No alternative trigger command
1: CMD_TRIGGER can be used as an alternative trigger
Definition at line 288 of file rf_common_cmd.h.
uint16_t rfc_CMD_RX_s::bFsOff |
0: Keep frequency synth on after command
1: Turn frequency synth off after command
Definition at line 302 of file rf_common_cmd.h.
uint16_t rfc_CMD_RX_s::bReportCrc |
0: Do not write CRC to receive buffer
1: Write received CRC to receive buffer
Definition at line 310 of file rf_common_cmd.h.
uint16_t rfc_CMD_RX_s::bUseCrc |
0: No CRC
1: The last bytes of the packet are a CRC
Definition at line 304 of file rf_common_cmd.h.
uint16_t rfc_CMD_RX_s::commandNo |
The command ID number 0x0805.
Definition at line 280 of file rf_common_cmd.h.
struct { ... } rfc_CMD_RX_s::condition |
uint16_t rfc_CMD_RX_s::endianness |
0: Least significant bit first
1: Most significant bit first
Definition at line 299 of file rf_common_cmd.h.
ratmr_t rfc_CMD_RX_s::endTime |
Time to end the operation.
Definition at line 326 of file rf_common_cmd.h.
struct { ... } rfc_CMD_RX_s::endTrigger |
Trigger classifier for ending the operation.
uint16_t rfc_CMD_RX_s::endType |
0: Packet is received to the end if end trigger happens after sync is obtained
1: Packet reception is stopped if end trigger happens
Definition at line 312 of file rf_common_cmd.h.
struct { ... } rfc_CMD_RX_s::lenConfig |
uint16_t rfc_CMD_RX_s::lenFieldPos |
Bit position of the first bit in the length field.
Definition at line 321 of file rf_common_cmd.h.
uint16_t rfc_CMD_RX_s::lenOffset |
Signed number to add to the received length field.
Definition at line 322 of file rf_common_cmd.h.
uint16_t rfc_CMD_RX_s::maxLen |
Maximum number of bytes in the received packet (including header, excluding CRC)
Definition at line 324 of file rf_common_cmd.h.
uint16_t rfc_CMD_RX_s::nRx2Nok |
Counter of number of received packets with CRC error and second sync word; may safely be omitted if pktConfig.bDualSw
is 0.
Definition at line 342 of file rf_common_cmd.h.
uint16_t rfc_CMD_RX_s::nRx2Ok |
Counter of number of received packets with CRC OK and second sync word; may safely be omitted if pktConfig.bDualSw
is 0.
Definition at line 340 of file rf_common_cmd.h.
uint16_t rfc_CMD_RX_s::nRxNok |
Counter of number of received packets with CRC error and first sync word.
Definition at line 339 of file rf_common_cmd.h.
uint16_t rfc_CMD_RX_s::nRxOk |
Counter of number of received packets with CRC OK and first sync word.
Definition at line 338 of file rf_common_cmd.h.
uint8_t rfc_CMD_RX_s::nSkip |
Number of skips if the rule involves skipping.
Definition at line 296 of file rf_common_cmd.h.
uint16_t rfc_CMD_RX_s::numHdrBits |
Number of bits in the header.
Definition at line 301 of file rf_common_cmd.h.
uint16_t rfc_CMD_RX_s::numLenBits |
Number of bits in the length field.
Definition at line 320 of file rf_common_cmd.h.
uint8_t rfc_CMD_RX_s::pastTrig |
0: A trigger in the past is never triggered, or for start of commands, give an error
1: A trigger in the past is triggered as soon as possible
Definition at line 291 of file rf_common_cmd.h.
struct { ... } rfc_CMD_RX_s::pktConfig |
rfc_radioOp_t* rfc_CMD_RX_s::pNextOp |
Pointer to the next operation to run after this operation is done.
Definition at line 284 of file rf_common_cmd.h.
uint8_t* rfc_CMD_RX_s::pRecPkt |
Pointer to buffer for received packet. NULL: Do not store the contents.
Definition at line 325 of file rf_common_cmd.h.
uint16_t rfc_CMD_RX_s::recLen |
Number of bytes written to receive buffer.
Definition at line 336 of file rf_common_cmd.h.
int8_t rfc_CMD_RX_s::rssi |
RSSI of received packet.
Definition at line 335 of file rf_common_cmd.h.
uint8_t rfc_CMD_RX_s::rule |
Condition for running next command: Rule for how to proceed.
Definition at line 295 of file rf_common_cmd.h.
ratmr_t rfc_CMD_RX_s::startTime |
Absolute or relative start time (depending on the value of startTrigger
)
Definition at line 285 of file rf_common_cmd.h.
struct { ... } rfc_CMD_RX_s::startTrigger |
Identification of the trigger that starts the operation.
uint16_t rfc_CMD_RX_s::status |
An integer telling the status of the command. This value is updated by the radio CPU during operation and may be read by the system CPU at any time.
Definition at line 281 of file rf_common_cmd.h.
uint32_t rfc_CMD_RX_s::syncWord |
Sync word to receive.
Definition at line 317 of file rf_common_cmd.h.
uint32_t rfc_CMD_RX_s::syncWord2 |
Secondary sync word to receive if pktConfig.bDualSw
= 1.
Definition at line 318 of file rf_common_cmd.h.
ratmr_t rfc_CMD_RX_s::timeStamp |
Time stamp of received packet.
Definition at line 337 of file rf_common_cmd.h.
uint8_t rfc_CMD_RX_s::triggerNo |
The trigger number of the CMD_TRIGGER command that triggers this action.
Definition at line 290 of file rf_common_cmd.h.
uint8_t rfc_CMD_RX_s::triggerType |
The type of trigger.
Definition at line 287 of file rf_common_cmd.h.