CC26xx Driver Library
rfc_CMD_BLE_ADV_SCAN_s Struct Reference

#include <rf_ble_cmd.h>

Data Fields

uint16_t commandNo
 The command ID number 0x1806. More...
 
uint16_t status
 An integer telling the status of the command. This value is updated by the radio CPU during operation and may be read by the system CPU at any time. More...
 
rfc_radioOp_tpNextOp
 Pointer to the next operation to run after this operation is done. More...
 
ratmr_t startTime
 Absolute or relative start time (depending on the value of startTrigger) More...
 
struct {
   uint8_t   triggerType:4
 The type of trigger. More...
 
   uint8_t   bEnaCmd:1
 0: No alternative trigger command
1: CMD_TRIGGER can be used as an alternative trigger More...
 
   uint8_t   triggerNo:2
 The trigger number of the CMD_TRIGGER command that triggers this action. More...
 
   uint8_t   pastTrig:1
 0: A trigger in the past is never triggered, or for start of commands, give an error
1: A trigger in the past is triggered as soon as possible More...
 
startTrigger
 Identification of the trigger that starts the operation. More...
 
struct {
   uint8_t   rule:4
 Condition for running next command: Rule for how to proceed. More...
 
   uint8_t   nSkip:4
 Number of skips if the rule involves skipping. More...
 
condition
 
uint8_t channel
 Channel to use
0–39: BLE advertising/data channel number 60–207: Custom frequency; (2300 + channel) MHz 255: Use existing frequency Others: Reserved More...
 
struct {
   uint8_t   init:7
 If bOverride = 1 or custom frequency is used:
0: Do not use whitening
Other value: Initialization for 7-bit LFSR whitener. More...
 
   uint8_t   bOverride:1
 0: Use default whitening for BLE advertising/data channels
1: Override whitening initialization with value of init More...
 
whitening
 
rfc_bleAdvPar_tpParams
 Pointer to command specific parameter structure. More...
 
rfc_bleAdvOutput_tpOutput
 Pointer to command specific output structure. More...
 

Detailed Description

Definition at line 331 of file rf_ble_cmd.h.

Field Documentation

uint8_t rfc_CMD_BLE_ADV_SCAN_s::bEnaCmd

0: No alternative trigger command
1: CMD_TRIGGER can be used as an alternative trigger

Definition at line 340 of file rf_ble_cmd.h.

uint8_t rfc_CMD_BLE_ADV_SCAN_s::bOverride

0: Use default whitening for BLE advertising/data channels
1: Override whitening initialization with value of init

Definition at line 359 of file rf_ble_cmd.h.

uint8_t rfc_CMD_BLE_ADV_SCAN_s::channel

Channel to use
0–39: BLE advertising/data channel number 60–207: Custom frequency; (2300 + channel) MHz 255: Use existing frequency Others: Reserved

Definition at line 350 of file rf_ble_cmd.h.

uint16_t rfc_CMD_BLE_ADV_SCAN_s::commandNo

The command ID number 0x1806.

Definition at line 332 of file rf_ble_cmd.h.

struct { ... } rfc_CMD_BLE_ADV_SCAN_s::condition
uint8_t rfc_CMD_BLE_ADV_SCAN_s::init

If bOverride = 1 or custom frequency is used:
0: Do not use whitening
Other value: Initialization for 7-bit LFSR whitener.

Definition at line 356 of file rf_ble_cmd.h.

uint8_t rfc_CMD_BLE_ADV_SCAN_s::nSkip

Number of skips if the rule involves skipping.

Definition at line 348 of file rf_ble_cmd.h.

uint8_t rfc_CMD_BLE_ADV_SCAN_s::pastTrig

0: A trigger in the past is never triggered, or for start of commands, give an error
1: A trigger in the past is triggered as soon as possible

Definition at line 343 of file rf_ble_cmd.h.

rfc_radioOp_t* rfc_CMD_BLE_ADV_SCAN_s::pNextOp

Pointer to the next operation to run after this operation is done.

Definition at line 336 of file rf_ble_cmd.h.

rfc_bleAdvOutput_t* rfc_CMD_BLE_ADV_SCAN_s::pOutput

Pointer to command specific output structure.

Definition at line 363 of file rf_ble_cmd.h.

rfc_bleAdvPar_t* rfc_CMD_BLE_ADV_SCAN_s::pParams

Pointer to command specific parameter structure.

Definition at line 362 of file rf_ble_cmd.h.

uint8_t rfc_CMD_BLE_ADV_SCAN_s::rule

Condition for running next command: Rule for how to proceed.

Definition at line 347 of file rf_ble_cmd.h.

ratmr_t rfc_CMD_BLE_ADV_SCAN_s::startTime

Absolute or relative start time (depending on the value of startTrigger)

Definition at line 337 of file rf_ble_cmd.h.

struct { ... } rfc_CMD_BLE_ADV_SCAN_s::startTrigger

Identification of the trigger that starts the operation.

uint16_t rfc_CMD_BLE_ADV_SCAN_s::status

An integer telling the status of the command. This value is updated by the radio CPU during operation and may be read by the system CPU at any time.

Definition at line 333 of file rf_ble_cmd.h.

uint8_t rfc_CMD_BLE_ADV_SCAN_s::triggerNo

The trigger number of the CMD_TRIGGER command that triggers this action.

Definition at line 342 of file rf_ble_cmd.h.

uint8_t rfc_CMD_BLE_ADV_SCAN_s::triggerType

The type of trigger.

Definition at line 339 of file rf_ble_cmd.h.

struct { ... } rfc_CMD_BLE_ADV_SCAN_s::whitening