CC26xx Driver Library
prcm.c File Reference
#include <driverlib/prcm.h>

Go to the source code of this file.

Macros

#define PRCM_PERIPH_INDEX(a)   (((a) >> 8) & 0xf)
 
#define PRCM_PERIPH_MASKBIT(a)   (0x00000001 << ((a) & 0xf))
 

Functions

void PRCMInfClockConfigureSet (uint32_t ui32ClkDiv, uint32_t ui32PowerMode)
 Configure the infrastructure clock. More...
 
uint32_t PRCMInfClockConfigureGet (uint32_t ui32PowerMode)
 Use this function to get the infrastructure clock configuration. More...
 
void PRCMAudioClockConfigSet (uint32_t ui32ClkConfig, uint32_t ui32SampleRate)
 Configure the audio clock generation. More...
 
void PRCMAudioClockConfigSetOverride (uint32_t ui32ClkConfig, uint32_t ui32MstDiv, uint32_t ui32BitDiv, uint32_t ui32WordDiv)
 Configure the audio clock generation with manual setting of clock divider. More...
 
void PRCMPowerDomainOn (uint32_t ui32Domains)
 Turn power on in power domains in the MCU domain. More...
 
void PRCMPowerDomainOff (uint32_t ui32Domains)
 Turn off a specific power domain. More...
 
void PRCMPeripheralRunEnable (uint32_t ui32Peripheral)
 Enables a peripheral in Run mode. More...
 
void PRCMPeripheralRunDisable (uint32_t ui32Peripheral)
 Disables a peripheral in Run mode. More...
 
void PRCMPeripheralSleepEnable (uint32_t ui32Peripheral)
 Enables a peripheral in sleep mode. More...
 
void PRCMPeripheralSleepDisable (uint32_t ui32Peripheral)
 Disables a peripheral in sleep mode. More...
 
void PRCMPeripheralDeepSleepEnable (uint32_t ui32Peripheral)
 Enables a peripheral in deep-sleep mode. More...
 
void PRCMPeripheralDeepSleepDisable (uint32_t ui32Peripheral)
 Disables a peripheral in deep-sleep mode. More...
 
uint32_t PRCMPowerDomainStatus (uint32_t ui32Domains)
 Get the status for a specific power domain. More...
 
void PRCMDeepSleep (void)
 Put the processor into deep-sleep mode. More...
 

Variables

static const uint32_t g_pui32RCGCRegs []
 
static const uint32_t g_pui32SCGCRegs []
 
static const uint32_t g_pui32DCGCRegs []
 

Macro Definition Documentation

#define PRCM_PERIPH_INDEX (   a)    (((a) >> 8) & 0xf)
#define PRCM_PERIPH_MASKBIT (   a)    (0x00000001 << ((a) & 0xf))

Variable Documentation

const uint32_t g_pui32DCGCRegs[]
static
Initial value:
=
{
PRCM_O_GPTCLKGDS,
PRCM_O_SSICLKGDS,
PRCM_O_UARTCLKGDS,
PRCM_O_I2CCLKGDS,
PRCM_O_SECDMACLKGDS,
PRCM_O_GPIOCLKGDS,
PRCM_O_I2SCLKGDS
}

Definition at line 112 of file prcm.c.

Referenced by PRCMPeripheralDeepSleepDisable(), and PRCMPeripheralDeepSleepEnable().

const uint32_t g_pui32RCGCRegs[]
static
Initial value:
=
{
PRCM_O_GPTCLKGR,
PRCM_O_SSICLKGR,
PRCM_O_UARTCLKGR,
PRCM_O_I2CCLKGR,
PRCM_O_SECDMACLKGR,
PRCM_O_GPIOCLKGR,
PRCM_O_I2SCLKGR
}

Definition at line 88 of file prcm.c.

Referenced by PRCMPeripheralRunDisable(), and PRCMPeripheralRunEnable().

const uint32_t g_pui32SCGCRegs[]
static
Initial value:
=
{
PRCM_O_GPTCLKGS,
PRCM_O_SSICLKGS,
PRCM_O_UARTCLKGS,
PRCM_O_I2CCLKGS,
PRCM_O_SECDMACLKGS,
PRCM_O_GPIOCLKGS,
PRCM_O_I2SCLKGS
}

Definition at line 100 of file prcm.c.

Referenced by PRCMPeripheralSleepDisable(), and PRCMPeripheralSleepEnable().