CC26xx Driver Library
aon_rtc.h File Reference
#include <stdbool.h>
#include <stdint.h>
#include <inc/hw_types.h>
#include <inc/hw_memmap.h>
#include <inc/hw_aon_rtc.h>
#include <driverlib/debug.h>

Go to the source code of this file.

Macros

#define AON_RTC_CH_NONE   0x0
 
#define AON_RTC_CH0   0x1
 
#define AON_RTC_CH1   0x2
 
#define AON_RTC_CH2   0x4
 
#define AON_RTC_ACTIVE   0x8
 
#define AON_RTC_CONFIG_DELAY_NODELAY   0
 
#define AON_RTC_CONFIG_DELAY_1   1
 
#define AON_RTC_CONFIG_DELAY_2   2
 
#define AON_RTC_CONFIG_DELAY_4   3
 
#define AON_RTC_CONFIG_DELAY_8   4
 
#define AON_RTC_CONFIG_DELAY_16   5
 
#define AON_RTC_CONFIG_DELAY_32   6
 
#define AON_RTC_CONFIG_DELAY_48   7
 
#define AON_RTC_CONFIG_DELAY_64   8
 
#define AON_RTC_CONFIG_DELAY_80   9
 
#define AON_RTC_CONFIG_DELAY_96   10
 
#define AON_RTC_CONFIG_DELAY_112   11
 
#define AON_RTC_CONFIG_DELAY_128   12
 
#define AON_RTC_CONFIG_DELAY_144   13
 
#define AON_RTC_MODE_CH1_CAPTURE   1
 
#define AON_RTC_MODE_CH1_COMPARE   0
 
#define AON_RTC_MODE_CH2_CONTINUOUS   1
 
#define AON_RTC_MODE_CH2_NORMALCOMPARE   0
 

Functions

static void AONRTCEnable (void)
 Enable the RTC. More...
 
static void AONRTCDisable (void)
 Disable the RTC. More...
 
static void AONRTCReset (void)
 Reset the RTC. More...
 
static bool AONRTCActive (void)
 Check if the RTC is active (enabled). More...
 
static bool AONRTCChannelActive (uint32_t ui32Channel)
 Check if an RTC channel is active (enabled). More...
 
static void AONRTCDelayConfig (uint32_t ui32Delay)
 Configure Event Delay for the RTC. More...
 
static void AONRTCCombinedEventConfig (uint32_t ui32Channels)
 Configure the source of the combined event. More...
 
static void AONRTCEventClear (uint32_t ui32Channel)
 Clear event from a specified channel. More...
 
static bool AONRTCEventGet (uint32_t ui32Channel)
 Get event status for a specified channel. More...
 
static uint32_t AONRTCSecGet (void)
 Get integer part (seconds) of RTC free-running timer. More...
 
static uint32_t AONRTCFractionGet (void)
 Get fractional part (sub-seconds) of RTC free-running timer. More...
 
static uint32_t AONRTCSubSecIncrGet (void)
 Get the sub second increment of the RTC. More...
 
static void AONRTCModeCh1Set (uint32_t ui32Mode)
 Set operational mode of channel 1. More...
 
static uint32_t AONRTCModeCh1Get (void)
 Get operational mode of channel 1. More...
 
static void AONRTCModeCh2Set (uint32_t ui32Mode)
 Set operational mode of channel 2. More...
 
static uint32_t AONRTCModeCh2Get (void)
 Get operational mode of channel 2. More...
 
static void AONRTCChannelEnable (uint32_t ui32Channel)
 Enable event operation for the specified channel. More...
 
static void AONRTCChannelDisable (uint32_t ui32Channel)
 Disable event operation for the specified channel. More...
 
static void AONRTCCompareValueSet (uint32_t ui32Channel, uint32_t ui32CompValue)
 Set the compare value for the given channel. More...
 
static uint32_t AONRTCCompareValueGet (uint32_t ui32Channel)
 Get the compare value for the given channel. More...
 
uint32_t AONRTCCurrentCompareValueGet (void)
 Get the current value of the RTC counter in a format that matches RTC compare values. More...
 
uint64_t AONRTCCurrent64BitValueGet (void)
 Get the current 64-bit value of the RTC counter. More...
 
static void AONRTCIncValueCh2Set (uint32_t ui32IncValue)
 Set the channel 2 increment value when operating in continuous mode. More...
 
static uint32_t AONRTCIncValueCh2Get (void)
 Get the channel2 increment value when operating in continuous mode. More...
 
static uint32_t AONRTCCaptureValueCh1Get (void)
 Get the channel 1 capture value. More...